Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
NX-IGBT-Slide9

Powerex offers a wide lineup of 6th generation 1700 volt options in the NX-M and NX-L packages such as a 75A 7-pack, 150, 200, 300, and 450 amp dual modules in the NX-M package 450 and 600A dual modules in the NX-L package. Note that the VLA500K-01R DC/DC converter and hybrid IC gate driver can be used in conjunction with the 1700 volt NX-Series modules.

PTM Published on: 2014-04-09