Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
NX-IGBT-Slide4

Due to the better characteristics highlighted in the previous table the simulation at the top of this slide shows that operation at 5kHz results in 6% lower losses than company B’s module. The ΔTj  is significantly lower as well, 13° versus 17° for the competing module. At 10kHz the results are even better, 7% lower losses and ΔTj  is 19° versus 25° for Company B.

PTM Published on: 2014-04-09