Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
NX-IGBT-Slide6

The Powerex VLA536-01R is a complete gate driver assembly designed to mount directly to the 1200 volt NX-M dual IGBT modules. It provides 2500Vrms electrical isolation and up to 5A of gate current; sufficient to drive the entire lineup of NX-M 1200 volt duals. The VLA536-01R provides an easy plug-in solution to prototype IGBT designs, and can be used as a production gate driver solution.

PTM Published on: 2014-04-09