Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Features and Benefits

Hakko’s redesigned thermal wire stripper boasts an improved blade alignment which includes set screws to ensure ideal blade alignment. Its integrated handpiece holder maximizes workbench space, providing a shield which prevents the operator from getting burned. The blade removal plate on the holder displaces the blades from the handpiece without touching them. The ergonomic design of the handpiece has a built-in heat resistance feature which provides another layer of protection to the operator while working. The G4 blades possess an optimized edge for wire stripping and have superior thermal performance that make wire stripping even easier than before.

PTM Published on: 2021-11-05