Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
SBR Solutions
Turn key software stack means fully qualified, production ready, feature rich software that covers most of the engineering requirements out of the box thus significantly reducing the design cycle time line. The USP is hardware acceleration of various work loads. This enhances application performance and reduces CPU utilization as the work loads are not processed by the ARM cores. The same software stack and architecture is supported on LS1024A, LS1043A, and LS1046A which gives the engineers the flexibility to build scalable platforms that can deliver performance from 2 to 20 Gbps.
PTM Published on: 2018-09-13