Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
S08D-Slide4
The 9S08DZ is pin, peripheral, and tool compatible with the previous AZ and GZ versions, as well as between the other members in the S08D family. The primary differences between the DN, DV, and the DZ are the EEPROM and CAN bus capabilities. For customers that only need EEPROM and not CAN, the DN version is offered. For customers that only need the CAN interface and not the EEPROM, the DV version is offered. If both CAN and EEPROM are needed, the DZ version is available.
PTM Published on: 2011-09-19