Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
summary

In summary, the FR-410 High Power Desoldering Station provides 24V output, 140 watts of power, and 3 temperature presets along with the widest selection of nozzle configurations that can meet almost every need. The two option handpieces accommodate most applications and allow the operator to use the handpiece that best suits the situation. There are a variety of replacement parts available to an operator when needed.

PTM Published on: 2016-12-09