Partitioning and IoT Design Brings 8-bit MCUs into the Limelight
Contributed By Electronic Products
2014-10-29
Although microcontroller system design practice started to shift toward 32-bit devices several years ago, the dominance of uncomplicated circuits and thin clients in Internet of Things (IoT) applications is likely to keep the 8-bit MCU market on a healthy growth path. This will add to the already healthy 8-bit market in automotive, industrial, and commercial applications that so far has not moved to 32-bit instructions set devices.
From a market-share perspective, there is little doubt that the design world is evolving toward 32-bit MCUs, according to UK-based market research firm IC Insights. In 2013, 32-bit MCU shipments increased by about 20 percent while 4/8-bit MCUs shipments grew by about 6 percent and 16-bit volume grew by 9 percent. Despite the growing popularity of 32-bit designs, however, unit volumes of 4/8-bit and 16-bit MCUs continue to be larger, as shown in Figure 1.

The growth of 32-bit computing is due to several factors, including a trend toward unit costs that are, in some instances, competitive with the smaller-bit-width MCUs. From a technical perspective, 32-bit popularity is due to its expanded memory requirements, native 32-bit math, and advanced peripherals.
When these features are not required, the case for choosing 32-bit MCUs is considerably weakened and one of these applications domains is IoT.
IoT example
It is a foregone conclusion that managing a single sensor or a small group of sensors in smart home applications — such as thermostats or monitoring whether a door is open or closed — requires only an 8-bit MCU from a performance perspective. Once the data is delivered to a gateway device, however, security, privacy, and computing requirements — as well as the advantage of coding in C — often put the application in the 32-bit space.
Similarly, any wearable health device, such as a blood pressure cuff or glucose meter that can be purchased off-the-shelf in a pharmacy or other retail outlet, will have an 8-bit MCU managing the sensor. A 32-bit MCU may be included if data has to be transported through a gateway. The same is true in industrial and commercial applications.
In short, partitioning a design can lead to savings in cost, design time, and power consumption, as well as making the design easier to upgrade to the next generation.
Unfortunately, not all products benefit from the advantages of design partitioning because some designers almost automatically opt for a 32-bit MCU for every part of an IoT-connected system. They believe its expanded memory requirements, native 32-bit math, and advanced peripherals are always an advantage. These decisions are often based on misconceptions.
A few misconceptions that can lead to a sub-optimal decision include:
- The 8-bit architecture suffers from low-code density. This is true only if the designer asks the MCU to do 32-bit math. Control applications, such as offloading the main processor, do not suffer from low density. Since 8-bit MCUs have very little overhead code, total code density for control-type functions is higher than equivalent functions implemented on 32-bit MCUs.
- 32-bit pricing is comparable to 8-bit pricing. Actually, fab process shrinks for 32-bit MCUs do not have the same linear relationship with total chip area and cost as they do for DRAM (or 8-bit MCUs for that matter). This is because the 32-bit architecture and peripherals have higher gate counts than 8-bit architectures and consume more silicon area when compared to 8-bit solutions in the same process geometry. Moving to a smaller process geometry shrinks the digital portion (which is about half the area of a typical 32-bit MCU). Moving to a new process node, therefore, does not deliver savings. During the first few years of a process node — when it is in high demand and producing lower volume, costs per device actually increase.
- 32-bit execution is invariably faster than 8-bit. While 32-bit MCUs operate at higher clock rates, their architecture, which is layered to facilitate easier coding, gets in the way when only a few bits are being processed. For simple control applications, 8-bit MCUs are more deterministic and perform better.
Silicon vendors with 8-bit product lines have added features that remove whatever perceived edge the 32-bit MCU may have at the periphery of an IoT system. This most often takes the form of integrating analog peripherals. One example is capacitive touch.
Although IoT applications are usually thought of as machine-to-machine (M2M) interactions, human-to-machine interfaces (HMI) also have a significant role to play. Handheld, human-operated industrial devices, toys, gaming machines, and remote controls, as well as control panels for white goods such as washers, dryers, ovens, and dishwashers now all offer an IoT dimension.
Capacitive touch is a prominent HMI implementation technology. By integrating a 10-bit ADC, voltage reference, charge-timing capacitance to digital converter, and a temperature sensor in an 8-bit MCU, capacitive-sensing functionality can be achieved at optimal cost.
Silicon Labs' F97x MCU family offers a leading example of this technology. The C8051F970-A-GM features a sub-micro-amp (<1 µA) wake-on-touch average current, 16-bit resolution, and 100:1 dynamic range to support buttons, sliders, wheels, and capacitive proximity sensing with up to 43 channels and multiple scanning modes.
Figure 2 is a generic-block diagram for the C8051F97XX Silicon Labs 8-bit MCU family.

Another MCU vendor that has integrated capacitive-sensing peripherals into their 8-bit chips is Microchip Technology. Its PIC10F204 family includes the PIC10F204T-I/OT. Unlike the 8051-based Silicon Labs chip, it has a RISC architecture with only 33 single-word single-cycle (1 µs) instructions, except for program branches, which take two cycles.
A different approach to capacitive-touch applications — still utilizing 8-bit MCUs — is to provide software and ancillary hardware that works with a general-purpose MCU to create a capacitive-sensing system. Atmel Corporation’s QTouch Library helps designers implement capacitive-touch button, slider, and wheel functionality into its general-purpose 8-bit AVR MCUs, such as the ATTINY5-TSHR.
The QTouch Library files for each device and supports different numbers of touch channels, enabling both flexibility and efficiency in touch applications. By selecting the library file supporting the exact number of channels needed, developers can achieve a more compact and efficient code using less RAM.
Motor control
The final example of analog peripherals making 8-bit MCUs ideal for IoT applications is motor control.
In smart homes, commercial HVAC systems, and some industrial networks, the value of controlling brushless DC motors remotely is a growing use of IoT application space. In this M2M application, the process for selecting when to use an 8-bit MCU is once again a matter of partitioning. Not much computing power is required simply to spin the motor in these relatively simple applications.
Silicon Labs' C8051F850-C-GM illustrates the degree to which innovative design raises 8-bit MCUs to a new level of motor control performance. Silicon Labs chip designers started with a high-speed 8051 core that enables finer pulse-width modulation (PWM), enhanced motor-control efficiency and the ability to execute more complex algorithms for a broad range of motor speeds.
The F85x/6x family of MCUs also support three independent high-resolution PWM channels, with a built-in overcurrent protection/fault detection capability specifically targeting motor control and power supply applications. Also integrated are a 12-bit multi-channel analog-to-digital converter (ADC), two analog comparators with programmable hysteresis and response time, and a precise internal voltage reference.
Conclusion
Although the trend toward 32-bit MCUs is cutting into the market share of 4-, 8-, and 16-bit MCUs, the older chips are still going strong in several markets and IoT applications will in all likelihood benefit from the 8-bit chips in particular. While some MCU vendors have virtually abandoned the older architectures, a few are tweaking them in interesting ways to provide better performance and functionality than their 32-bit competitors.
Benefiting from these advantages is sometimes overlooked because there is no reason that 32-bit MCUs cannot be configured with the same analog peripherals — and MCU vendors do exactly that. In order to recognize the benefits of 8-bit MCUs, design engineers should partition their systems and look for places on the periphery where 8-bit devices actually deliver better performance.
Sensor management and motor control are good examples in the IoT application space. In many instances they require none of the three core features of 32-bit devices. The same is true for automotive and industrial applications where the MCU is located at the periphery.
For more information on the parts discussed in this article, use the links provided to access product information pages on the DigiKey website.
Disclaimer: The opinions, beliefs, and viewpoints expressed by the various authors and/or forum participants on this website do not necessarily reflect the opinions, beliefs, and viewpoints of DigiKey or official policies of DigiKey.