Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Gyro-Slide4

Available measurement range combinations are ±100°/s gyroscope with ±2g 3-axis accelerometer, or ±300°/s gyroscope with ±6g 3-axis accelerometer. The stand alone SCR1100 gyroscopes provide the same gyro performance as the gyros in the SCC1300, but without the accelerometer. Additionally, the SCC1300 and SCR1100 use the same package, so they are pin-to-pin compatible.

PTM Published on: 2010-01-19