Maker.io main logo

VL53L5CX Time of Flight (ToF) breakout and MicroPython

344

2022-08-11 | By Pimoroni

License: See Original Project Time-of-Flight (ToF)

Courtesy of Pimoroni

Guide by Pimoroni

This super quick guide will show you how to use our new VL53L5CX distance ‎sensor breakout with a Raspberry Pi Pico (or other RP2040 board) using ‎pirate brand MicroPython.‎

About VL53L5CX

VL53L5CX is a fancy new Time of Flight (ToF) distance sensor from ‎STMicroelectronics. It can do fast and accurate multizone ranging - find out ‎more about its vital statistics on the shop page!‎

The firmware for this sensor is rather large, so we've not included it into our ‎MicroPython build as standard - you'll need to download it separately and ‎copy it across using Thonny. We'll show you how to do that here, but If you're ‎brand new to Pico/RP2040 microcontrollers you might also find our beginner ‎friendly Getting Started with Raspberry Pi Pico guide useful.‎

Installing MicroPython

download_1

  • Hold down the BOOT button of your microcontroller, and then plug in ‎the USB cable (or tap the RESET button if you have one). This will put it ‎into bootloader mode, and it should appear as a drive on your computer ‎called RPI-RP2.‎

  • Copy the .uf2 file to the RPI-RP2 drive and your microcontroller will ‎reboot running MicroPython. From now on, it won't show up as a drive, ‎you'll need to use an interpreter (Thonny) to program it.‎

Installing Thonny

Download and install Thonny. It's available for Windows, Mac, and ‎Linux.‎

• Open up Thonny. Make sure the interpreter (shown in the box on the ‎bottom right corner) is set to 'MicroPython (Raspberry Pi Pico)' and that ‎the 'Files' window is visible (if not, it's under 'View > Files'). If set up ‎correctly, it should look something like this:‎

files_2

If you don't see the MicroPython prompt in the 'Shell' box, try pressing the ‎‎'stop' button to interrupt whatever your microcontroller is doing.‎

Installing VL53L5CX Firmware

  • Download the VL53L5CX firmware.‎

  • Navigate to the .bin file using the top 'Files' box in Thonny. Right click ‎on it and select 'Upload to /' to save it to your Pico.‎

navigate_3

Note that the .bin firmware file must be named 'vl53l5cx_firmware.bin' and it ‎must be in the root directory of your microcontroller's filesystem.‎

Running the Examples

  • You can find the MicroPython VL53L5CX examples here. Copy and ‎paste one into Thonny and press the green 'run' button to run it on your ‎Pico (you'll be prompted to give it a filename if you haven't run it ‎before).‎

  • Wiggle your fingers in front of the sensor to check that it's working!‎

working_3

Using Alternate I2C Pins

Most boards use GP4 and GP5 as the I2C pins for their Breakout Garden slots ‎and Qw/ST connectors so our examples will assume you're using those pins ‎by default. However, the Breakout Garden slots on Pico Explorer Base (and ‎the Qw/ST connectors on some of our more crowded RP2040 boards, ‎like Interstate 75, Plasma 2040, and Servo 2040) use alternate I2C pins - ‎GP20 and GP21.‎

If you have a board that uses the alternate pins you'll need find this line in ‎your code:

Copy Code

and change it to:‎

Copy Code

Next Steps

We mounted one of these breakouts on the front of a tiny Raspberry Pi Pico-‎powered robot we made using our new Motor SHIM for Pico and adapted the ‎object tracking example to get it to follow a business card on a stick. Here is ‎BusinessBot in action!‎

steps_4

That's all folks!‎

Référence fabricant VL53L5CX-SATEL
BREAKOUT BOARDS FOR VL53L5CX
STMicroelectronics
Référence fabricant PIM550
PICO EXPLORER BASE
Pimoroni Ltd
Référence fabricant PIM584
INTERSTATE 75
Pimoroni Ltd
Référence fabricant PIM582
PLASMA 2040
Pimoroni Ltd
Référence fabricant PIM622
VL53L5CX 8X8 TIME OF FLIGHT (TOF
Pimoroni Ltd
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.