Articles et blogs

Image of Utilizing GMSL for High Bandwidth Robotic Vision Applications Utilizing GMSL for High-Bandwidth Robotic Vision Applications Date de publication : 2026-04-23

ADI's GMSL simplifies the development of high-bandwidth, low-latency robotic vision applications.

Image of Power Resistor Selection Tips for Industrial Motor Drives Power Resistor Selection Tips for Industrial Motor Drives Date de publication : 2026-04-22

Learn how carefully selected power resistors with specialized architectures solve inrush, braking, and thermal challenges in industrial motor drives.

Image of Webinar – Making CO2 Sensing Mainstream: Miniaturized, Efficient, and Cost Optimized Webinar – Making CO2 Sensing Mainstream: Miniaturized, Efficient, and Cost Optimized

This webinar will dive into how to overcome traditional CO2 sensor constraints without sacrificing performance.

Image of Beginner Parts Kit Identification Guide Beginner Parts Kit Identification Guide

In this tutorial, we'll provide a quick rundown of each part in the kit, to help reinforce your understanding of the component. For some parts, we'll include an example application, in case you're in need of a circuit to plug your new toys into.

Image of How ODU MINI-SNAP® & ODU MEDI-SNAP® Elevate the Catheter Market with Connector Solutions How ODU MINI-SNAP® & ODU MEDI-SNAP® Elevate the Catheter Market with Connector Solutions

ODU MEDI-SNAP® interconnect solutions have IEC 60601-1 compliance, sterilization compatibility, rapid custom prototyping, and regulatory alignment.

Image of Resistor-Integrated Microswitches Improve System Reliability Through Four-State Detection Resistor-Integrated Microswitches Improve System Reliability Through Four-State Detection Date de publication : 2026-04-21

Resistor-integrated microswitches simplify wiring and improve system reliability with four-state detection for self-diagnosis and remote fault monitoring.

Image of How Hardware Gets Hacked (Part 3): Adopting the Attacker Mindset How Hardware Gets Hacked (Part 3): Adopting the Attacker Mindset

Explore how attackers gather device info, map inputs, and uncover vulnerabilities using reconnaissance in embedded hardware security.

Image of Webinar – Technologies Driving Drones, Autonomy, and eVTOL Webinaire – Technologies au service des drones, de l'autonomie et des systèmes eVTOL

Ce webinaire explique comment le variateur de fréquence Altivar™ ATV320 de Schneider Electric permet de relever les défis de la commande moteur.

Image of Piezoelectric Ceramics: Driving the Silent Interaction Revolution Piezoelectric Ceramics: Driving the Silent Interaction Revolution

Piezoelectric ceramic technology generates an electric charge when subjected to mechanical stress and undergoes deformation when an electric field is applied.

Image of Kitronik Arcade for BBC micro:bit and MakeCode Arcade Kitronik Arcade for BBC micro:bit and MakeCode Arcade

If you want to learn to code, learning to write games is a great way to get started, and our new hand held gamer has everything you need right now and it also has the connectivity for everything you might need tomorrow.

Image of Selecting Power Supplies for Harsh Industrial Applications and Hazardous Locations Selecting Power Supplies for Harsh Industrial Applications and Hazardous Locations Date de publication : 2026-04-16

Designers of industrial systems for harsh and potentially explosive environments must select power supplies that prioritize reliability and safety.

Image of Webinar – Programming Hardware Two Ways: CircuitPython and Verilog Webinaire – Deux approches de programmation matérielle : CircuitPython et Verilog

Ce webinaire présente la conception de systèmes embarqués via les niveaux d'abstraction logicielle et matérielle.

Image of Optimize High-Current Buck-Boost DC/DC Converter Efficiency Optimiser le rendement des convertisseurs CC/CC abaisseurs-élévateurs à fort courant Date de publication : 2026-04-15

Utilisez des régulateurs abaisseurs-élévateurs µModule pour trois approches architecturales d'intégration des inductances et de détection de courant pour la conversion CC/CC à fort courant.

Image of Webinar – Topology is Just the Start: Building Reliable Wide-Input SEPIC Converters Webinaire – La topologie n'est que le début : concevoir des convertisseurs SEPIC à large plage d'entrée fiables

La réussite d'une conception robuste et adaptée à la production exige une compréhension du comportement des composants, des contraintes électriques et des limites de conception pratiques, ainsi que la sélection de la topologie SEPIC.

Image of Sound Generation and Musical Microcontrollers Sound Generation and Musical Microcontrollers

Explore audio output options, including piezos, speakers, DACs, and playback boards for creating music and sound effects in microcontroller projects.

Image of Understanding Field Programmable Analog Arrays in Modern Mixed-Signal Design Comprendre les composants analogiques programmables dans la conception à signaux mixtes moderne Date de publication : 2026-04-14

Les composants analogiques programmables (FPAA) permettent de configurer les fonctionnalités analogiques via logiciel plutôt que via des chaînes de signaux analogiques fixes au niveau du matériel.

Image of Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1) Low-Cost, Power Efficient EMG Prosthetic Hand (Part 1)

Developing prosthetic technology that is both affordable and functional is challenging in today’s space, mainly due to the costly fabrication and specialized calibration requirements.

Image of Building a Dynamometer for the Openwheel Project - Part 1 Building a Dynamometer for the Openwheel Project - Part 1

Explore a custom-built dyno for hub motors using load cells and Arduino, enabling accurate power and torque measurements.

Image of The Importance of Certification in the Selection of Connector Products Importance de la certification lors de la sélection de connecteurs

La certification des produits garantit la sécurité, la fiabilité et la compatibilité des produits et des opérations.

Image of The Kitronik ARCADE Max for Makecode Arcade The Kitronik ARCADE Max for Makecode Arcade

Introducing the new ARCADE Max for Makecode Arcade from Kitronik, gamification has never been this exciting! It’s our smallest handheld gamer to date but packs the biggest screen we’ve ever had!