Versafit V2/V4 Tubing Spec Datasheet by TE Connectivity Raychem Cable Protection

View All Related Products | Download PDF Datasheet
American Sociexy for Testing and Materials ASTM)
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision.
TE Connectivity
300 Constitution Drive
Menlo Park, CA 94025 USA
Raychem
Tubing
Specification
This Issue:
Date:
Replaces:
RW-3023
Issue 9
Nov 21, 2016
Issue 8
VERSAFIT V2 AND V4 TUBING
Polyolefin, Flexible, Heat-Shrinkable, Flame-Retardant
1. SCOPE
This specification covers the requirements for one type of flexible electrical insulating, extruded tubing whose
diameter will reduce to a predetermined size upon the application of heat in excess of 90°C (194°F). The
tubing is free of polybrominated biphenyls (PBB) and polybrominated biphenyl oxides (PBBO).
VERSAFIT V2, a standard wall 125°C, VW-1 rated, UL recognized tubing meeting the requirements of
UL 224. VERSAFIT V2 also meets the requirements of Standard C22.2 No. 198.1 and is CSA certified.
VERSAFIT V4, a thin wall very flexible 125°C, 300 volt, VW-1 rated, UL recognized tubing meeting the
requirements of UL 224. VERSAFIT V4 also meets the requirements of Standard C22.2 No. 198.1 and is
CSA certified with a 150 volt rating.
2. APPLICABLE DOCUMENTS
This specification takes precedence over documents referenced herein. Unless otherwise specified, the latest
issued of referenced documents applies. The following documents form a part of this specification to the
extent specified herein.
2.1 UNDERWRITERS LABORATORIES, INCORPORATED
UL Subject 224 Extruded Insulating Tubing
(Copies of UL publication may be obtained from Underwriters Laboratories, Inc., 1285 Walt Whitman Road,
Melville, Long Island, New York 11746.)
2.2 CANADIAN STANDARDS ASSOCIATION
C22.2 No. 198.1 Extruded Insulating Tubing
(Copies of CSA publications may be obtained from Canadian Standards Association, 1897 Rexdale
Boulevard, Rexdale, Ontario, Canada M9W 1R3.)
2.3 OTHER PUBLICATIONS
ISO 846 Plastics-Evaluation of the action of microorganisms
(Copies of ISO publications may be obtained from the International Organization for Standardization, 1, rue
de Varembé, CH-1211 Geneva 20, Switzerland or via the ISO website at
http://www.iso.ch/iso/en/ISOOnline.frontpage)
American Society for Testing and Materials (ASTM)
ASTM D 2671 Standard Methods of Testing Heat-Shrinkable Tubing for Electrical Use
(Copies of ASTM publications may be obtained from the American Society for Testing and Materials, 1916
Race Street, Philadelphia, Pennsylvania 19103.)
Quahficauon Tcsls Acccglancc Tests Quahficauon Tcsl Sam glcs Acccglancc Test Sam glcs
Page 2 SPECIFICATION RW-3023 ISSUE 9
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
3. REQUIREMENTS
3.1 MATERIAL
The tubing shall be fabricated from thermally stabilized, flame-retardant, modified polyolefin and shall be
crosslinked by irradiation. It shall be homogeneous and essentially free from flaws, defects, pinholes,
bubbles, seams, cracks and inclusions.
3.2 PROPERTIES
The tubing shall meet the requirements of Table 3.
3.3 COLOR
The tubing shall be available in black, white, red, yellow, blue, green, brown, orange, violet and gray.
4. QUALITY ASSURANCE PROVISIONS
4.1 CLASSIFICATION OF TESTS
4.1.1 Qualification Tests
Qualification tests are those performed on tubing submitted for qualification as a satisfactory product and
shall consist of all tests listed in this specification.
4.1.2 Acceptance Tests
Acceptance tests are those performed on tubing submitted for acceptance under contract. Acceptance tests
shall consist of the following:
Dimensions
Longitudinal Change
Tensile Strength
Ultimate Elongation
4.2 SAMPLING INSTRUCTIONS
4.2.1 Qualification Test Samples
Qualification test samples shall consist of 15m (50 feet) of tubing of the size and color specified.
Qualification of one size or color shall qualify all sizes and colors.
4.2.2 Acceptance Test Samples
Acceptance test samples shall consist of not less than 5m (16 feet) of tubing selected at random from each lot.
A lot shall consist of all tubing of the same size from the same production run and offered for inspection at the
same time.
4.3 TEST PROCEDURES
Unless otherwise specified, tests shall be performed on specimens which have been fully recovered by
conditioning in accordance with 4.3.1 Prior to all testing, the test specimen (and measurement gauges, when
applicable) shall be conditioned for 3 hours at 23 ± 3°C (73 ± 5°F) and 50 ± 5 percent relative humidity. All
ovens shall be of the mechanical convection type in which air passes the specimens at a velocity of 30 - 60m
(100 to 200 feet) per minute.
Dimension ( 1d Lolwiludinal Change Te 8 Slrenglh and Ultimate Elong n Secanl Modulus Copper Slab|l|lv Dielectric W|lh§land, Breakdowl | Effecl
SPECIFICATION RW-3023 ISSUE 9 Page 3
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
4.3.1 Dimensions and Longitudinal Change
Three 150mm (6 inch) specimens of tubing, as supplied, shall be measured for length, to an accuracy of
± 1 mm 1/32 inch) and inside diameter in accordance with ASTM D 2671. The specimens then shall be
conditioned for 3 minutes in a 200 ± 3°C (392 ± 5°F) oven, removed from the oven, cooled to 23 ± 3°C
(73 ± 5°F), re-measured for length, inside diameter and wall thickness in accordance with ASTM D 2671.
The longitudinal change shall be calculated as follows:
C = L1 - L0
L0 x 100
Where: C = Longitudinal Change (percent)
L0 = Length Before Conditioning [mm (inches)]
L1 = Length After Conditioning [mm (inches)]
4.3.2 Tensile Strength and Ultimate Elongation
The tensile strength and ultimate elongation of the tubing shall be determined in accordance with
ASTM D 2671 using 25mm (1 inch) bench marks and a 25 mm (1 inch) initial jaw separation. The speed of
jaw separation shall be 500 ± 50 mm (20 ± 2 inches) per minute.
4.3.3 Secant Modulus
The secant modulus of the tubing shall be tested using tubing as supplied in accordance with ASTM D 2671.
4.3.4 Copper Stability
Three 150mm (6 inch) specimens of tubing shall be slipped over a snug filling, straight, clean, bare copper
conductor. For tubing sizes 1/4 and smaller a solid conductor shall be used; for tubing sizes 3/8 and larger a
solid or tubular conductor shall be used. The specimens on the conductors shall be conditioned for 24 hours
in a desiccator or similar humidity chamber at 90 to 95 percent relative humidity and 23 ± 3°C (73 ± 5°F)
(three specimens shall be conditioned for 7 days in 158.0 ± 1.0°C (316.4± 1.8°F) oven. After conditioning,
the specimens shall be removed from the oven and cooled to 23 ± 3°C (73 ± 5°F). The copper conductor then
shall be removed from the tubing, the tubing and conductor shall then be examined. Darkening of the copper
due to normal air oxidation shall not be cause for rejection. The tubing then shall be conditioned at room
temperature for 16 to 96 hours and tested for ultimate elongation in accordance with 4.3.2.
4.3.5 Dielectric Withstand, Breakdown and Strength
The dielectric strength of the tubing shall be measured under oil in accordance with ASTM D 2671. Five
150mm (6 inch) specimens of tubing shall be recovered over a metal mandrel by conditioning for 3 minutes in
a 200 ± 3°C (392 ± 5°F) oven. The mandrel diameter shall be slightly larger than the fully recovered inside
diameter of the tubing being tested. The metal mandrel shall serve as one electrode and a 25mm (1 inch) wide
strip of lead foil wrapped around the outside of the tubing as the other electrode. The test voltage shall be
applied at a rate of rise of 500 volts per second. Thickness measurements for calculating dielectric strength
shall be made adjacent to the point of breakdown. Specimens for dielectric withstand shall be held for 60
seconds at 2500 volts.
4.3.6 Corrosive Effect
Three specimens of tubing shall be tested for copper contact corrosion in accordance with ASTM D 2671,
Procedure B. Three specimens shall be conditioned for 7 days in a 158.0 ± 1.0°C (316.4 ± 1.8°F) oven.
After conditioning, the specimens shall be visually examined for evidence of corrosion.
4.4 REJECTION AND RETEST
Failure of any samples of tubing to conform to any one of the requirements of this specification shall be cause
for rejection of the lot represented. Tubing which has been rejected may be replaced or reworked to correct
the defect and then resubmitted for acceptance. Before resubmitting, full particulars concerning the rejection
and the action taken to correct the defect shall be furnished to the inspector.
AsSu liedmlm) As Recovered (mm) Inside Diameter Wall Thickness Inside Diameter Wall '1 ickness
Page 4 SPECIFICATION RW-3023 ISSUE 9
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
5. PREPARATION FOR DELIVERY
5.1 FORM
The tubing shall be supplied on spools, unless otherwise specified.
5.2 PACKAGING
Packaging shall be in accordance with good commercial practice.
5.3 MARKING
Each container of tubing shall be permanently and legibly marked with the size, quantity, manufacturer's
identification, specification number, product designation and lot number.
TABLE 1
V2 TUBING DIMENSIONS,
METRIC
As Recovered (mm)
Inside Diameter
Wall Thickness
Inside Diameter
Wall Thickness
Size
nominal
maximum
minimum
0.8/0.4
1.2 ± 0.2
0.2
0.4
0.33
1.0/0.5
1.5 ± 0.2
0.2
0.5
0.33
1.5/0.75
2.1 ± 0.2
0.2
0.75
0.36
2.0/1.0
2.6 ± 0.2
0.25
1.0
0.43
2.5/1.25
3.1 ± 0.2
0.25
1.25
0.43
3.0/1.5
3.6 ± 0.2
0.25
1.5
0.43
3.5/1.75
4.1 ± 0.3
0.25
1.75
0.43
4.0/2.0
4.6 ± 0.3
0.25
2.0
0.43
5.0/2.5
5.6 ± 0.3
0.3
2.5
0.56
6.0/3.0
6.6 ± 0.3
0.3
3.0
0.56
7.0/3.5
7.6 ± 0.3
0.3
3.5
0.56
8.0/4.0
8.6 ± 0.3
0.3
4.0
0.56
9.0/4.5
9.6 ± 0.3
0.3
4.5
0.56
10.0/5.0
10.4 ± 0.3
0.3
5.0
0.56
11.0/5.5
11.4 ± 0.3
0.3
5.5
0.56
12.0/6.0
12.7 ± 0.3
0.3
6.0
0.56
13.0/6.5
13.5 ± 0.3
0.35
6.5
0.66
14.0/7.0
14.4 ± 0.4
0.35
7.0
0.68
15.0/7.5
15.7 ± 0.4
0.35
7.5
0.68
16.0/8.0
16.9 ± 0.4
0.35
8.0
0.68
18.0/9.0
19.0 ± 0.4
0.4
9.0
0.76
20.0/10.0
21.4 ± 0.4
0.4
10.0
0.76
22.0/11.0
23.2 ± 0.4
0.45
11.0
0.89
25.0/12.5
26.8 ± 0.4
0.45
12.5
0.89
27.0/12.5
28.2 ± 0.5
0.45
12.5
0.89
28.0/14.0
30.0 ± 0.5
0.45
14.0
0.89
30.0/15.0
32.1 ± 0.5
0.45
15.0
0.89
As Sn lied mm As Recovered mm Inside Diameter “'21" Thickness Inside Diameter Wall Thickness
SPECIFICATION RW-3023 ISSUE 9 Page 5
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
TABLE 2
V4 TUBING DIMENSIONS,
METRIC
As Supplied (mm)
As Recovered (mm)
Inside Diameter
Wall Thickness
Inside Diameter
Wall Thickness
Size
nominal
maximum
minimum
0.4/0.2
0.7 ± 0.2
0.1
0.22
0.187
0.6/0.3
0.95 ± 0.25
0.1
0.3
0.187
0.8/0.4
1.2 ± 0.25
0.1
0.4
0.25
1.0/0.5
1.4 ± 0.25
0.1
0.5
0.25
1.5/0.75
1.9 ± 0.25
0.1
0.75
0.25
2.0/1.0
2.3 ± 0.25
0.1
1.0
0.25
2.5/1.25
2.8 ± 0.25
0.15
1.25
0.25
3.0/1.5
3.3 ± 0.25
0.15
1.5
0.25
3.5/1.75
3.8 ± 0.25
0.15
1.75
0.25
4.0/2.0
4.4 ± 0.25
0.15
2.0
0.25
5.0/2.5
5.5 ± 0.25
0.15
2.5
0.25
6.0/3.0
6.5 ± 0.4
0.15
3.0
0.28
7.0/3.5
7.5 ± 0.4
0.15
3.5
0.28
8.0/4.0
8.5 ± 0.4
0.15
4.0
0.28
9.0/4.5
9.5 ± 0.4
0.15
4.5
0.28
10.0/5.0
10.5 ± 0.5
0.15
5.0
0.28
V4 TUBING DIMENSIONS,
USA CUSTOMARY
AS SUPPLIED
RECOVERED
Inside Diameter
Inside Diameter
Wall Thickness
Size
Minimum
Maximum
mm.
in.
mm.
in.
mm.
in.
3/64
1.17
.046
0.58
.023
.30 ± .05
.012 ± .002
1/16
1.60
.063
0.79
.031
.30 ± .05
.012 ± .002
3/32
2.36
.093
1.17
.046
.30 ± .05
.012 ± .002
1/8
3.17
.125
1.57
.062
.33 ± .05
.013 ± .002
3/16
4.74
.187
2.36
.093
.33 ± .05
.013 ± .002
1/4
6.35
.250
3.17
.125
.36 ± .05
.014 ± .002
3/8
9.52
.375
4.74
.187
.36 ± .05
.014 ± .002
1/2
12.70
.500
6.35
.250
.36 ± .05
.014 ± .002
3/4
19.05
.750
9.52
.375
.46 ± .08
.017 ± .003
1
25.40
1.000
12.70
.500
.51 ± .08
.020 ± .003
METHOD
Page 6 SPECIFICATION RW-3023 ISSUE 9
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
TABLE 3
Requirements
PROPERTY
UNIT
REQUIREMENT
TEST
METHOD
PHYSICAL
Dimensions
mm (inches)
In accordance with Table 1
Section 4.3.1
Dimensional Recovery
ASTM D 2671
Longitudinal Change
Section 4.3.1
V2 - ASTM D 2671
Percent
+1, -5
ASTM D 2671
V4 ASTMD 2671
Percent
+1, -15
ASTMD 2671
UL 224
Percent
+3, -3
UL 224
Eccentricity (Recovered)
Percent
30 maximum
ASTM D 2671
Tensile Strength
MPa (psi)
10.3 (1500) minimum
Section 4.3.2
Ultimate Elongation
Percent
200 minimum
ASTM D 2671
Secant Modulus (expanded)
MPa (psi)
172 (2.5 x 104) maximum
ASTM D 2671
Low Temperature Flexibility
1 hour at -30°C (-22°F)
--
No cracking
UL 224
Heat Shock
4 hours at 250°C (482°F)
--
No cracking
UL 224
Heat Aging
7 days at 158°C (316
F)
Followed by tests for:
--
--
UL 224
Tensile Strength
MPa (psi)
70% minimum of unaged specimens
Section 4.3.2
UL 224
Ultimate Elongation
Percent
100 minimum
Flexibility
--
No cracking
Dielectric Withstand at 2500 V
Seconds
60 minimum
Dielectric Breakdown
Volts
50% minimum of unaged specimen
Section 4.3.5
ASTM D 2671
Dielectric Strength
kV/mm
(Volts/mil)
19.7 (500) minimum
Copper Stability
7 days at 158°C (316°F)
Followed by test for
No brittleness, glazing, cracking or
severe discoloration of tubing. No
pitting or blackening of copper.
Section 4.3.4
ASTM D 2671
Ultimate Elongation
Percent
100 minimum
Section 4.3.2
Restricted Shrinkage
--
Pass
UL 224
ELECTRICAL
Dielectric Withstand at 2500 V
Seconds
60 minimum
UL 224
Dielectric Strength
kV/mm
(Volts/mil)
19.7 (500) minimum
Section 4.3.5
Volume Resistivity
Ohm-cm
1 x 1014 minimum
ASTM D 2671
METHOD
SPECIFICATION RW-3023 ISSUE 9 Page 7
© 2004-2016 TE Connectivity Ltd. All rights reserved
If this document is printed it becomes uncontrolled. Check for the latest revision
TABLE 3
Requirements
(continued)
PROPERTY
UNIT
REQUIREMENT
TEST
METHOD
CHEMICAL (continued)
Corrosive Effect
7 days at 158° C (316°F)
--
No Corrosion
Section 4.3.6
ASTM D 2671
Flammability
--
Pass
UL 224, VW-1
Water Absorption (Recovered)
24 hrs at 23°C ± 2° C ( 73°F ± 3° F )
Percent
0.5 maximum
ASTM D 2671
Fungus Resistance
Followed by tests for:
Tensile Strength
Ultimate Elongation
Dielectric Strength
MPa (psi)
percent
Volts per mm
(volts per mil)
10.3 (1500) minimum
200 minimum
19,700 (500) minimum
ISO 846
Method B
Section 4.3.2
ASTM D 2671
ASTM D 2671

Products related to this Datasheet

HEATSHRINK 0.3" X 164' BLACK
HEATSHRK BLK 0.183X6" 1=50PC
HEATSHRINK 0.181" X 656.2' BLACK
HEATSHRINK 0.378" X 164' BLACK
HEATSHRK BLK 0.339X0.75" 1=50PC
HEAT SHRINK TUBING BLACK 1M
HEATSHRINK 0.45" X 164' BLACK
HEATSHRINK 0.075" X 656.2' BLACK
HEATSHRINK 0.221" X 328.1' BLACK
HEAT SHRINK TUBING BLACK 1M
HEATSHRINK 0.102" X 656.2' BLACK
HEATSHRINK 0.531" X 164' BLACK
HEATSHRINK 0.13" X 656.2' BLACK
HEAT SHRINK TUBING BLACK 2M
HEATSHRK BLK 0.175X1" 1=50PC
HEATSHRINK 0.175" X 656.2' BLACK
HEAT SHRINK TUBING BLACK 5M
HEATSHRINK 0.409" X 164' BLACK
HEATSHRINK 0.161" X 656.2' BLACK
HEATSHRINK 0.083" X 656.2' BLACK
HEATSHRINK 0.092" X 656.2' BLACK
HEATSHRINK 0.122" X 656.2' BLACK
HEATSHRINK 0.843" X 164' BLACK
HEATSHRK BLK 0.75" 1=50PC
HEAT SHRINK TUBING BLACK 5M
HEATSHRINK 0.567" X 164' BLACK
HEATSHRINK 0.142" X 656.2' BLACK
HEATSHRINK 0.339" X 164' BLACK
HEATSHRINK 0.26" X 328.1' BLACK
HEAT SHRINK TUBING BLACK 25M