STK12C68-5 Datasheet by Infineon Technologies

3m \e under
STK12C68-5 (SMD5962-94599)
64 Kbit (8K x 8) AutoStore nvSRAM
Cypress Semiconductor Corporation 198 Champion Court San Jose,CA 95134-1709 408-943-2600
Document Number: 001-51026 Rev. ** Revised March 02, 2009
Features
35 ns and 55 ns access times
Hands off automatic STORE on power down with external
68 µF capacitor
STORE to QuantumTrap™ nonvolatile elements is initiated
by software, hardware, or AutoStore™ on power down
RECALL to SRAM initiated by software or power up
Unlimited Read, Write, and Recall cycles
1,000,000 STORE cycles to QuantumTrap
100 year data retention to QuantumTrap
Single 5V+10% operation
Military temperature
28-pin (300mil) CDIP and 28-pad LCC packages
Functional Description
The Cypress STK12C68-5 is a fast static RAM with a nonvol-
atile element in each memory cell. The embedded nonvolatile
elements incorporate QuantumTrap technology producing the
world’s most reliable nonvolatile memory. The SRAM provides
unlimited read and write cycles, while independent nonvolatile
data resides in the highly reliable QuantumTrap cell. Data
transfers from the SRAM to the nonvolatile elements (the
STORE operation) takes place automatically at power down.
On power up, data is restored to the SRAM (the RECALL
operation) from the nonvolatile memory. Both the STORE and
RECALL operations are also available under software control.
A hardware STORE is initiated with the HSB pin.
Logic Block Diagram
STORE/
RECALL
CONTROL
POWER
CONTROL
SOFTWARE
DETECT
STATIC RAM
ARRAY
128 X 512
Quantum Trap
128 X 512
STORE
RECALL
COLUMN I/O
COLUMN DEC
ROW DECODER
INPUT BUFFERS
OE
CE
WE
HSB
V
CC V
CAP
A0- A12
A0A1A2A3A4A10
A5
A6
A7
A8
A9
A11
A12
DQ0
DQ1
DQ2
DQ3
DQ4
DQ5
DQ6
DQ7
[+] Feedback
iiCYPRESS rfarnrM mul:10 2‘ij: / IT 1“ 7 3 2 1 23 27 A" :2 n :I v: AeRA 26H HSB 1» I:« as :| >151! ( ;A3 A‘ I:A 25 :l A. “<5 25j="" “:5="" “:l="" "v="" ara="" 24;a9="" aa="" cs="" 2:="" :|="" 1="" a3="" ’7="" 2%="" a“="" a:="" l:1="" top="" vpew="" 22="" :|="" oz="" a2[‘g="" (top)="" 22:10?="" “:2="" s:="" ajaw="" a‘:="" ,‘a="" a1="" :9="" mafia="" cae)="" m="" :|="" ce="" 1[’9="" 21=""> w A“ CW 15 :| am Au }‘0 ZOWCE W I:” us :I Dos DQuE“ IBSDQY om :42 17 :| Des DO , 13 DO w :4; u :I my p12 j s C“ ‘5 3 \ LULE )EJA/ N M o" c7 c? g > o o a
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 2 of 18
Pinouts
Pin Definitions
Pin Name Alt IO Type Description
A0–A12 Input Address Inputs. Used to select one of the 8,192 bytes of the nvSRAM.
DQ0-DQ7Input or Output Bidirectional Data IO Lines. Used as input or output lines depending on operation.
WE WInput Write Enable Input, Active LOW. When the chip is enabled and WE is LOW, data on the IO
pins is written to the specific address location.
CE EInput Chip Enable Input, Active LOW. When LOW, selects the chip. When HIGH, deselects the
chip.
OE GInput Output Enable, Active LOW. The active LOW OE input enables the data output buffers during
read cycles. Deasserting OE HIGH causes the IO pins to tri-state.
VSS Ground Ground for the Device. The device is connected to ground of the system.
VCC Power Supply Power Supply Inputs to the Device.
HSB Input or Output Hardware Store Busy (HSB). When LOW, this output indicates a Hardware Store is in
progress. When pulled low external to the chip, it initiates a nonvolatile STORE operation. A
weak internal pull up resistor keeps this pin high if not connected (connection optional).
VCAP Power Supply AutoStore Capacitor. Supplies power to nvSRAM during power loss to store data from SRAM
to nonvolatile elements.
Figure 1. Pin Diagram - 28-Pin DIP Figure 2. Pin Diagram - 28-Pin LLC
[+] Feedback
if CYPRESS r1570.» Geigerforms a gamgp JI‘ aid aflxher add A Wr _ _ le prior (Le rin ffl’ soy beffi @E me entireiv is m L w flflflflflflflflflflflflflfl \ UUUUUUUUUUUf lakfl acefl
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 3 of 18
Device Operation
The STK12C68-5 nvSRAM is made up of two functional compo-
nents paired in the same physical cell. These are an SRAM
memory cell and a nonvolatile QuantumTrap cell. The SRAM
memory cell operates as a standard fast static RAM. Data in the
SRAM is transferred to the nonvolatile cell (the STORE
operation) or from the nonvolatile cell to SRAM (the RECALL
operation). This unique architecture enables the storage and
recall of all cells in parallel. During the STORE and RECALL
operations, SRAM Read and Write operations are inhibited. The
STK12C68-5 supports unlimited reads and writes similar to a
typical SRAM. In addition, it provides unlimited RECALL opera-
tions from the nonvolatile cells and up to one million STORE
operations.
SRAM Read
The STK12C68-5 performs a Read cycle whenever CE and OE
are LOW while WE and HSB are HIGH. The address specified
on pins A0–12 determines the 8,192 data bytes accessed. When
the Read is initiated by an address transition, the outputs are
valid after a delay of tAA (Read cycle 1). If the Read is initiated
by CE or OE, the outputs are valid at tACE or at tDOE, whichever
is later (Read cycle 2). The data outputs repeatedly respond to
address changes within the tAA access time without the need for
transitions on any control input pins, and remains valid until
another address change or until CE or OE is brought HIGH, or
WE or HSB is brought LOW.
SRAM Write
A Write cycle is performed whenever CE and WE are LOW and
HSB is HIGH. The address inputs must be stable prior to entering
the Write cycle and must remain stable until either CE or WE
goes HIGH at the end of the cycle. The data on the common IO
pins DQ0–7 are written into the memory if it has valid tSD, before
the end of a WE controlled Write or before the end of an CE
controlled Write. Keep OE HIGH during the entire Write cycle to
avoid data bus contention on common IO lines. If OE is left LOW,
internal circuitry turns off the output buffers tHZWE after WE goes
LOW.
AutoStore Operation
The STK12C68-5 stores data to nvSRAM using one of three
storage operations:
1. Hardware store activated by HSB
2. Software store activated by an address sequence
3. AutoStore on device power down
AutoStore operation is a unique feature of QuantumTrap
technology and is enabled by default on the STK12C68-5.
During normal operation, the device draws current from VCC to
charge a capacitor connected to the VCAP pin. This stored
charge is used by the chip to perform a single STORE operation.
If the voltage on the VCC pin drops below VSWITCH, the part
automatically disconnects the VCAP pin from VCC. A STORE
operation is initiated with power provided by the VCAP capacitor.
Figure 3 shows the proper connection of the storage capacitor
(VCAP) for automatic store operation. A charge storage capacitor
between 68 µF and 220 µF (+20%) rated at 6V must be provided.
The voltage on the VCAP pin is driven to 5V by a charge pump
internal to the chip. A pull up is placed on WE to hold it inactive
during power up.
In system power mode, both VCC and VCAP are connected to the
+5V power supply without the 68 μF capacitor. In this mode, the
AutoStore function of the STK12C68-5 operates on the stored
system charge as power goes down. The user must, however,
guarantee that VCC does not drop below 3.6V during the 10 ms
STORE cycle.
To reduce unnecessary nonvolatile stores, AutoStore, and
Hardware Store operations are ignored, unless at least one Write
operation has taken place since the most recent STORE or
RECALL cycle. Software initiated STORE cycles are performed
regardless of whether a Write operation has taken place. An
optional pull up resistor is shown connected to HSB. The HSB
signal is monitored by the system to detect if an AutoStore cycle
is in progress.
Figure 3. AutoStore Mode
9FF
9
&$3
PK
2N
)
5
Y
PK2N
:(
+6%
9VV
)
5
VVDS\
%
[+] Feedback
if CYPRESS warn... w TORE WA? {or con gin \s DELAY SRAM lake SRAM H et SHAM Rea to comp Write f how u STORE w m resismrg: K1206i5 ‘Wfi atioi
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 4 of 18
Figure 4. AutoStore Inhibit Mode
If the power supply drops faster than 20 us/volt before Vcc
reaches VSWITCH, then a 2.2 ohm resistor must be connected
between VCC and the system supply to avoid momentary
excess of current between VCC and VCAP
.
AutoStore Inhibit Mode
If an automatic STORE on power loss is not required, then VCC
is tied to ground and +5V is applied to VCAP (Figure 4). This is
the AutoStore Inhibit mode, where the AutoStore function is
disabled. If the STK12C68-5 is operated in this configuration,
references to VCC are changed to VCAP throughout this data
sheet. In this mode, STORE operations are triggered through
software control or the HSB pin. To enable or disable Autostore
using an IO port pin see Preventing Store on page 5. It is not
permissible to change between these three options “on the
fly”.
Hardware STORE (HSB) Operation
The STK12C68-5 provides the HSB pin for controlling and
acknowledging the STORE operations. The HSB pin is used
to request a hardware STORE cycle. When the HSB pin is
driven LOW, the STK12C68-5 conditionally initiates a STORE
operation after tDELAY
. An actual STORE cycle only begins if a
Write to the SRAM takes place since the last STORE or
RECALL cycle. The HSB pin also acts as an open drain driver
that is internally driven LOW to indicate a busy condition, while
the STORE (initiated by any means) is in progress.
SRAM Read and Write operations, that are in progress when
HSB is driven LOW by any means, are given time to complete
before the STORE operation is initiated. After HSB goes LOW,
the STK12C68-5 continues SRAM operations for tDELAY
.
During tDELAY, multiple SRAM Read operations take place. If
a Write is in progress when HSB is pulled LOW, it allows a
time, tDELAY to complete. However, any SRAM Write cycles
requested after HSB goes LOW are inhibited until HSB returns
HIGH.
During any STORE operation, regardless of how it is initiated,
the STK12C68-5 continues to drive the HSB pin LOW,
releasing it only when the STORE is complete. After
completing the STORE operation, the STK12C68-5 remains
disabled until the HSB pin returns HIGH.
If HSB is not used, it is left unconnected.
Hardware RECALL (Power Up)
During power up or after any low power condition (VCC <
VRESET), an internal RECALL request is latched. When VCC
once again exceeds the sense voltage of VSWITCH, a RECALL
cycle is automatically initiated and takes tHRECALL to complete.
If the STK12C68-5 is in a Write state at the end of power up
RECALL, the SRAM data is corrupted. To help avoid this
situation, a 10 Kohm resistor is connected either between WE
and system VCC or between CE and system VCC.
Software STORE
Data is transferred from the SRAM to the nonvolatile memory
by a software address sequence. The STK12C68-5 software
STORE cycle is initiated by executing sequential CE controlled
Read cycles from six specific address locations in exact order.
During the STORE cycle, an erase of the previous nonvolatile
data is first performed followed by a program of the nonvolatile
elements. When a STORE cycle is initiated, input and output
are disabled until the cycle is completed.
Because a sequence of Reads from specific addresses is
used for STORE initiation, it is important that no other Read or
Write accesses intervene in the sequence. If they intervene,
the sequence is aborted and no STORE or RECALL takes
place.
To initiate the software STORE cycle, the following Read
sequence is performed:
1. Read address 0x0000, Valid READ
2. Read address 0x1555, Valid READ
3. Read address 0x0AAA, Valid READ
4. Read address 0x1FFF, Valid READ
5. Read address 0x10F0, Valid READ
6. Read address 0x0F0F, Initiate STORE cycle
The software sequence is clocked with CE controlled Reads
or OE controlled Reads. When the sixth address in the
sequence is entered, the STORE cycle commences and the
chip is disabled. It is important that Read cycles and not Write
cycles are used in the sequence. It is not necessary that OE
is LOW for a valid sequence. After the tSTORE cycle time is
fulfilled, the SRAM is again activated for Read and Write
operation.
Software RECALL
Data is transferred from the nonvolatile memory to the SRAM
by a software address sequence. A software RECALL cycle is
initiated with a sequence of Read operations in a manner
similar to the software STORE initiation. To initiate the
RECALL cycle, the following sequence of CE controlled Read
operations is performed:
1. Read address 0x0000, Valid READ
2. Read address 0x1555, Valid READ
3. Read address 0x0AAA, Valid READ
[+] Feedback
a} QEBESS ’EIIOIM isfis an_V fimSLm dbye mm mm mm «M; S 8 8 mm. m Cam: (mm 8 8 8 8 8 m cms' so ma no mo Qummu ‘ x. ‘ I“, CMos 50 ‘00 150 200 cm- mum-y must 0v CC 5 sz n the w
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 5 of 18
4. Read address 0x1FFF, Valid READ
5. Read address 0x10F0, Valid READ
6. Read address 0x0F0E, Initiate RECALL cycle
Internally, RECALL is a two step procedure. First, the SRAM data
is cleared; then, the nonvolatile information is transferred into the
SRAM cells. After the tRECALL cycle time, the SRAM is again
ready for Read and Write operations. The RECALL operation
does not alter the data in the nonvolatile elements. The nonvol-
atile data can be recalled an unlimited number of times.
Data Protection
The STK12C68-5 protects data from corruption during low
voltage conditions by inhibiting all externally initiated STORE
and Write operations. The low voltage condition is detected
when VCC is less than VSWITCH. If the STK12C68-5 is in a Write
mode (both CE and WE are low) at power up after a RECALL or
after a STORE, the Write is inhibited until a negative transition
on CE or WE is detected. This protects against inadvertent writes
during power up or brown out conditions.
Noise Considerations
The STK12C68-5 is a high speed memory. It must have a high
frequency bypass capacitor of approximately 0.1 µF connected
between VCC and VSS, using leads and traces that are as short
as possible. As with all high speed CMOS ICs, careful routing of
power, ground, and signals reduce circuit noise.
Hardware Protect
The STK12C68-5 offers hardware protection against inadvertent
STORE operation and SRAM Writes during low voltage condi-
tions. When VCAP<VSWITCH, all externally initiated STORE
operations and SRAM Writes are inhibited. AutoStore can be
completely disabled by tying VCC to ground and applying +5V to
VCAP
. This is the AutoStore Inhibit mode; in this mode, STOREs
are only initiated by explicit request using either the software
sequence or the HSB pin.
Low Average Active Power
CMOS technology provides the STK12C68-5 the benefit of
drawing significantly less current when it is cycled at times longer
than 50 ns. Figure 5 and Figure 6 shows the relationship
between ICC and Read or Write cycle time. Worst case current
consumption is shown for both CMOS and TTL input levels
(commercial temperature range, VCC = 5.5V, 100% duty cycle
on chip enable). Only standby current is drawn when the chip is
disabled. The overall average current drawn by the STK12C68-5
depends on the following items:
The duty cycle of chip enable
The overall cycle rate for accesses
The ratio of Reads to Writes
CMOS versus TTL input levels
The operating temperature
The VCC level
Preventing Store
The STORE function is disabled by holding HSB high with a
driver capable of sourcing 30 mA at a VOH of at least 2.2V,
because it must overpower the internal pull down device. This
device drives HSB LOW for 20 μs at the onset of a STORE.
When the STK12C68-5 is connected for AutoStore operation
(system VCC connected to VCC and a 68 μF capacitor on VCAP)
and VCC crosses VSWITCH on the way down, the STK12C68-5
attempts to pull HSB LOW. If HSB does not actually get below
VIL, the part stops trying to pull HSB LOW and abort the STORE
attempt.
Figure 5. Current Versus Cycle Time (Read)
Figure 6. Current Versus Cycle Time (Write)
[+] Feedback
3.“: alcmmss as A?
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 6 of 18
Best Practices
nvSRAM products have been used effectively for over 15
years. While ease-of-use is one of the product’s main system
values, experience gained working with hundreds of applica-
tions has resulted in the following suggestions as best
practices:
The nonvolatile cells in an nvSRAM are programmed on the
test floor during final test and quality assurance. Incoming
inspection routines at customer or contract manufacturer’s
sites sometimes reprograms these values. Final NV patterns
are typically repeating patterns of AA, 55, 00, FF, A5, or 5A.
The end product’s firmware must not assume that an NV
array is in a set programmed state. Routines that check
memory content values to determine first time system config-
uration, cold or warm boot status, and so on must always
program a unique NV pattern (for example, complex 4-byte
pattern of 46 E6 49 53 hex or more random bytes) as part of
the final system manufacturing test to ensure these system
routines work consistently.
Power up boot firmware routines must rewrite the nvSRAM
into the desired state. While the nvSRAM is shipped in a
preset state, best practice is to again rewrite the nvSRAM
into the desired state as a safeguard against events that
might flip the bit inadvertently (program bugs, incoming
inspection routines, and so on).
The Vcap value specified in this data sheet includes a
minimum and a maximum value size. The best practice is to
meet this requirement and not exceed the maximum Vcap
value because the higher inrush currents may reduce the
reliability of the internal pass transistor. Customers who want
to use a larger Vcap value to make sure there is extra store
charge must discuss their Vcap size selection with Cypress.
Table 1. Hardware Mode Selection
CE WE HSB A12–A0 Mode IO Power
H X H X Not Selected Output High Z Standby
L H H X Read SRAM Output Data Active[3]
L L H X Write SRAM Input Data Active
X X L X Nonvolatile STORE Output High Z ICC2[1]
L H H 0x0000
0x1555
0x0AAA
0x1FFF
0x10F0
0x0F0F
Read SRAM
Read SRAM
Read SRAM
Read SRAM
Read SRAM
Nonvolatile STORE
Output Data
Output Data
Output Data
Output Data
Output Data
Output High Z
Active ICC2[2, 3]
L H H 0x0000
0x1555
0x0AAA
0x1FFF
0x10F0
0x0F0E
Read SRAM
Read SRAM
Read SRAM
Read SRAM
Read SRAM
Nonvolatile RECALL
Output Data
Output Data
Output Data
Output Data
Output Data
Output High Z
Active[2, 3]
Notes
1. HSB STORE operation occurs only if an SRAM Write is done since the last nonvolatile cycle. After the STORE (If any) completes, the part goes into standby
mode, inhibiting all operations until HSB rises.
2. The six consecutive addresses must be in the order listed. WE must be high during all six consecutive CE controlled cycles to enable a nonvolatile cycle.
3. IO state assumes OE < VIL. Activation of nonvolatile cycles does not depend on state of OE.
[+] Feedback
i _ a! CYPRESS 5:1 w ‘0 m w w 0&3 szozv org m m m m Logxc H» E
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 7 of 18
Maximum Ratings
Exceeding maximum ratings may shorten the useful life of the
device. These user guidelines are not tested.
Storage Temperature ................................. –65°C to +150°C
Temperature under Bias ............................. –55°C to +125°C
Voltage on Input Relative to GND.....................–0.5V to 7.0V
Voltage on Input Relative to Vss............–0.6V to VCC + 0.5V
Voltage on DQ0-7 or HSB .......................–0.5V to Vcc + 0.5V
Power Dissipation..........................................................1.0W
DC output Current (1 output at a time, 1s duration) .... 15 mA
Operating Range
Range Ambient Temperature VCC
Military -55°C to +125°C 4.5V to 5.5V
DC Electrical Characteristics
Over the operating range (VCC = 4.5V to 5.5V) [4]
Parameter Description Test Conditions Min Max Unit
ICC1 Average VCC Current tRC = 35 ns
tRC = 55 ns
Dependent on output loading and cycle rate. Values
obtained without output loads.
IOUT = 0 mA.
75
55 mA
mA
ICC2 Average VCC Current
during STORE All Inputs Do Not Care, VCC = Max
Average current for duration tSTORE
3mA
ICC3 Average VCC Current at
tRC= 200 ns, 5V, 25°C
Typical
WE > (VCC – 0.2V). All other inputs cycling.
Dependent on output loading and cycle rate. Values
obtained without output loads.
10 mA
ICC4 Average VCAP Current
during AutoStore Cycle All Inputs Do Not Care, VCC = Max
Average current for duration tSTORE
2mA
ISB1[5] VCC Standby Current
(Standby, Cycling TTL
Input Levels)
tRC = 35 ns, CE > VIH
tRC = 55 ns, CE > VIH
24
19 mA
mA
ISB2 [5] VCC Standby Current CE > (VCC – 0.2V). All others VIN < 0.2V or > (VCC 0.2V).
Standby current level after nonvolatile cycle is complete.
Inputs are static. f = 0 MHz.
2.5 mA
IIX Input Leakage Current VCC = Max, VSS < VIN < VCC -1 +1 μA
IOZ Off State Output
Leakage Current VCC = Max, VSS < VIN < VCC, CE or OE > VIH or WE < VIL -5 +5 μA
VIH Input HIGH Voltage 2.2 VCC + 0.5 V
VIL Input LOW Voltage VSS – 0.5 0.8 V
VOH Output HIGH Voltage IOUT = –4 mA 2.4 V
VOL Output LOW Voltage IOUT = 8 mA 0.4 V
VBL Logic ‘0’ Voltage on
HSB Output IOUT = 3 mA 0.4 V
VCAP Storage Capacitor Between Vcap pin and Vss, 6V rated. 68 µF +20% nom. 54 260 µF
Notes
4. VCC reference levels throughout this data sheet refer to VCC if that is where the power supply connection is made, or VCAP if VCC is connected to ground.
5. CE > VIH does not produce standby current levels until any nonvolatile cycle in progress has timed out.
[+] Feedback
if, a! CYPRESS ‘ TA : 25a
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 8 of 18
Data Retention and Endurance
Parameter Description Min Unit
DATARData Retention 100 Years
NVCNonvolatile STORE Operations 1,000 K
Capacitance
In the following table, the capacitance parameters are listed.[6]
Parameter Description Test Conditions Max Unit
CIN Input Capacitance TA = 25°C, f = 1 MHz,
VCC = 0 to 3.0 V 8pF
COUT Output Capacitance 7pF
Thermal Resistance
In the following table, the thermal resistance parameters are listed.[6]
Parameter Description Test Conditions 28-CDIP 28-LCC Unit
ΘJA Thermal Resistance
(Junction to Ambient) Test conditions follow standard test methods and
procedures for measuring thermal impedance, per
EIA / JESD51.
TBD TBD °C/W
ΘJC Thermal Resistance
(Junction to Case) TBD TBD °C/W
Figure 7. AC Test Loads
AC Test Conditions
5.0V
Output
30 pF
R1 963Ω
R2
512Ω
5.0V
Output
5 pF
R1 963
Ω
R2
512
Ω
For Tri-state Specs
Input Pulse Levels....................................................0V to 3V
Input Rise and Fall Times (10% to 90%)...................... <5 ns
Input and Output Timing Reference Levels.......................1.5
Note
6. These parameters are guaranteed by design and are not tested.
[+] Feedback
ifCYPBESS. w as
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 9 of 18
AC Switching Characteristics
SRAM Read Cycle
Parameter Description 35 ns 55 ns Unit
Min Max Min Max
Cypress
Parameter Alt
tACE tELQV Chip Enable Access Time 35 55 ns
tRC [7] tAVAV, tELEH Read Cycle Time 35 55 ns
tAA [8] tAVQV Address Access Time 35 55 ns
tDOE tGLQV Output Enable to Data Valid 15 35 ns
tOHA [8] tAXQX Output Hold After Address Change 5 5 ns
tLZCE [9] tELQX Chip Enable to Output Active 5 5 ns
tHZCE [9] tEHQZ Chip Disable to Output Inactive 10 12 ns
tLZOE [9] tGLQX Output Enable to Output Active 0 0 ns
tHZOE [9] tGHQZ Output Disable to Output Inactive 10 12 ns
tPU [6] tELICCH Chip Enable to Power Active 0 0 ns
tPD [6] tEHICCL Chip Disable to Power Standby 35 55 ns
Switching Waveforms
Figure 8. SRAM Read Cycle 1: Address Controlled [7, 8]
Figure 9. SRAM Read Cycle 2: CE and OE Controlled [7]
W
5&
W
$$
W
2+$
$''5(66
'4'$7$287 '$7$9$/,'
$''5(66
W
5&
&(
W
$&(
W
/=&(
W
3'
W
+=&(
2(
W
'2(
W
/=2(
W
+=2(
'$7$9$/,'
$&7,9(
67$1'%<
W
38
'4'$7$287
,&&
Notes
7. WE and HSB must be High during SRAM Read cycles.
8. Device is continuously selected with CE and OE both Low.
9. Measured ±200 mV from steady state output voltage.
[+] Feedback
aiCYFBFSS. )
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 10 of 18
SRAM Write Cycle
Parameter Description 35 ns 55 ns Unit
Min Max Min Max
Cypress
Parameter Alt
tWC tAVAV Write Cycle Time 35 55 ns
tPWE tWLWH, tWLEH Write Pulse Width 25 45 ns
tSCE tELWH, tELEH Chip Enable To End of Write 25 45 ns
tSD tDVWH, tDVEH Data Setup to End of Write 12 25 ns
tHD tWHDX, tEHDX Data Hold After End of Write 0 0 ns
tAW tAVWH, tAVEH Address Setup to End of Write 25 45 ns
tSA tAVWL, tAVEL Address Setup to Start of Write 0 0 ns
tHA tWHAX, tEHAX Address Hold After End of Write 0 0 ns
tHZWE [9,10] tWLQZ Write Enable to Output Disable 13 15 ns
tLZWE [9] tWHQX Output Active After End of Write 5 5 ns
Switching Waveforms
Figure 10. SRAM Write Cycle 1: WE Controlled [11, 12]
Figure 11. SRAM Write Cycle 2: CE Controlled [11, 12]
tWC
tSCE
tHA
tAW
tSA
tPWE
tSD tHD
tHZWE tLZWE
ADDRESS
CE
WE
DATA IN
DATA OUT
DATA VALID
HIGH IMPEDANCE
PREVIOUS DATA
t
WC
ADDRESS
t
SA
t
SCE
t
HA
t
AW
t
PWE
t
SD
t
HD
CE
WE
DATA IN
DATA OUT HIGH IMPEDANCE
DATA VALID
Notes
10. If WE is Low when CE goes Low, the outputs remain in the high impedance state.
11. HSB must be high during SRAM Write cycles.
12. CE or WE must be greater than VIH during address transitions.
[+] Feedback
31a PRESS Vcc \lswwcn VREEET Aumsmra POWEREUP RECALL *kmm W L1 1 \ \ m) (DAYA out) fff f POWER up BROWN our RROWN om BROWN our RECALL ND stE Amoslore w Amsm w (No SRAM WRWES) NO RECALL NO RECALL RECALL WHEN «w Du) NOT GD (Vt: Du: NOI’ (30 v” RETURNS BELOW Wm; EELDW qu ABOVE vswaR
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 11 of 18
AutoStore or Power Up RECALL
Parameter Alt Description STK12C68-5 Unit
Min Max
tHRECALL [13] tRESTORE Power up RECALL Duration 550 μs
tSTORE [14, 15, 16] tHLHZ STORE Cycle Duration 10 ms
tDELAY [9, 15] tHLQZ , tBLQZ Time Allowed to Complete SRAM Cycle 1 μs
VSWITCH Low Voltage Trigger Level 4.0 4.5 V
VRESET Low Voltage Reset Level 3.9 V
tVCCRISE VCC Rise Time 150 μs
tVSBL[11] Low Voltage Trigger (VSWITCH) to HSB Low 300 ns
Switching Waveform
Figure 12. AutoStore/Power Up RECALL
WE
Notes
13. tHRECALL starts from the time VCC rises above VSWITCH.
14. CE and OE low for output behavior.
15. CE and OE low and WE high for output behavior.
16. HSB is asserted low for 1us when VCAP drops through VSWITCH. If an SRAM Write has not taken place since the last nonvolatile cycle, HSB is released and no store
takes place.
[+] Feedback
aiCYPBESS. ) @
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 12 of 18
Software Controlled STORE/RECALL Cycle
The software controlled STORE/RECALL cycle follows. [18]
Parameter Alt Description 35 ns 55 ns Unit
Min Max Min Max
tRC[14] tAVAV STORE/RECALL Initiation Cycle Time 35 55 ns
tSA[17] tAVEL Address Setup Time 0 0 ns
tCW[17] tELEH Clock Pulse Width 25 30 ns
tHACE[17] tELAX Address Hold Time 20 20 ns
tRECALL RECALL Duration 20 20 μs
Switching Waveform
Figure 13. CE Controlled Software STORE/RECALL Cycle [18]
t
RC
t
RC
t
SA
t
SCE
t
HACE
t
STORE
/ t
RECALL
DATA VALID
DATA VALID
6#SSERDDA1#SSERDDA
HIGH IMPEDANCE
ADDRESS
CE
OE
DQ (DATA)
Notes
17. The software sequence is clocked on the falling edge of CE without involving OE (double clocking aborts the sequence).
18. The six consecutive addresses must be read in the order listed in Table 1 on page 6. WE must be HIGH during all six consecutive cycles.
[+] Feedback
i a] CYPRESS ) r‘!.‘)w:~. i 1 _ HSBUN) ”m” ‘ fl tom ‘SVORE i 17mm fl) Hsmoun Hm \MFEDANCE S W tutw DQ1DATAOUT) DATAVALID g S DATAVAUD
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 13 of 18
Hardware STORE Cycle
Parameter Alt Description STK12C68-5 Unit
Min Max
tSTORE [9, 14] tHLHZ STORE Cycle Duration 10 ms
tDHSB [14, 19] tRECOVER, tHHQX Hardware STORE High to Inhibit Off 700 ns
tPHSB tHLHX Hardware STORE Pulse Width 15 ns
tHLBL Hardware STORE Low to STORE Busy 300 ns
Switching Waveform
Figure 14. Hardware STORE Cycle
Note
19. tDHSB is only applicable after tSTORE is complete.
[+] Feedback
CYPRESS
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 14 of 18
Speed:
35 - 35 ns
55 - 55 ns
Package:
C = Ceramic 28-pin 300 mil DIP (gold lead finish)
Part Numbering Nomenclature
STK12C68 - 5 C 35 M
Temperature Range:
M - Military (-55 to 125°C)
K
L = Ceramic 28-pin LLC
= Ceramic 28-pin 300 mil DIP (Solder dip finish)
Retention / Endurance
5 = Military (10 years or 10
5
cycles)
Case Outline
X = Ceramic 28-pin 300 mil DIP
Y = Ceramic 28-pin LLC
Device Class Indicator - Class M
SMD5962 - 94599 01 MX X
Lead Finish
A = Solder DIP lead finish
Device Type:
01 = 55 ns
03 = 35 ns
C = Gold lead DIP finish
X = Lead finish “A” or “C” is acceptable
[+] Feedback
is alcyPBEss )
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 15 of 18
Ordering Information
Speed (ns) Ordering Code Package Diagram Package Type Operating Range
35 STK12C68-5C35M 001-51695 28-pin CDIP (300 mil) Military
STK12C68-5K35M 001-51695 28-pin CDIP (300 mil)
STK12C68-5L35M 001-51696 28-pin LCC (350 mil)
55 STK12C68-5C55M 001-51695 28-pin CDIP (300 mil)
STK12C68-5K55M 001-51695 28-pin CDIP (300 mil)
STK12C68-5L55M 001-51696 28-pin LCC (350 mil)
The above table contains Final information. Contact your local Cypress sales representative for availability of these parts
[+] Feedback
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 16 of 18
Package Diagrams
Figure 15. 28-Pin (300-Mil) Side Braze DIL (001-51695)
001-51695 **
[+] Feedback
STK12C68-5 (SMD5962-94599)
Document Number: 001-51026 Rev. ** Page 17 of 18
Figure 16. 28-Pad (350-Mil) LCC (001-51696)
Package Diagrams (continued)
1. ALL DIMENSION ARE IN INCHES AND MILLIMETERS [MIN/MAX]
2. JEDEC 95 OUTLINE# MO-041
3. PACKAGE WEIGHT : TBD
001-51696 **
[+] Feedback
a} CYPRESS ”no."
Document Number: 001-51026 Rev. ** Revised March 02, 2009 Page 18 of 18
AutoStore and QuantumTrap are registered trademarks of Cypress Semiconductor Corporation. All products and company names mentioned in this document may be the trademarks of their respective
holders.
STK12C68-5 (SMD5962-94599)
© Cypress Semiconductor Corporation, 2009. The information contained herein is subject to change without notice. Cypress Semiconductor Corporation assumes no responsibility for the use of any
circuitry other than circuitry embodied in a Cypress product. Nor does it convey or imply any license under patent or other rights. Cypress products are not warranted nor intended to be used for medical,
life support, life saving, critical control or safety applications, unless pursuant to an express written agreement with Cypress. Furthermore, Cypress does not authorize its products for use as critical
components in life-support systems where a malfunction or failure may reasonably be expected to result in significant injury to the user. The inclusion of Cypress products in life-support systems
application implies that the manufacturer assumes all risk of such use and in doing so indemnifies Cypress against all charges.
Any Source Code (software and/or firmware) is owned by Cypress Semiconductor Corporation (Cypress) and is protected by and subject to worldwide patent protection (United States and foreign),
United States copyright laws and international treaty provisions. Cypress hereby grants to licensee a personal, non-exclusive, non-transferable license to copy, use, modify, create derivative works of,
and compile the Cypress Source Code and derivative works for the sole purpose of creating custom software and or firmware in support of licensee product to be used only in conjunction with a Cypress
integrated circuit as specified in the applicable agreement. Any reproduction, modification, translation, compilation, or representation of this Source Code except as specified above is prohibited without
the express written permission of Cypress.
Disclaimer: CYPRESS MAKES NO WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, WITH REGARD TO THIS MATERIAL, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE. Cypress reserves the right to make changes without further notice to the materials described herein. Cypress does not
assume any liability arising out of the application or use of any product or circuit described herein. Cypress does not authorize its products for use as critical components in life-support systems where
a malfunction or failure may reasonably be expected to result in significant injury to the user. The inclusion of Cypress’ product in a life-support systems application implies that the manufacturer
assumes all risk of such use and in doing so indemnifies Cypress against all charges.
Use may be limited by and subject to the applicable Cypress software license agreement.
Document History Page
Sales, Solutions, and Legal Information
Worldwide Sales and Design Support
Cypress maintains a worldwide network of offices, solution centers, manufacturer’s representatives, and distributors. To find the office
closest to you, visit us at cypress.com/sales.
Products
PSoC psoc.cypress.com
Clocks & Buffers clocks.cypress.com
Wireless wireless.cypress.com
Memories memory.cypress.com
Image Sensors image.cypress.com
PSoC Solutions
General psoc.cypress.com/solutions
Low Power/Low Voltage psoc.cypress.com/low-power
Precision Analog psoc.cypress.com/precision-analog
LCD Drive psoc.cypress.com/lcd-drive
CAN 2.0b psoc.cypress.com/can
USB psoc.cypress.com/usb
Document Title: STK12C68-5 (SMD5962-94599), 64 Kbit (8K x 8) AutoStore nvSRAM
Document Number: 001-51026
Rev ECN No. Orig. of
Change Submission
Date Description of Change
** 2666844 GVCH/PYRS 03/02/09 New data sheet
[+] Feedback