AN, PN Assembly Instr Datasheet by Bud Industries

View All Related Products | Download PDF Datasheet
FOR REPLACEMENT GASKET ONLY Center distance between screws on bclh sides of lhe sla ng 9 nl Overlag \ength
Form 518
Revised: 2-8-2014
Procedure for Assembly of Sealing Gasket
For AN, PN & PNR series boxes
1. If you are using the gasket that is included in the box, it is already cut to the exact length, NO
ADDITIONAL CUTTING IS REQUIRED.(move to step 2)
If you received a replacement gasket, cut one end square and perpendicular to length:
NOT THIS WAY
THIS WAY
2. Start laying the gasket in the cover groove approximately 1” from a corner on the longer side as
shown below:
START HERE
GO THIS
DIRECTION
3. Lay down the gasket in the groove of the cover and go in the direction shown. Without stretching
or twisting the gasket, press the gasket down into the groove.
4. Continue laying down the gasket without stretching it until you reach the starting point.
FOR REPLACEMENT GASKET ONLY
Mark the end of the gasket by overlapping the starting end by the amount shown below:
Center distance between screws on both sides
of the starting point
Up to 4
Over 4
Overlap length
1/8”
3/16”
Cut the other end at the marked point square and perpendicular to the length as shown in step 1.
Form 518
Revised: 2-8-2014
5. Butt the end against the starting end in the groove, press against the starting end and then press the
gasket end down into the groove while keeping the pressure against the starting end. This procedure
ensures that there is some compression pressure between the two ends of the gasket.
Fig. 1 Fig. 2 Screw Tiqhtenlnq Sequence For 4'H0leS Screw Titheninq Sequence For 67Holes For 4rhole covers squeeze hard in the middle of the cover aqalnst the bodv. Sometimes on larger PN series boxes with 4 holes vcu may hear a snail noise. This is normal and indicates that the sealing lip in body is now lully seated and aliqned with the gasket.
Form 518
Revised: 2-8-2014
Procedure for Assembly of Cover
For AN, PN & PNR series boxes
1. Cover screws on the PN series are captive screws, so assemble the screws on the cover first by
threading them through the cover holes. Skip this step for AN series.
2. Place the cover over the body and align the screws or cover holes with corresponding holes in the body.
3. Loosely assemble cover screws in sequence shown in figures 1 and 2 below and finger tighten screws.
1
4
3
2
Fig. 1
Screw Tightening Sequence For 4-Holes
6
5
1
4
3
2
Fig. 2
Screw Tightening Sequence For 6-Holes
4. Follow the sequence shown above to tighten all screws to a torque as shown in the table below. Use a
torque screw driver.
Type of Gasket
Torque in Inch-Pounds
Solid Silicone (translucent white)
8
Sponge Silicone (off-white opaque)
6
5. Inspect the sealed joint and ensure that the gasket track in cover is properly aligned with the lip in the
body. For 4-hole covers, squeeze hard in the middle of the cover against the body. Sometimes on
larger PN series boxes with 4 holes, you may hear a snap noise. This is normal and indicates that the
sealing lip in body is now fully seated and aligned with the gasket.
6. Re-tighten the screws again to the proper torque as shown in paragraph 4.

Products related to this Datasheet

BOX ALUM BLACK 4.920"L X 3.150"W
Available Quantity: 77
Unit Price: 36.43
BOX ALUM BLACK 4.920"L X 3.150"W
Available Quantity: 47
Unit Price: 28.94
BOX ALUM BLACK 8.750"L X 5.750"W
Available Quantity: 45
Unit Price: 78.74
BOX ALUM BLACK 7.870"L X 4.270"W
Available Quantity: 33
Unit Price: 69.49
BOX ALUM NATURAL 6.3"L X 3.940"W
Available Quantity: 26
Unit Price: 44.37
BOX ALUM NAT 4.920"L X 3.150"W
Available Quantity: 19
Unit Price: 20.27
BOX ALUM BLACK 3.531"L X 1.409"W
Available Quantity: 18
Unit Price: 28.35
BOX ALUM BLACK 6.300"L X 3.940"W
Available Quantity: 14
Unit Price: 62.29
BOX ALUM NAT 4.920"L X 3.150"W
Available Quantity: 6
Unit Price: 24.09
BOX ALUM BLACK 3.860"L X 2.520"W
Available Quantity: 0
Unit Price: 33.5
BOX ALUM NAT 4.900"L X 3.140"W
Available Quantity: 0
Unit Price: 37.61
BOX ALUM BLACK 4.900"L X 3.140"W
Available Quantity: 0
Unit Price: 38.64
BOX ALUM NAT 4.900"L X 3.140"W
Available Quantity: 0
Unit Price: 37.76
BOX ALUM BLACK 4.900"L X 3.140"W
Available Quantity: 0
Unit Price: 42.6
BOX ALUM NAT 5.910"L X 2.520"W
Available Quantity: 0
Unit Price: 40.4
BOX ALUM BLACK 5.910"L X 2.520"W
Available Quantity: 0
Unit Price: 43.63
BOX ALUM NAT 6.290"L X 3.930"W
Available Quantity: 0
Unit Price: 56.27
BOX ALUM BLACK 6.290"L X 3.930"W
Available Quantity: 0
Unit Price: 62.44
BOX ALUM NAT 6.290"L X 3.930"W
Available Quantity: 0
Unit Price: 66.4
BOX ALUM BLACK 6.290"L X 3.930"W
Available Quantity: 0
Unit Price: 66.7
BOX ALUM BLACK 4.530"L X 2.560"W
Available Quantity: 0
Unit Price: 27.62
BOX ALUM BLACK 4.920"L X 3.150"W
Available Quantity: 0
Unit Price: 27.33
BOX ALUM NAT 4.920"L X 3.150"W
Available Quantity: 0
Unit Price: 19.1
BOX ALUM BLACK 4.920"L X 3.150"W
Available Quantity: 0
Unit Price: 34.52
BOX ALUM NAT 4.920"L X 3.150"W
Available Quantity: 0
Unit Price: 22.77
BOX ALUM BLACK 6.300"L X 3.940"W
Available Quantity: 0
Unit Price: 51.71
BOX ALUM NATURAL 6.3"L X 3.940"W
Available Quantity: 0
Unit Price: 37.32
BOX ALUM NATURAL 6.3"L X 3.940"W
Available Quantity: 0
Unit Price: 40.25
BOX ALUM BLACK 6.300"L X 3.940"W
Available Quantity: 0
Unit Price: 55.24
BOX ALUM NAT 7.870"L X 4.270"W
Available Quantity: 0
Unit Price: 57