VISHAY.
ww vxshay om/how/leadfree
www hay om/doc 9037
www.vxshay.com/doc?20036
www.vishay.com/doc?20008
hIIQ //sm.|ec.ch/Iec62474
e at www.gadsl.og
hmg://echa.eumga.eu/cand \da‘thsHab‘e
mmkmmcmg@wshay.com
www.v\shay.CUm/doc?91000
D/CRCW e3
www.vishay.com Vishay
Revision: 27-Oct-2020 4Document Number: 20035
For technical questions, contact: thickfilmchip@vishay.com
THIS DOCUMENT IS SUBJECT TO CHANGE WITHOUT NOTICE. THE PRODUCTS DESCRIBED HEREIN AND THIS DOCUMENT
ARE SUBJECT TO SPECIFIC DISCLAIMERS, SET FORTH AT www.vishay.com/doc?91000
DESCRIPTION
Production is strictly controlled and follows an extensive set
of instructions established for reproducibility. A cermet film
layer and a glass-over are deposited on a high grade (Al2O3)
ceramic substrate with its prepared inner contacts. A
special laser is used to achieve the target value by smoothly
fine trimming the resistive layer without damaging the
ceramics. The resistor elements are covered by a protective
coating designed for electrical, mechanical and climatic
protection. The terminations receive a final pure tin on nickel
plating.
The result of the determined production is verified by an
extensive testing procedure on 100 % of the individual chip
resistors. Only accepted products are laid directly into
the tape in accordance with IEC 60286-3 Type 1a and
Type 2a (1).
ASSEMBLY
The resistors are suitable for processing on automatic SMD
assembly systems. They are suitable for automatic
soldering using wave, reflow or vapor phase as shown in
IEC 61760-1 (1). The encapsulation is resistant to all
cleaning solvents commonly used in the electronics
industry, including alcohols, esters and aqueous solutions.
The suitability of conformal coatings, potting compounds
and their processes, if applied, shall be qualified by
appropriate means to ensure the long-term stability of the
whole system.
The resistors are RoHS-compliant, the pure tin plating
provides compatibility with lead (Pb)-free and
lead-containing soldering processes. Solderability is
specified for 2 years after production or requalification. The
permitted storage time is 20 years. The immunity of the
plating against tin whisker growth has been proven under
extensive testing.
MATERIALS
Vishay acknowledges the following systems for the
regulation of hazardous substances:
• IEC 62474, Material Declaration for Products of and for the
Electrotechnical Industry, with the list of declarable
substances given therein (2)
• The Global Automotive Declarable Substance List
(GADSL) (3)
• The REACH regulation (1907/2006/EC) and the related list
of substances with very high concern (SVHC) (4) for its
supply chain
The products do not contain any of the banned
substances as per IEC 62474, GADSL, or the SVHC list,
see www.vishay.com/how/leadfree.
Hence the products fully comply with the following
directives:
• 2000/53/EC End-of-Life Vehicle Directive (ELV) and
Annex II (ELV II)
• 2011/65/EU Restriction of the Use of Hazardous
Substances Directive (RoHS) with amendment
2015/863/EU
• 2012/19/EU Waste Electrical and Electronic Equipment
Directive (WEEE)
Vishay pursues the elimination of conflict minerals from its
supply chain, see the Conflict Minerals Policy at
www.vishay.com/doc?49037.
APPROVALS
The resistors are qualified according to AEC-Q200.
Where applicable, the resistors are tested in accordance
with EN 140401-802 which refers to EN 60115-1,
EN 60115-8 and the variety of environmental test
procedures of the IEC 60068 (1) series.
RELATED PRODUCTS
For more information about products with better TCR and
tighter tolerance please refer to the “Lead (Pb)-Free Thick
Film, Rectangular, Semi-Precision Chip Resistors”
datasheet (www.vishay.com/doc?20036).
The D/CRCW with SnPb termination plating is designed for
applications where lead bearing terminations are
mandatory. For ordering D/CRCW with SnPb terminations
please refer to latest edition of datasheet D/CRCW
(www.vishay.com/doc?20008).
Notes
(1) The quoted IEC standards are also released as EN standards with the same number and identical contents
(2) The IEC 62474 list of declarable substances is maintained in a dedicated database, which is available at http://std.iec.ch/iec62474
(3) The Global Automotive Declarable Substance List (GADSL) is maintained by the American Chemistry Council and available at www.gadsl.org
(4) The SVHC list is maintained by the European Chemical Agency (ECHA) and available at http://echa.europa.eu/candidate-list-table