Plug Knockout Tools for 929 Series Datasheet by 3M

View All Related Products | Download PDF Datasheet
Plug Knockout Tools For use with 3M 929 Series .100" Thru Board Sockets 3M offers 2 Plug Knockout Tools for the removal ollnle- gral solder mask plugs {or all levels ofpmducllon. Both are designed for use as a hand 1001. Eaell tool can easlly be adapted for use wllh standard 3Vl presses, The 929013 with Ihe 3640 assembly press and Ille 929012 will: Ille 929050 (long neck) press. For Prototype and Low Volume Production 929013 Knuckulll Tuul (Irma; 304" Pics» For Medium and High Volume Production 929m 2 Knockout Tool (1mm 929050 I‘m. Order Information: Knockout Tool 929013 Nulc. This does not include a molded head. Hand Press (Standard) 3640 Molded Head (with staggered pins) 929025-0)‘(—XX l l : ()ne Row Number ol'plns z = Two Ron per row Order Information: l Klmckoul 'l'ool Kl! 929012 200 Qty. Replacement Pins 929013 l-lund Press(Long neck) 929050
Press Setup 3640 Assembly Press Only With each hand tool, you will receive a plastic sleeve that is designed to slip over the press shofi. This acts as a safety stop so that the pins in the knockout tool will not hit the base of the press. 1. Unscrew the black handle from the knockout tool. 2. a. Remove the four (4) hex screws on the assembly head. b. Remove the two (2) hex screws on the bottom of the assembly head. 0. Slide the shafi out of the assembly head. d. Put the plastic sleeve that comes with each hand tool inside the retunii spring by bending the spring in the middle. e. Replace the shaft by sliding it through the spring and into the plastic sleeve, and then through the press casting f Replace the hex screws removed in steps a and b. Adjust the press to the uppermost position 4. Attach the knockout tool to the shafl using the latch provided. ’r" 929012 Knockout Tool Assembly 1. Loosen the three screws from the pin holder with a 3/32“ allen key wrench. Do not unscrew the cap screws com- pletely. If the center supports should become loose it is important they are correctly reassembled. The pressure heels must face inward. Call 800-225-5373 for sales, ordering and technical product information Important Notice All statements, technical intormation and recommendations related to the Seller's products are based on intormaticn believed to be reliable, but the accuracy or completeness thereol is not guaranteed Belore urilizmg the product. the user should determine the suitability ot the product lor its intended use The user assumes all risks and liability whatsoever in connection with such use Any statements or recommendations or the Seller which are not con- tained in the Seller’s current publications shall have no lorce or eiteci unless contained in an agreement signed by an authorized oltlcer at Electronic Products Divlsion 6801 River Place Blvd Austin, Texas 78726-9000 2. Place the desired number of pins into the pin holder. It is important not to bend the pins. Make sure that all pins are properly positioned in the holder. Tighten all three screws with an allen wrench. Press Setup 929050 Press (Long neck) 1. Loosen the down stop on the press with an allen wrench. 2. Raise the ram and screw the pin holder into the bottom of the ram. 3. To properly align the holder on the press» the holder must be lowered until it rests in the alignment slot. 4. Adjust the down stop on the top of the ram by loosening the two screws with an allen key. Set the tool to your desired height and retighten the screws. A the adj ust- ment for the height is available. This is located on the top of the stop and can be adjusted with an allen key. For more details please refer to ineructions for 929012 & 929050 Literatule code 34-7034-0145—4. Also it is recom- mended to follow detailed instructions on how to use Thru board sockets in your production on "Tech Brief" Literature code 80-6106-0815-2. the Seller The statements contained herelrl are made in lieu at all warranties. express or implied, ll'lcluding but not limited to the implied warranties ol merchantability and litness for a paniculai purpose which warranties are hereby expressly disclaimed Seller shall not be liable to the user or any other person under any legal theory, including but not limited to negligence or strict liability. tor any iniury or tor any direct or consequential damages sustained or incurred by reason or the use bl any ot the seller‘s products that were detective. ® Pnnred on recycled paper. Printed in the USA o (M 1993 Bil-6106413194 (oeeiooiw-t

Products related to this Datasheet

KNOCKOUT TOOL
Available Quantity: 0
Unit Price: 0
REPLACEMENT PIN
Available Quantity: 0
Unit Price: 0