VeriSafe™ AVT Safety Notice Datasheet by Panduit Corp

View All Related Products | Download PDF Datasheet
Insnucmn Manua‘
VeriSafe AVT Safety Notice January 15, 2018
IMPORTANT SAFETY INFORMATION REGARDING
PANDUIT VERISAFE ABSENCE OF VOLTAGE TESTER
VeriSafe AVT Models VS-AVT-C02-L03, VS-AVT-C02-L10, VS-AVT-C08-L10, VS-AVT-RKBB2, VS-AVT-RKBB3, VS-AVT-RKBB4
The VeriSafe AVT Instruction Manual is being updated to provide additional important safety information. Panduit was recently
made aware of a potential connection scheme with the VeriSafe AVT that could result in the VeriSafe AVT showing a green
absence of voltage, when in fact voltage is present. This would only occur if the sensor leads were not properly terminated and
secured. While the probability of this happening is low, Panduit strongly recommends following some simple mitigation techniques
to significantly reduce the likelihood of such failure.
Warning: Please take time to read and follow the mitigation steps on any installed (or to be installed)
VeriSafe AVT at your facility. Failure to perform the recommended mitigation techniques set forth in this
document could result in injury, including death.
This notice applies to VeriSafe AVT units with QC numbers less than 678208002.
Sensor Leads & Connectivity Test
The VeriSafe AVT is designed with two sensor leads for each phase conductor. The two leads in each set have different functions:
one lead is used to detect voltage (detection lead) and the other lead is used to verify that the detection lead is in contact with a
conductor (termination lead). The termination lead does not detect voltage. There are no labels distinguishing the detection and
termination leads for each phase because it is critical that all are properly terminated.
Each time the absence of voltage test is initiated, a “connectivity test” occurs to ensure that each detection lead is in contact with a
conductor. If the connectivity test fails on any detection lead, the green absence of voltage indicator on the AVT will not illuminate.
Potential Installation Issue
If a detection lead is not properly terminated to a power conductor and comes in contact with a low impedance path to ground, the
connectivity test could pass. This may result in a green absence of voltage indication, even though the power conductor is
energized. This scenario would require a series of multiple faults, but is possible if terminations are not made properly and secured.
This is primarily a concern on single-phase systems since they may only have one detection lead terminated to a current carrying
conductor. If the detection lead were to become loose and make contact with a low impedance path to ground, the connectivity
test would pass. However, voltage would not be detected because the termination lead does not detect voltage and the detection
lead is no longer in contact with the power conductor. Therefore, the device could indicate there is no voltage present when in fact
there is voltage.
In the case of split-phase or three-phase systems, this condition is not likely to occur as all detection lead terminations would need
to fail and each detection lead would have to make contact with a low impedance path to ground at the time of the test. However,
even the loss of a single detection lead termination on a multi-phase system could result in the scenario described above, if voltage
was only present on a single phase.
There is a Commissioning Checklist in the Instruction Manual that, if followed correctly, will verify proper function at the time of
installation. Utilization of the commissioning test described in the Instruction Manual, will verify proper functionality of the AVT at
the time of installation and calls attention to inspecting terminations. The failure modes described in this section would be the
result of sensor lead terminations not being maintained over time and sensor leads not being secured to the power conductors at
time of installation.
The likelihood of this scenario occurring can be prevented by using the mitigation techniques described in this notice.
mum ‘ mam 1 5mm ‘ muosws mm K [Nunsuni fl: “ u E“ u n u firm PROYECIWE coNNinoA vsmwn pkamcmz mum-n rewwu Instrucuon Manua‘ Instrunion Manua‘. com vensafe/Vensafe Manual EN
VeriSafe AVT Safety Notice January 15, 2018
Mitigation Technique 1
Securing the sensor leads to the power conductor or another nearby rigid feature would prevent movement in the event that the
termination point failed, significantly reducing the likelihood of that detection lead contacting ground. Sensor Leads can be secured
using cable ties, clamps, mounts, or tape. The sensor leads should be secured at multiple locations, including near the termination
point. This best practice is illustrated in Figure 1 and should be followed for all VeriSafe AVT installations.
In addition, the sensor lead terminations should be inspected periodically, similar to other critical terminations inside an electrical
enclosure, to ensure they are tight and the sensor leads are secure.
Figure 1: Sensor leads are secured with cable ties near the termination point
Mitigation Technique 2
In a single-phase installation, two sets of sensor leads can be terminated to the power conductor and one to the neutral line (see
Figure 2). Using this wiring method creates a redundant detection lead and provides an additional reliability. With this method, if a
detection lead was to separate from the termination point on an energized power conductor and contact a low impedance path to
ground, there would still be a second detection lead on that power conductor to detect any voltage that may be present. This is an
optional connection method that may be utilized in addition to securing the sensor leads.
Single-Phase: 2 Wire + PE Single-Phase: 2 Wire + PE Redundant Detection
Figure 2: Options for wiring the AVT in a single-phase system
Summary
The VeriSafe AVT Instruction Manual (B21052English; B21053Français; B21057Español) is being updated to provide a better
explanation of the sensor lead function and potential for this scenario, along with the mitigation techniques described in this
notice. Please use revision 03 or greater of the Instruction Manual. The current revision can be found at
http://www.panduit.com/verisafe/VeriSafe_Manual_EN. VeriSafe AVT units with QC numbers greater than 678208002 will include
the revised Instruction Manual.
The VeriSafe AVT verifies the absence of voltage before equipment is accessed, allowing qualified electrical workers to confirm an
electrically safe work condition without exposure to electrical hazards in a fraction of the time required when using a hand-held
tester. This product was developed within the strict analysis and reliability requirements of SIL 3 in accordance with the IEC61508
standard. Panduit is committed to the safety of our customers and communicating any new information that will help them install
and use this products in the safest way possible.

Products related to this Datasheet

VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 64
Unit Price: 585.34
VERISAFE INSULATION PIERCING CON
Available Quantity: 61
Unit Price: 194.62
VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 36
Unit Price: 614.59
VERISAFE REPLACEMENT AVT SYSTEM
Available Quantity: 12
Unit Price: 71.86
VERISAFE HAZARDOUS LOCATION AVT-
Available Quantity: 10
Unit Price: 649.13
VERISAFE CONNECTION KIT FOR TAPP
Available Quantity: 5
Unit Price: 122.33
VERISAFE CONNECTION KIT FOR TAPP
Available Quantity: 5
Unit Price: 186.33
VERISAFE CONNECTION KIT FOR TAPP
Available Quantity: 5
Unit Price: 227.01
VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 5
Unit Price: 686.66
VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 4
Unit Price: 633.19
VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 2
Unit Price: 720.66
COMPLETE ENCLOSURE TO RETROFIT E
Available Quantity: 2
Unit Price: 1485.86
VERISAFE ABSENCE OF VOLTAGE TEST
Available Quantity: 0
Unit Price: 0
VERISAFE REPLACEMENT AVT SYSTEM
Available Quantity: 0
Unit Price: 81.73