1096 Datasheet by Adafruit Industries LLC

wad—51mm uuuuuuuuuuuu
Simple RF M4 Receiver - 315MHz
Momentary Type
PRODUCT ID: 1096
Description
These Simple RF receivers are the easiest way possible to add wireless control, painlessly! There's no
programming, configuring or addressing - simply power the receiver with 5-10VDC and press the buttons
on our matching RF keyfob remote. When the A button is pressed, it activates the first pin, when the B
button is pressed, it activates the second one, and so forth for all four buttons. There's no microcontroller
required, its just a simple one-to-one link.
These modules make it easy to control your project once its in an enclosure or from across the room, but
there are some things to watch out for. One is that they do not have 'addressing' - if you have multiple
receivers in a room, they'll all work at the same time with a single remote. Another is that there's no error
checking or bi-directional link - that means the remote doesn't know if the module received the message or
not. Third, there are a few different types of receivers and each one looks identical but they're act
differently!
o The M4 momentary type acts like a push button - when the A button is held down, the matching
pin goes high. When the A button is released, the matching pin goes low. The pins only go high
when a button is pressed
o The T4 toggle type acts like an alternating toggle switch - when the A button is pressed the first
time, the matching pin goes high. When the A button is pressed a second time, the matching pin
goes low. The pins are turned on and off by repeated presses
o The L4 latch type acts like a selector switch - when the A button is pressed the first time, the
matching pin goes high. When the B button is pressed it turns A's pin off and turns B's pin on.
When C is pressed, it turns B off, etc. Only one is on at a time. If you press the same button twice,
it doesn't turn that pin off.
This product ID is for the Momentary M4 type! It only includes the receiver module, you will also need
to pick up a keyfob transmitter Each receiver also has a VT pin, which will go high if any of the pins are
activated. You can sort of use it as an 'interrupt' indicator.
Note: This product may have flux residue on the back, but will still work properly.
Technical Details
Based on the PT2272 chipset
EngineeredinNYCAdafruit®