VHB™ Series Surface Prep Guide Datasheet by 3M (TC)

View All Related Products | Download PDF Datasheet
Technical Bulletin December, 2012
Surface Preparation for
3MVHBTape Applications
Summary Most substrates are best prepared by cleaning with a 50:50 mixture of isopropyl alcohol (IPA)
and water*prior to applying 3M™ VHB™ Tapes.
Exceptions to this general procedure that may require additional surface preparation include:
Heavy Oils: A degreaser or solvent-based cleaner may be required to remove heavy oil or
grease from a surface and should be followed by cleaning with IPA/water.
Abrasion: Abrading a surface, followed by cleaning with IPA/water, can remove heavy dirt
or oxidation and can increase surface area to improve adhesion.
Adhesion Promoters: Priming a surface can significantly improve initial and ultimate
adhesion to many materials such as plastics and paints.
Porous Surfaces: Most porous and fibered materials such as wood, particleboard, concrete
etc. need to be sealed to provide a unified surface.
Unique Materials: Special surface preparation may be needed for glass and glass-like
materials, copper and copper containing metals and plastics or rubber that contain
components that migrate (e.g. plasticizers).
*Note: These cleaner solutions contain greater than 250 g/l of volatile organic compounds (VOC). Please consult your
local Air Quality Regulations to be sure the cleaner is compliant. When using solvents, be sure to follow the manufacturers
precautions and directions for use when handling such materials.
General
Procedure To obtain optimum adhesion, the bonding
surfaces must be well unified, clean and
dry. Typical surface cleaning solvents are
IPA/water mixture (rubbing alcohol) or
heptane.*(Steps A and B)
Bond strength is dependent upon the
amount of adhesive-to-surface contact
developed. Firm application pressure
develops better adhesive contact and helps
improve bond strength. (Steps C and D)
Generally, this means that the tape should
experience at least 15 psi (100 kPa) in roll
down or platen pressure.
(Sources- page #4)
After application, the bond strength
will increase as the adhesive flows
onto the surface. At room temperature,
approximately 50% of the ultimate
strength will be achieved after
20 minutes, 90% after 24 hours and
100% after 72 hours. In some cases,
bond strength can be increased and
ultimate bond strength can be achieved
more quickly by exposure of the bond
to elevated temperatures (e.g. 150°F
[66°C] for 1 hour).
100
80
60
40
20
0
20 MIN 1 HOUR 24 HOURS 72 HOURS
■■■■
150°F or ABRADE
50°F
ROOM TEMP
PERCENT OF FULL BOND
Typical Bond Build Over Time
Step A:
Solvent wipe Step B:
Wipe dry
Step C:
Apply tape to surface Step D:
Roll finished joint
Technical Bulletin
Surface Preparation for 3MVHBTape Applications
Heavy Oils
On surfaces with a light oily film, or other light contamination, the 50:50 IPA/water solution is usually
adequate. Where heavy oils or grease are present, a “degreasing” solvent such as 3M™ Prep Solvent 70,
3M™ Citrus Base Cleaner, mineral spirits, naphtha or similar solvents are suggested to cut the oil. This
should always be followed with an IPA/water cleaning to help ensure that any residue or film is
Abrasion
Abrading a surface can serve several functions:
Remove heavy levels of dirt or oxide from metals or paints (e.g. galvanized steel).
Create additional surface area that can increase adhesion.
Smooth a surface to obtain more flatness, allowing improved contact area.
Abrasion often helps adhesion to paints and plastics. When abrading, it is important for tapes to have a
finely abraded surface. Very small scratches in the surface, generated with circular motion rather than
straight-line motion, are most desirable. A surface with many micro-scratches in it can have up to 40%
additional available surface area, translating to higher ultimate strength and greater initial adhesion.
Scotch-Brite
®
Hand Pads (such as 7447 Maroon or Heavy Duty Green) are good for achieving the right
level of abrasion. Tools such as a power palm sander will assist on large jobs. Avoid grinding a surface
with coarse abrasive materials, since they may create too rough of a texture for the adhesive to
adequately flow into the surface. Always clean the surface with the IPA/water solution or additional
methods previously described, and be certain that all loose particles are removed prior to bonding.
Exceptions to these abrading guidelines are 3M™ VHB™ Tapes 4932 and 4952, as they typically
perform best on smooth glossy surfaces and abrasion may reduce the bond strength.
*Note: These cleaner solutions contain greater than 250 g/l of volatile organic compounds (VOC). Please consult your
local Air Quality Regulations to be sure the cleaner is compliant. When using solvents, be sure to follow the manufacturers
precautions and directions for use when handling such materials.
Adhesion
Promoters
Priming a surface can significantly improve initial and ultimate adhesion to many materials such as
plastics and paints because of their low surface energy or the additives they may contain. A primer
creates a new surface for 3M™ VHB™ Tape to adhere to and can also create a layer that may impede
the migration of additives that may be present in a material. It is important for the user to determine the
suitability of the 3M™ VHB™ Tape, the adhesion promoter and the application process.
Porous
Surfaces
Rough, porous or fibered materials such as wood, particleboard, cement, etc., have an open surface and
require sealing to provide a unified surface for tape bonding. Common sealing materials would include
paint, varnish or other hard surface coatings. Fast drying 3M™ Rubber and Vinyl Spray 80 can also be
used to unify the surface and improve the tape bond.
Unique
Surfaces
Glass, stone, ceramic or other siliceous materials are hydrophilic (water-loving) by nature. Normally, the
hydrophilic nature makes pressure sensitive adhesive bond durability susceptible to change under high
humidity or exposure to moisture. In basic terms, water vapor can undercut the tape bond and interfere
with the normal adhesion forces. Silane coupling agents, added to the IPA/water cleaning solution, can
help reduce the “water-loving” tendency of these surfaces and enhance the tape bond in high moisture
environments.
Copper, brass, and bronze are prone to oxidation even after the 3M™ VHB™ Tape is applied. To prevent
a weakening of the bond, a lacquer or varnish should be applied to these surfaces. Be sure to test the tape
bond to the sealer on a metal surface to verify good adhesion.
Flexible PVC (vinyl) contains plasticizers that can migrate into the tape and affect adhesion. There are
several 3M™ VHB™ Tapes that are formulated to be resistant to plasticizer migration, or 3M™
Scotch-Grip™ Plastic Adhesive 2262, thinned, can serve as a barrier to migration. Rubber materials
(e.g. EPDM, neoprene) can have low surface energy and may also contain plasticizers and oils. These
require the use of an adhesion promoter for stable bond strength. Test for compatibility with flexible
PVC and rubber materials by aging bonded samples for a week at 150°F (66°C) and check for
softening of the adhesive, discoloration or reduction in bond strength.
- 2 -
Technical Bulletin
Surface Preparation for 3MVHBTape Applications
Suggested Primers The table below offers suggested primers and alternative methods that commonly require
primers, adhesion promoters or other surface treatments for successful use with 3M™ VHB™
Tapes. This list is not intended to be fully comprehensive but may be useful for many
applications. It is very important for the user to determine the suitability of the
3M™ VHB™
Tape, primer and application process and compliance with local Air Quality Regulations.
Primer Source
and Description 3M™ Primer 94, 3M™ Adhesion Promoter 111 and 3M™ Silane Glass Treatment AP 115
are available through distributors that carry 3M™ VHB™ Tapes.
3M™ Scotch-Grip™ Plastic Adhesive 2262 must be thinned in acetone or MEK*in a 1:5 or
1:10 ratio (e.g., 1 part Scotch-Grip plastic adhesive 2262 to 5 parts acetone or MEK). The
product is available premixed in either acetone or MEK from: PRC DeSoto at (317) 290-1600.
3M™ Scotch-Grip™ Plastic Adhesive 2262T, thinned in 10:1 MEK solution or 3M™ Scotch-
Grip™ Plastic Adhesive 2262TA, thinned in 10:1 acetone solution.*When diluted in acetone
at this ratio, this material contains 196 g/l VOC.*
Diluted 3M™ Scotch-Grip™ Plastic Adhesive 1099 must be thinned in acetone*in a
1:3 ratio (e.g., 1 part Scotch-Grip plastic adhesive 1099 to 3 parts acetone). This thinned
material contains zero VOC’s when diluted in these ratios.
3M™ Adhesion Promoter N-200J is available from PRC DeSoto at (317) 290-1600.
Silane Coupling Agent is also available premixed in a 91:9 IPA/water solution or as a
concentrate. A 0.5 wt. % level of silane*adhesion promoter diluted in a 91:9 IPA/water
cleaning solution has been found to be sufficient.
Suggested Sources for Silane Coupling Agents:
Custom-Pak Products, Inc. (262) 251-6180 available premixed in IPA/water
Lancaster Synthesis, Inc. (603) 889-3306 available 100% concentrated
*Note: Be sure to read and follow silane and solvent manufacturers precautions and directions
for use for proper handling and storage information.
Note: These primers contain greater than 250 g/l of volatile organic compounds (VOC). Please contact your local Air Quality Regulations
to be sure these primers are compliant.
(a)3M™ Scotch-Grip™ Plastic Adhesive 2262 contains 196 g/l VOC.
(b)See supplier information.
- 3 -
Surface Concern Suggested Primer Alternatives
Steel or Aluminum Surface must be clean None suggested Abrasion may clean surface, 3M™ Adhesion
Promoter 111 for increased adhesion.
Copper, Brass, Bronze Oxidation after bonding Lacquer or varnish(b) Architectural grade coatings
Concrete, Brick Non-unified or rough surface, 3M™ Rubber and Vinyl Spray 80 Concrete sealer, paint
moisture
Glass, Stone, Ceramic Tile High humidity, moisture 3M™ Silane Glass Treatment AP 115 or 3M™ Primer 94
similar silane coupling agent in IPA/water
mixture(b)
Wood (soft, hard Weak fiber layer on surface 3M™ Rubber and Vinyl Spray 80, Urethane paint, varnish
particle board, etc.) (e.g., low surface strength) 3M™ Fastbond™ 30 Contact Adhesive
Plastics: Polyolefin Low adhesion 3M™ Primer 94 (additional surface Flame treatment, Corona treatment
preparation may be required)
Non-olefin Additives, low adhesion 3M™ Primer 94, 3M™ Scotch-Grip™ Abrade or
Plastic Adhesive 2262(a) 3M™ VHB™ Tapes 4932/4952/5925/5952/5962
Polyurethane Mold release, low adhesion 3M™ Adhesion Promoter N-200J, Abrade and prime
(Molded or Rubber) 3M™ Scotch-Grip™ Plastic Adhesive 1099
Rubber: Neoprene, Santoprene Migrating oils 3M™ Primer 94, 3M™ Scotch-Grip™ 3M™ Weather Strip Tapes
Plastic Adhesive 1099
EPDM Low adhesion 3M™ Primer 94 3M™ Weather Strip Tapes
Paints Low adhesion 3M™ Adhesion Promoter 111 Abrade or
3M™ VHB™ Tapes 4932/4952/5925/5952/5962, or
3M™ Primer 94, 3M™ Scotch-Grip™ Plastic
Adhesive 2262(a), 3M™ Adhesion Promoter N-200J
Coil Coated Aluminum Low adhesion 3M™ Adhesion Promoter 111 Abrade or
3M™ VHB™ Tapes 4932/4952/5925/5952/5962, or
3M™ Primer 94, 3M™ Scotch-Grip™ Plastic
Adhesive 2262(a), 3M™ Adhesion Promoter N-200J
Flexible PVC (Vinyl) Plasticizer migration 3M™ Scotch-Grip Plastic Adhesive 2262(a), 3M™ VHB™ Tapes 4945 and 4941
3M™ Rubber and Vinyl Spray 80 (test for migration)
Technical Bulletin
Surface Preparation for 3MVHBTape Applications
Sources Hand held J-Roller:
Rockler Woodworking and Hardware
Phone: (800) 279-4441 Specify #39463
www.rockler.com
Scotch-Brite is a registered trademark of
3M Company.
3M, VHB and Scotch-Grip are trademarks
of 3M Company.
Printed in U.S.A.
©3M 2012 70070487015 (12/12)
Run an Evaluation Because 3M cannot anticipate all of the different possible surfaces and contaminants
that may exist, it is imperative that the user conduct an evaluation to determine the
suitability of 3M™ VHB™ Tapes, surface preparations procedures, and any other
processes that may have an influence on the tape or the bonded parts. Likewise,
where there are any changes in plastic or paint formulation, or suppliers of these
materials, it is advisable to run evaluations to ensure that the change has not
influenced the compatibility of the surface with 3M™ VHB™ Tapes.
- 4 -
3M warrants for 24 months from the date of manufacture that 3M™ VHB™ Tape will be free of defects
in material and manufacture. 3M MAKES NO OTHER WARRANTIES, EXPRESS OR IMPLIED,
INCLUDING BUT NOT LIMITED TO, ANY IMPLIED WARRANTY OF MERCHANTABILITY OR
FITNESS FOR A PARTICULAR PURPOSE. This limited warranty does not cover damage resulting
from the use or inability to use 3M™ VHB™ Tape due to misuse, workmanship in application, or
application or storage not in accordance with 3M recommended procedures. AN APPLICATION
WARRANTY EXPRESSLY APPROVED AND ISSUED BY 3M IS AN EXCEPTION. THE CUSTOMER
MUST APPLY FOR A SPECIFIC APPLICATION WARRANTY AND MEET ALL WARRANTY AND
PROCESS REQUIREMENTS TO OBTAIN AN APPLICATION WARRANTY. CONTACT 3M FOR MORE
INFORMATION ON APPLICATION WARRANTY TERMS AND CONDITIONS.
Limited Warranty
If the 3M™ VHB™ Tape is proved to be defective within the warranty period stated above. THE EXCLUSIVE
REMEDY, AT 3M’S OPTION, SHALL BE TO REFUND THE PURCHASE PRICE OF OR TO REPAIR OR
REPLACE THE DEFECTIVE 3M™ VHB™ TAPE. 3M shall not otherwise be liable for loss or damages,
whether direct, indirect, special, incidental, or consequential, regardless of the legal theory asserted,
including negligence, warranty, or strict liability.
Limitation of
Remedies and
Liability
The technical information, recommendations and other statements contained in this document are
based upon tests or experience that 3M believes are reliable, but the accuracy or completeness of such
information is not guaranteed.
Technical Information
Many factors beyond 3M’s control and uniquely within user’s knowledge and control can affect the use
and performance of a 3M product in a particular application. Given the variety of factors that can affect
the use and performance of a 3M product, user is solely responsible for evaluating the 3M product and
determining whether it is fit for a particular purpose and suitable for user’s method of application.
Product Use
This Industrial Adhesives and Tapes Division product was manufactured under a 3M quality system registered to ISO 9001 standards.
ISO 9001
Recycled Paper
40% pre-consumer
10% post-consumer
Industrial Adhesives and Tapes Division
3M Center, Building 225-3S-06
St. Paul, MN 55144-1000
800-362-3550 • 877-369-2923 (Fax)
www.3M.com/VHB

Products related to this Datasheet

TAPE DBL COATED GRAY 3/4"X 2"
Available Quantity: 3,554
Unit Price: 4.89
TAPE DBL COATED GRAY 1/2"X 5YDS
Available Quantity: 131
Unit Price: 47.01
TAPE DBL COATED GRAY 2"X 2"
Available Quantity: 113
Unit Price: 5.89
TAPE DBL COATED GRAY 12"X 12"
Available Quantity: 34
Unit Price: 58.29
TAPE DBL COATED GRAY 1"X 5YDS
Available Quantity: 28
Unit Price: 84.76
TAPE DBL COATED GRAY 1/2"X 5YDS
Available Quantity: 23
Unit Price: 52.1
TAPE DBL COATED GRAY 12"X 12"
Available Quantity: 21
Unit Price: 61.62
TAPE DBL COATED GRAY 1"X 5YDS
Available Quantity: 18
Unit Price: 92.65
TAPE DBL COATED GRAY 1/2"X 1/2"
Available Quantity: 17
Unit Price: 4.18
TAPE DBL COATED GRAY 3/4" DIA
Available Quantity: 5
Unit Price: 4.51
TAPE DBL COATED GRAY 1"X 5YDS
Available Quantity: 15
Unit Price: 87.85
TAPE DBL COATED GRAY 1"X 5YDS
Available Quantity: 15
Unit Price: 76.5
TAPE DBL COATED GRAY 1/2"X 5YDS
Available Quantity: 11
Unit Price: 54
TAPE DBL COATED GRAY 12"X 12"
Available Quantity: 7
Unit Price: 55.51
TAPE DBL COATED GRAY 3/4"X 3/4"
Available Quantity: 6
Unit Price: 4.51
TAPE DBL COATED GRAY 3/4"X 5YDS
Available Quantity: 5
Unit Price: 69.76
TAPE DBL COATED GRAY 2"X 5YDS
Available Quantity: 5
Unit Price: 129.55
TAPE DBL COATED GRAY 3/4"X 5YDS
Available Quantity: 4
Unit Price: 67.3
TAPE DBL COATED GRAY 3/4"X 4"
Available Quantity: 2
Unit Price: 5.94
TAPE DBL COATED GRAY 3/4"X 5YDS
Available Quantity: 2
Unit Price: 60.76
TAPE DBL COATED GRAY 2" DIA
Available Quantity: 1
Unit Price: 5.89
TAPE DBL COATED GRAY 2"X 5YDS
Available Quantity: 1
Unit Price: 148.85
TAPE DBL COATED GRAY 3"X 5YDS
Available Quantity: 1
Unit Price: 191.47
TAPE DBL COATED GRAY 3"X 5YDS
Available Quantity: 1
Unit Price: 172.76
TAPE DBL COATED GRAY 3/4"X 3"
Available Quantity: 0
Unit Price: 5.406
TAPE DBL COATED GRAY 3"X 5YDS
Available Quantity: 0
Unit Price: 198.43
TAPE DBL COATED GRAY 2"X 5YDS
Available Quantity: 0
Unit Price: 143.62
TAPE DBL COATED GRAY 6"X 5YDS
Available Quantity: 0
Unit Price: 192.36
TAPE DBL COATED CLEAR 6"X 5YDS
Available Quantity: 0
Unit Price: 250.59
TAPE DBL COATED CLEAR 6"X 5YDS
Available Quantity: 0
Unit Price: 272.29