TB-9043 Page 2 of 5 © 2015 DESCO INDUSTRIES, INC.
Employee Owned
SCS - 926 JR Industrial Drive, Sanford, NC 27332 • (919) 718-0000 • Website: StaticControl.com
Installation
The Benchtop Air Ionizer mounts easily in a variety of
positions using the provided tilting bracket/stand. Mount
the bracket by following the illustration below. Secure
the mounting bracket with screws on table top. Adjust
the angle of air flow towards the target and secure it by
tightening the side knobs.
Maintenance
1. When performing emitter points maintenance,
disconnect the Power Adapter AC plug from the
outlet. Do not connect or disconnect the power
plug with wet hands as doing so puts you at risk of
electrical shock or injury.
2. Occasional cleaning of the case is the only routine
maintenance required. Although the emitter points
have a built-in automatic cleaner, a check is still
necessary for any abnormality within the emitter
points. Verification and adjustment may be required
to keep the balance within the specification range.
3. Cleaning the Case - Wipe the case with a
moistened, fully squeezed soft cloth with deionized
water. If a stronger cleaning solution is required,
use a soft cloth with a mixture of alcohol and water
(70% IPA and 30% DI water). Do not use any other
solvents that can damage the coating of the case.
Fully squeeze the cloth or sponge to remove any
excess liquid.
4. Cleaning the Emitter Points - The emitter points and
auto-cleaning brushes are accessible through the
front grill. To clean them, turn off the unit; clean the
points and brushes with a cotton swab. Use caution
when accessing the emitter points to avoid injury.
Access to the points is available by removing two
tab screws on each side, pressing the side tabs,
and pulling off the grill (see images below). Use
caution when removing the grill to avoid breaking
the cable that connects the grill. Be careful not to
bend the emitter points during cleaning. The emitter
points are fixed and therefore not replaceable.
5. The safety switch functions to turn off the power
to the ionizer when the front grill is removed while
the ionizer is in operation. Before any maintenance
is performed on the emitter points and before
removing the front grill, ensure the unit is powered
off and the power cord is removed from the ionizer
or the wall outlet.
6. Re-attach the front grill after cleaning the emitter
points and fan blades. Replace the two tab screws
on each side of the grill.
7. Service - If you believe that a unit is not functioning
properly, disconnect the unit from power. If the unit
is covered by Warranty, contact your SCS sales
representative or distributor.
CAUTION: There are no user replaceable parts.
Unauthorized replacement of parts will void the
warranty.
Metal screw
4 x 20mm
1. Remove both side knobs one
at a time.
2. Mount the bracket using
three screws.
3. Replace the fan body. Tighten
both knobs to a desired air flow
abgle towards the target of
ionization.
1. Remove both side
knobs one at a time.
2. Mount the bracket
using three screws.
3. Replace the fan body. Tighten
both knobs to a desired air flow
angle towards the target of
ionization.
Metal screw
4mm x 20mm
Figure 5. Installing the Benchtop Air Ionizer
The safety of any system incorporating this equipment
is the responsibility of the assembler of the system. The
ionizer’s performance is affected by its distance from
the worksurface and fan speed. As distance increases
or fan speed is reduced, the discharge time at the work
surface will increase.
WARNING: The Benchtop Air Ionizer is not designed to
be used in explosive areas or flammable atmospheres.
Sparks from the fan motor or emitter points may cause
ignition.
Electrical
Use the included AC/DC power adapter. For proper
operation, the unit must be grounded for safe operation.
Grounding
The Benchtop Air Ionizer must be connected to ground
through the GROUND Terminal behind the unit and
the ground wire included in the package. Connect the
ground wire to a known good electrical ground. Failure
to connect the ground terminal may cause the unit to
malfunction.
Operation
1. Insert the AC/DC power adapter plug into an
electrical outlet. Make certain that power line
voltage is within the operating range of the AC/DC
power adapter. The use of improper power line
voltages may impair operation or damage the unit.
This will void the warranty.
2. The power switch on the front of the unit turns
the power and LED Power Indicator illuminates
when it’s on. The dial knob adjusts the fan speed.
Rotating it clockwise increases the fan speed.