3. Important Design Considerations
3.1 ON_OFF Signal
To conserve power, the Telit CE910-DUAL does not automatically start up when
power is applied. The baseboard design must supply a means to assert the
ON_OFF signal for the specified time (1 second < hold time < 2 seconds) to
start-up the module. To make module automatically start when power is applied,
tie ON/OFF signal to GND permanently. See Telit Hardware User Guide for
additional details regarding the ON_OFF signal.
3.2 Power Supply Requirements
The module will regularly consume high amounts of current on the Main Power
Supply (VCC), up to 750mA during active transmits and receives. The
baseboard power supply should be designed to support peak currents up to 1
Amp. A 100uF capacitor should be placed near the VCC pin on the module to
ensure ample energy is available, with a low inductance path to the VCC pin.
For example power supply designs, there are multiple references available. See
the NimbeLink Skywire Development Kit schematic for a switching regulator
example, or reference the Telit Hardware User Guide which has an example of
both Linear and Switching regulator designs.
3.3 Network Connection Status LED
The ON/nSLEEP signal on pin 13 drives the on-board LED indicating network
status. By default, the 1xRTT module has this setting disabled. Use the following
commands to enable and save this feature.
First, configure the GPIO for alternate function:
AT#GPIO = 1,0,2
The modem should respond with:
OK
Next, set the desired LED behavior with this command:
AT#SLED=2,10,10
The modem should respond with:
OK
Finally, commit the changes to non-volatile memory so the setting will persist
across power down/power up:
AT#SLEDSAV
The modem should respond with:
OK
PN 30003 rev 8© NimbeLink Corp. 2017. All rights reserved. 8