Eterna Integration Guide Datasheet by Analog Devices Inc.

View All Related Products | Download PDF Datasheet
dus-t?='==" networks m
Dust Networks
Eterna Integration Guide
2 ETERNA INTEGRATION GUIDE
Table of Contents
Design Process ......................................................................................................... 4
About This Guide ...................................................................................................... 5
Audience ................................................................................................................. 5
Related Documents .................................................................................................. 5
Conventions and Terminology.................................................................................... 5
Revision History ....................................................................................................... 5
General Design Guidelines........................................................................................ 7
Schematic Design ..................................................................................................... 7
Crystal Selection ...................................................................................................... 9
System Configuration ..............................................................................................10
PCB Layout .............................................................................................................10
Eterna QFN 72 Lead Recommended Land Pattern (QFN package QH072AF2A) ...........12
Stencil Design for Ground Paddle (QFN package QH072AF2A) ..................................14
EMI Considerations ..................................................................................................14
Antenna ESD Considerations ....................................................................................16
Supply Design .........................................................................................................16
Voltage Supervision and Reset .................................................................................16
Design for Manufacture ............................................................................................17
External Memory Support ....................................................................................... 18
Schematic Design ....................................................................................................18
Device Configuration ...............................................................................................21
List of Figures
Figure 1 Eterna Example Schematic .......................................................................... 7
Figure 2 Sample 20 MHz Crystal Routing ................................................................. 11
Figure 3 Triple 20 MHz crystal footprint with solder mask over pad ............................ 12
Figure 4 72 Lead QFN Land Pattern (QFN package QH072AF2A) ................................ 13
Figure 5 Ground Paddle Stencil ............................................................................... 14
Figure 6 Eterna Extended Memory Example Schematic (page 1 of 2) ......................... 19
Figure 7 Eterna Extended Memory Example Schematic (page 2 of 2) ......................... 20
ETERNA INTEGRATION GUIDE 3
List of Tables
Table 1 Sample BOM .................................................................................................. 8
Table 2 20 MHz Crystals ............................................................................................. 9
Table 3 32 kHz Crystals............................................................................................ 10
Table 4 Recommended Land Pattern Dimensions ........................................................ 13
Table 5 External Memory Reference Bill of Materials ................................................... 20
SmartMesh IP User Guide SmartMesh WirelessHART User Guide. www.dustcloud.org Fuse Table Etema Board Sgecific Configuration Guide M Etema Board 5 ecific Configgration Guide Eterna Serial Programmer Eterna Serial Programmer Guide, ETERNA RF Certification Users Guide BDSL ETERNA RF Certification Users Guide the regulation ETERNA2 RF Certification Users Guide E'I'ERNA2 Certification Package
4 ETERNA INTEGRATION GUIDE
Design Process
The design process when working with the LTC5800 based products is very similar
to the design process when working with an embedded microprocessor with some
significant and important differences covered in this section. The integration guide
focuses on the steps to design and manufacture LTC5800 based PCAs. Design of a
system solution should be completed with an understanding of the integration guide
and the network as described in either the SmartMesh IP User Guide or the
SmartMesh WirelessHART User Guide. In addition, if developing software on the
LTC5800-IPM, the software development process and API definitions are provided
on www.dustcloud.org.
After defining how the product(s) should operate in network and how the design will
be partitioned between hardware and software the design will typically take the
following steps:
1) Review the example schematic provided in this document to gain familiarity
with the required additional PCA components.
2) For customers developing software on the LTC5800-IPM, use the Fuse Table
application as described in the Eterna Board Specific Configuration Guide to
assign functions, such as SPI, I2C and GPIO to IOs.
3) Follow this document to complete the schematic design and layout.
4) Use the Fuse Table application as described in the Eterna Board Specific
Configuration Guide to create a fuse table for the design.
5) Use the Eterna Serial Programmer to load all of the required images onto the
LTC5800, the Fuse Table, Loader, Partition table and Image.
6) As described in the Eterna Serial Programmer Guide, characterize the 20MHz
crystal in the design. Update the Fuse Table with the new 20 MHz load trim
(ox13) value.
7) Develop and debug the design. Use the commands described in the ETERNA RF
Certification Users Guide, to perform out of network RF tests as needed.
8) Have the design pre-screened for RF certification on each revision of the PCB.
9) Develop production tests. The Eterna Serial Programmer is intended for loading
flash images in production. The LTC5800 BDSL file provides an efficient
method to test PCB interconnect.
10) The ETERNA RF Certification Users Guide provides a complete set of the
LTC5800 specific information and commands required to certify an LTC5800
based PCB worldwide. Certification can be a lengthy process requiring
significant supporting documentation from the manufacturer. Customers are
recommended to work with a certification agency familiar with the regulations
in the geography/geographies the design will be certified. The ETERNA2 RF
Certification Users Guide and the ETERNA2 Certification Package can be used
as an example for the radio specific documentation required for several
geographies, including: Canada, United States of America, the European
Economic Union, Japan, Taiwan, Korea, Australia, New Zealand and India.
Elerna Integration Guide 600* 0180 MASTER SCHEMATIC ETERNA MOTE EUPHRATESfldf 600* 01 80 MASTER SCHEMATIC ETERNA MOTE EUPHRATES.dSn 600* 0180 ETERNA MOTE EUPHRATES.QCb Elerna Boards 901' ('0 Con i uration Guide Elerna Serial Programmer Guide 60570211 MASTER SCHEMATI C ETERNA MEMORY REFERENCE ELWHA.pdf 60570211 MASTER SCHEMATIC ETERNA MEMORY REFERENCE ELWHA.dsn
ETERNA INTEGRATION GUIDE 5
About This Guide
This document provides the design guidelines essential for incorporating a
LTC5800-based design. The document covers design, layout, EMI, some device
configuration and manufacturing considerations.
Audience
This document is intended for system developers, hardware designers, and layout
engineers.
Related Documents
The following related documents are available:
Eterna Integration Guide (this guide)
600- 0180 MASTER_SCHEMATIC_ETERNA_MOTE_EUPHRATES.pdf
600- 0180 MASTER_SCHEMATIC_ETERNA_MOTE_EUPHRATES.dsn
600- 0180 ETERNA_MOTE_EUPHRATES.pcb
Eterna Board Specific Configuration Guide
Eterna Serial Programmer Guide
605-0211 MASTER_SCHEMATIC_ETERNA_MEMORY_REFERENCE_ELWHA.pdf
605-0211 MASTER_SCHEMATIC_ETERNA_MEMORY_REFERENCE_ELWHA.dsn
Conventions and Terminology
This guide uses the following text conventions:
Computer type indicates information that you enter, such as a URL.
Bold type indicates buttons, fields, and menu commands.
Italic type is used to introduce a new term.
Note: Notes provide more detailed information about concepts.
Caution: Cautions advise about actions that might result in loss of data.
Warning: Warnings advise about actions that might cause physical harm to the
hardware or your person.
Revision History
Revision
Date
Description
040-0102 rev 1
5/6/2011
Initial Release
040-0102 rev 2
11/8/2011
Added QH072F1A Land Pattern
Recommendations. Added Solder mask
over pad recommendations for the 20 MHz
xtal. Added recommendations for
QH072F1A paddle solder stencil design.
6 ETERNA INTEGRATION GUIDE
Corrected pin out for J3 Target SPI
programming header.
040-0102 rev 3
2/9/2012
040-0102 rev 4
7/18/2012
Added description for RF filtering options.
040-0102 rev 5
10/15/2012
Corrected BOM part number and value fields
for C6 and C16.
040-0102 rev 6
12/14/2012
Added support of external memory and
updated status of the crystal verification.
Added warning for the use of the Fractus
FR05-S1-N-0-102 chip antenna.
040-0102 rev 7
4/2/2013
Defined the differences between the -IPRA
and IPRB performance and configuration
requirements.
040-0102 rev 8
5/8/2013
Added hyperlinks to published references.
040-0102 rev 9
1/7/2015
Added design process section.
040-0102 rev 10
6/3/2015
Added additional qualified crystals.
sm w Manchu is w 5N1 4 man Jx Mmjx ‘vsUPpu PE‘MEJP nm‘plmn RAD‘O mm arr V” ‘ um u c M um u m w pwpw m aw: 2M w ; 57w 5: 1" 4; w 55 w 4A W m 2:31:41 m MW ~ m Mam mam" ”MW; 5er Mos‘ m n m we 4‘1“?“ m , , n W Mse m ‘ swy‘sn H mm ax umrcux 7 Wm 1x ascmmw m a 1-4 mm; W @m. ' use an mm P05 ssn 3 ‘ m WW4 5 ° 4% ' mlzqui w m 5:, 1.; i“ muv )a mnmm 3 V ‘wIs—L A m 5 ‘D‘ .. at My» 5 war-flu D k .m m vmefiw V
ETERNA INTEGRATION GUIDE 7
General Design Guidelines
Schematic Design
The schematic shown in Figure 1 includes all the external connections and
components necessary for the operation of a full-featured Eterna-based design.
Please use the corresponding Bill of Materials (BOM), see Table 1, as the definitive
reference for the part numbers and values.
Figure 1 Eterna Example Schematic
DigiKey LTC eCOM
8 ETERNA INTEGRATION GUIDE
The design includes power supply filtering via C23, C16, R14, and L1. The capacitor,
C16, must always be included and must be a ceramic type (X7R is recommended for
solutions requiring a wide temperature range and X5R otherwise) in order to
support the high frequency transient currents on the Eterna power supply. Note that
R14 is present to de-Q L1. The Eterna is most sensitive to supply noise in the 100 to
2000 kHz band. The included filter will reduce noise in the most sensitive band by
roughly an order of magnitude and is not required for all supply designs. However, it
is essential to meet the Eterna’s power supply requirements for maximum noise
considering both steady state operation and transient response.
An RF shield is typically required to obtain modular certification. However, it
provides minimal benefit in typical environments in providing isolation from RF and
magnetic fields. The RF shield matching the reference designs is available from
DigiKey and LTC eCOM (part number DUST-SHLD01).
Capacitors C6 through C13 and C16 through C21 are used for on chip regulation of
power supplies and should be placed as close as possible to their corresponding
package leads. These capacitors must be X7R. L2, C22 and C28 are placeholders for
a Pi matching network, where these components may be either capacitors or
inductors as dictated by the match required. The values in the BOM represent the
current matching required for a 50-Ohm load. Warning: C29, acting as DC
blocking capacitor is required to connect Eternas ANTENNA pin to a DC grounded
antenna or a DC grounded ¼ wave stub.
STUB1, connected to the RF path near the antenna connector is a ¼ wave, at 2.44
GHz, microstrip terminated to ground. The ¼ wave stub provides a notch filter at
the 2nd harmonic, enabling Eterna to easily meet world wide certification
requirements while only having slight impact on radio performance. The use of the
¼ wave stub significantly improves ESD performance while having near zero cost
and is the preferred approach to lowering the 2nd Harmonic emissions. It should be
expected to trim the layout of a ¼ wave stub in layout to center the notch of the ¼
wave stub. Using the Pi matching network will have a higher production cost and
lower ESD performance; however, the Pi matching network provides customers with
the ability to tune the filter without requiring a spin of the PCB. Warning: The
Fractus FR05-S1-N-0-102 chip antenna has demonstrated high gain lobes when
used in combination with a ¼ wave stub which may prevent a design from passing
radio certification. When using the Fractus FR05-S1-N-0-102, ESD the Pi-filter
comprising L2, C22 andC28 should be used. When using a ¼ wave stub designs
need not incorporate L2, C22 and C28; however, conservative practice would be to
include the layout supporting those components and loading L2 with a 100 pF
capacitor (this allows for matching and additional filtering should it be necessary).
Should layout considerations prevent the use of a ¼ wave stub, a low pass Pi-filter
comprised of L2, C22 and C28 may be used. Board stack up should be chosen such
that the trace width of the RF path, a 50 ohm impedance, is equal to or near the pad
side for the 0201 components.
Table 1 Sample BOM
Reference
Value
Vendor
R14
0
Yageo
R8
237
Vishay
C7, C8, C9, C10,
C11, C12, C17,
C18, C19, C20
56 nF
Kemet
C21
220 nF
Taiyo
Yuden
C22*, C28*
1 pF
Murata
Fuse Table agglication
ETERNA INTEGRATION GUIDE 9
Reference
Value
Vendor
C29
100 pF
Murata
C6,C16
100 nF
Murata
C23
2.2 µF
Murata
C13
470 nF
TDK
L1
2.2 µH
Murata
L2*
3.3 nH 0201 or
2.7 nH 0402
Coilcraft
Coilcraft
0402CS-2N7XJL
J1
JST
X1
32.768 kHz
ECS Inc.
X2
20.000 MHz
ECS Inc.
J2, J3
5x2 header
Molex
SH1
Fotofab
Note: * - these components are not needed if a ¼ stub is implemented.
Crystal Selection
The 20 MHz source (either X2, X4 or X5 on the schematic) is required for radio
operation. The 32 kHz source, either X1 or X3 on the schematic, is required for long
term precise timing. For mesh network applications, selection of crystal sources is
significant as Eterna mesh networks depend on maintaining timing more precise
than provided by the crystal accuracy itself. While alternate sources for the 20 MHz
and 32 kHz crystals may operate without issue, it is strongly recommended that
designs incorporate crystals from Table 2 and Table 3 below, such that the designs
will benefit from the verification performed against those crystals. Commonly
available crystals have failed Dust Networks qualification suite. Network
performance for unverified crystals can not be guaranteed.
Selection of a particular 20MHz crystal for use in a design should be matched by
selecting the same crystal in the Board Support Parameter “20 MHz xtal Part
Number” in the Fuse Table application. The ECS-200-CDX-0998 and the Kyocera
CX3225SB20000F0FZZC1 may be used interchangeably with a single Fuse Table
image.
Table 2 20 MHz Crystals
Vendor
Part Number
Form Factor
ECS
ECS-200-CDX-0998*
3.2x2.5x0.8mm, SMD
KYOCERA
CX3225SB20000F0FZZC1*
3.2x2.5x0.9mm, SMD
ECS
ECS-200-CDX-0778
2.5x2.0x0.55mm, SMD
ECS
ECS-200-CDX-0914
7.6x4.1x2.3mm, SMD
* These crystals are both footprint compatible and will work with a single Fuse Table
configuration. As a result one can be second sourced for the other.
2kB image via the Eterna Board Specific Con Emma Board S Jeci ic Con i uration Guide Eterna Serial Programmer Guide.
10 ETERNA INTEGRATION GUIDE
Table 3 32 kHz Crystals
Vendor
Part Number
Form Factor
ECS
ECS-.327-12.5-17X
8.7x3.7x2.5mm, SMD
Abracon
ABS07-32.768KHZ-4-T
3.2x1.5x0.9mm, SMD
ECS
ECS-.327-12.5-34B-TR
3.2x1.5x0.9mm, SMD
NDK
NX3215SA-32.768K-STD-MUA-8
3.2x1.5x0.9mm, SMD
System Configuration
Eterna supports hardware and software configuration of devices via two tables
stored in the first page of Eterna’s flash. These configurations are set by creating a
2kB image via the Eterna Board Specific Configuration application described in the
Eterna Board Specific Configuration Guide and written to Eterna’s flash via the
Eterna Serial Programmer described in the Eterna Serial Programmer Guide.
Eterna includes a hardware engine for configuring the device immediately on exit
from power-on reset and is the preferred method for configuring the
multifunction IO. Configuration controls include the mapping of pins to functions,
setting drive strength, IO direction, GPIO output value, pull enable, pull direction,
and input enable. In addition the Eterna’s Hardware lock key, a user defined key
that locks all external access (including debug access) to flash and RAM memory,
can be set via the Eterna Board Specific Configuration application. The Eterna
Board Specific Configuration application inherently provides an expedient method
to map out the functions assigned to Eternas multifunction IO, greatly reducing the
need to manually cross reference multiple tables in the product’s data sheet.
PCB Layout
Eterna-based designs should adhere to the following layout-sensitive guidelines:
1. The trace from the ANTENNA pin to the antenna connector should be 50-Ohm
characteristic impedance. Note that the drawn trace width will be a function of
the dielectric constant, height of the dielectric and the thickness of the plating.
For example, for an 8-mil FR4 substrate with 0.5 oz copper plating, the width
for a 50-Ohm trace is 14.5 mils. Keep all other active signals as far as possible
from this trace and at least five times the dielectric height to the RF ground
plane. No signals should be routed between this trace and its respective ground
plane.
2. The ground return for the ANTENNA pin is through the QFN paddle. The layout
should ensure that at least a 25 mils wide ground (and preferably as wide as
practically manageable) continues in a straight line through to the points where
the paddle is via stitched to ground.
3. Capacitors C6 through C13 and C16 through C21 should be placed no further
than 250 mils from their respective leads. All power supply traces for VSUPPLY,
VPRIME, VDDPA, VOSC, VCORE and VDDA should be a minimum of 25 mils
wide.
4. Noise from other digital signals can couple onto the 20 MHz crystal reference
and impair the radio performance. Traces from the 20 MHz crystal should be
routed on the same outside layer as the Eterna QFN, with no overlap from any
ETERNA INTEGRATION GUIDE 11
other signal, as shown in Figure 2. The adjacent layer on the PCB shall provide a
ground plane, isolating the crystal traces from other traces on the PCB. The
crystal leads and the corresponding traces should be surrounded by a co-planer
ground trace to reduce coupling onto the crystal pads and traces. If a shield is
present in the design the signals should rout through an opening in the exposed
metal trace described in the RF shield section below.
Figure 2 Sample 20 MHz Crystal Routing
5. Noise from other digital signals can couple onto the 32-kHz crystal reference
creating timing jitter for the low frequency clock. Traces from the 32 kHz crystal
should be routed on the same outside layer as the Eterna QFN, with no overlap
from any other signal. The adjacent layer on the PCB shall provide a ground
plane, isolating the crystal traces from other traces on the PCB. If a shield is
present in the design the signals should rout through an opening in the exposed
metal trace described in the RF shield section below.
6. In applications where EMI necessitates the inclusion of an RF shield, a thick
outside layer exposed metal trace, tapped to ground approximately every 100 to
250 mils, should encircle (save the path for the antenna and crystal signals) the
device. Determination for the size of the shield should account for the routing
challenges placed due to the limited area to create vias from the outside layer
with the QFN to other layers for routing. The shield will create a bounding box
on the outside with the QFN paddle will create an internal bounding box. Also,
consider the number of connections that should be as short as possible for the
required power supply components that should be placed near the QFN leads.
o 275 mm 02mm 55mm , 02mm. 4mm 600 0180 ETERNA MOTE EUPHRATES Cb 55mm, 135mm 0 275 mm
12 ETERNA INTEGRATION GUIDE
7. The recommended land pattern for the smaller footprint crystals, 3.2mm x
1.5mm, includes pads that are much wider than the crystal leads. Creating a
dual footprint for both the large and smaller form factor 20 MHz crystals further
enlarges the pad size. The large pad size can result in crystals drifting from their
placement during the reflow process. Reducing the pad size reduces a designs
robustness to vibration, which could be an important factor given the mass of
either the larger 20 MHz crystals. With the purpose of reducing the drift of the
crystal during the reflow process, it is recommended to include additional solder
mask over the pad as show in red in Figure 3.
Figure 3 Triple 20 MHz crystal footprint with solder mask over pad
An example layout corresponding to the provided example schematic, can be found
in 600- 0180 ETERNA_MOTE_EUPHRATES.pcb, a PADs formatted PCB file and
it’s corresponding gerber files.
Eterna QFN 72 Lead Recommended Land Pattern (QFN package QH072AF2A)
Two common practices for defining land patterns are Non Solder Mask Defined,
NSMD, and Solder Mask Defined, SMD. Given the lead pitch of the QH072AF2A
package and that tolerances for metal etch are commonly more precise than solder
mask deposition, the use of NSMD land patterns is recommended and documented
here. The solder mask opening should provide sufficient margin for registration
tolerance to avoid solder mask infringing on the pad, typically 60 to 75 um from the
edge of the pad and the solder mask. Note that the lead length for the corner
leads are shorter than the non-corner leads.
While Eterna does not require the ground paddle to dissipate significant thermal
energy, the paddle provides the RF return path and should both be low inductance
and provide a path near the ANTENNA pin for a return path. A pattern of 3 x 3 vias
separated over a 4.5 mm x 4.5 mm square is recommended. Vias should be plugged
with epoxy or tented to avoid solder wicking into the plated through holes,
potentially resulting in low package standoff height or secondary reflow on the
reverse side of the PCB.
H‘»
ETERNA INTEGRATION GUIDE 13
Land Pattern and Via placement dimensions are provided in Table 4 and illustrated
in Figure 4.
Table 4 Recommended Land Pattern Dimensions
Symbol
Description
Dimension (mm)
Min
Typ
Max
A
Lead land width
0.25
-
0.29
B
Lead land length
0.85
-
-
Corner Lead land length
0.75
-
-
C
Lead land pad inside dimension
8.70
8.80
Corner lead land pad inside
dimension
8.90
9.00
D
Lead land pad outside dimension
10.50
-
-
E
Ground paddle land width
6.15
-
-
F
Center first lead to package edge
-
0.75
-
G
Ground via spacing center to
center
-
4.5
-
E
E
D
D
C
F
F
A
B
G
G
Figure 4 72 Lead QFN Land Pattern (QFN package QH072AF2A)
14 ETERNA INTEGRATION GUIDE
Stencil Design for Ground Paddle (QFN package QH072AF2A)
As the Eterna (QH072AF2A QFN) includes a 6 x 6 mm ground paddle, appropriate
care should be taken in designing the solder stencil. Large apertures in the solder
stencil can lead to:
1) inadequate solder paste due to “scooping”
2) splatter and solder balling as a result of outgassing
3) increased standoff mismatch between leads on a QFN package
4) solder bridging
It is recommended to use smaller openings separated by at least 0.2 mm, with a
coverage of between 50 and 80%. An example of such a stencil with 1.6 mm
squares separated by 0.3 mm, providing 64% coverage is shown in Figure 5.
Figure 5 Ground Paddle Stencil
EMI Considerations
Like all radio devices, Eterna can be sensitive to EMI. In cases where the
deployment environment is known to have very low EMI, both in and out of band,
the RF shield may not be necessary. It should be noted; however, that for modular
radio certifications, regulatory bodies regularly require an RF shield. The following
considerations should be taken into account when selecting an RF shield for an
Eterna based design:
1. The RF shield should provide at least 0.5 mm (20 mils) clearance around the
Eterna package in the X and Y dimensions.
2. The RF shield should provide 1 mm (40 mils) of clearance above the top of the
PCB to the inside of the shield.
3. The RF shield should have a minimum of three asymmetric through hole pins.
In vibration intensive use cases, a minimum of four through hole pins should be
used and the RF shield should mate those pins to plated mounting holes and the
majority of the shield perimeter should be soldered to the PCB.
4. Ideally, the RF shield should allow for the smallest opening, but still greater
than 5 times the dielectric thickness between the antenna trace and the ground
plane from edge/top of the antenna trace to the nearest edge of the shield, for
ETERNA INTEGRATION GUIDE 15
the antenna signal to exit on the top layer of the PCB. This needs to be traded-off
against the cost of manufacture, including the ability to clean the PCB
underneath the shield.
5. In environments with high AC and DC magnetic fields, the use of a mu-metal
shield is recommended. Further, RF shield thickness is application dependent.
Consult your Linear FAE for support.
16 ETERNA INTEGRATION GUIDE
Antenna ESD Considerations
The antenna pin is a particularly sensitive node for electro-static discharge (ESD)
since it must detect small, high-frequency signals. ESD damage to the Eterna may
result in decreased receive or transmit performance, or other system failure. Many
applications for the Eterna have an exposed antenna that provides an entry point for
ESD events. Proper consideration of antenna design as well as antenna protection
can substantially improve ESD robustness in harsh environments.
A radome (protective covering) made of highly resistive material may be used to
prevent direct contact with the antenna and/or dissipate charge. To avoid ESD
events caused by triboelectric charging generated by wind passing over the antenna
in dry climates, the radome design should consider bulk and surface resistivity as
well as the size of the gap between the antenna metal and the interior of the radome.
In general, DC-grounded antennas (the antenna and ground have a DC short)
provide superior protection to ESD events. DC-grounded antennas are highly
recommended in harsh environments. Additionally, a DC path-to-earth ground
should be provided whenever possible to help bleed off accumulated charge from the
antenna as well as leak charge from the radome.
While these general guidelines should improve robustness to ESD events, individual
implementations may have unique factors that complicate ESD protection. Upon
request, your Linear FAE can provide contact information for an external consultant
able to perform a review for ESD and other system considerations.
Supply Design
Due to the heavy duty cycling, the Eternas current consumption can change
substantially over a short period. This does not represent an issue for systems with
supplies having low source impedance (less than 5 Ohms). Regulated supplies,
however, may have difficulty in the sudden changes in current consumption (more
than an order of magnitude in less than 1 µs), resulting in transient voltages on the
supply co-incident with the higher current consumption of the radio operation. To
ensure proper operation of the radio, a supply should be able to ramp from 250 µA
to 10 mA in less than 1 µs without generating a transient greater than 200 mV. For
systems with regulated supplies, consultation with your Linear Technology FAE is
strongly recommended.
The Eterna can be configured to support current limited supplies. Contact your
Linear FAE for details.
Voltage Supervision and Reset
The Eterna includes a power-on reset to safely set its own state during power up,
and includes a brown-out circuit that immediately halts flash erase cycles and
interrupts flash write cycles at the next 32-bit boundary, generating an interrupt to
the CPU and maintaining state for the CPU to correct should the power supply
return to normal operating levels. In the interest in avoiding flash corruption, it is
not considered best practice to connect the Eterna RESETn lead to a voltage
supervisor or to asynchronously assert RESETn without previously suspending
network and flash activity.
Elerna Serial Programmer Guide. Eterna Serial Programmer Guide here.
ETERNA INTEGRATION GUIDE 17
Design for Manufacture
The schematic shown in Figure 1 includes a header, J3, intended to provide an
interface to allow programming the Eterna. A mechanism to program the Eterna for
manufacturing is needed and prudent for design development. The header provides
connectivity through a cable to the DC9010 USB serial programmer described in the
Eterna Serial Programmer Guide. Software provided for controlling the
programmer allows users to program and verify pages in flash, and optionally the
entire flash contents. Note that the DC9010 programmer has a limited capability for
supplying current to the DUT see the Specifications section of the Eterna Serial
Programmer Guide for details. A BDSL file for the LTC5800 can be found here.
SmartMesh 1P Manager CLI Guide SmartMesh IP Manager API Guide.
18 ETERNA INTEGRATION GUIDE
External Memory Support
Without the addition of external SRAM, Eterna IP managers are limited to
supporting networks of 32 or fewer motes. External memory may be added to
Eterna IP Manager products to:
1) manage networks of up to 100 motes and / or
2) increase throughput of the manager from 24 to 36 packets per second
The LTC5800-IPRA is limited to supporting 32 motes with or without external
RAM; however, a license key can be purchased to raise the limit to 100 motes,
provided the external RAM is populated. To obtain a license key, a certificate must
first be purchased. Contact your Linear Sales representative for details on how to
order license key certificates. The certificate contains a product key and instructions
for requesting the generation of a license key, which typically takes one to two
business days to receive a license key. License keys are entered via either the set
config command documented in SmartMesh IP Manager CLI Guide or the
setLicense command documented in the SmartMesh IP Manager API Guide. The
LTC5800-IPRA by itself has a maximum sustained throughput of 24 packets per
second. The LTC5800-IPRB with external SRAM support has a maximum sustained
throughput of 36 packets per second.
The LTC5800-IPRB supports networks of up to 100 motes and has a maximum
throughput of 36 packets per second; however, external RAM must be provided.
Schematic Design
The schematic shown in Figure 6 and Figure 7 includes all the external connections
and components necessary to add the external RAM. The schematic differs from the
base schematic shown in Figure 1 in that:
1) CLI access is on UARTC1, not UARTC0
2) Mapping of external bus signals to Eterna’s general purpose function pins
3) The Memory, latches and pulse generators shown in Figure 7
The reference Bill of Materials (BOM) for the addition components needed for the
external memory interface is shown in Table 1. Common footprints exist for
128Kbyte, 256Kbyte and 512Kbyte RAMs. While the LTC5800-IPRB only requires
128Kbyte of RAM, it is recommended to include support for 256Kbyte and 512Kbyte
RAM variants in the layout, providing flexibility in using alternate equivalent
components during manufacture.
:5 m1 trace: for vsuppm, and vaussm} 22- : °‘ “3,! w {9 n I, , fix? §§ 1122.. m w .m... “Hi, 09*.“ m: « 35 5 § § E 5 ‘-* ** mu m um u m 5m sm-a M Egg 3; g .. m5“ mum 3 awn. '5 “E E E §§ g 5 olz‘Ju‘x 35.53;; m g: §5 i? g u wmwwalv : vw 5“" TflL way; 25:75:: ALE-“ii °° 5'" W 3:? m ‘ WZPAZM salsjosl Lm—U‘m‘ RX wT—aré'g—L “UL” 9'5 "'50 3—Way“ L—LPA my} an cw st- enjuu on w A w_u_u4 sm_ss_o.. m up PA 4;: 5m 55 1.. 46‘ , , on 5. ”“9” W vow m “‘5 fi‘ig a m % WEN” W was m RADDO TX" 4‘" Amm maznm 41 m m1 AL Jfl—w % “J : 1 u a “:2 47 L2 and C15 (Datpxlnts “snap. so am 11:: from ANTENNA ca .71 u“ .2 .m. m my mama — H W 73 Lou am a! .m, m m. - <7 m.="" '="" (a)="" fi="" ”b.”="" s"="" x,="" 1,...="" m="" m;="" a?“="" 1="" ‘="" .="" 1-="" “m”;="" $="" ‘="" mam-s="" a.="" a="" m="" mwaszumz="" ~—="" a:="" mm="" a...="" p.="" macaw="" .....="" «a="" m="" «an="" place="" all="" xml="" nets="" on="" top="" layer="" and="" guazd="" with="" ground="" tracks="" place="" tsmlnatian="" close="" to="" m="" fine="" 3.="" vex="">
ETERNA INTEGRATION GUIDE 19
Figure 6 Eterna Extended Memory Example Schematic (page 1 of 2)
2“ ml trace.) far VSUPPLLM , V5” ”W M >>vsumv_s m am. an w W eh m e wagon A [nuts W "LE-w eh m wen FILM—0'“ — way" an m m an m ‘32 621 m. vsuPPLv u2 must-.73 ozn \ cc Du on m 01 D2 02 m 03 m m as 05 as as m a7 am: LE am: 11 «2 a M 15 15 n w m MAHcsn nwomn OEn vcc Do an m m D: a2 m as m m as 05 us as m 07 cm: LE Gm) 222 mu Ewwmw u,- 3 us some mumesa vsumv M Note: yptess STSOP-:2 erA 1 15 at pm 9, 0: AN R5 mm am an 5150932 cvamsarvammszlxxw m on As no As can m um Win Ios Stuff it Ms I05 fcr 256mm "’ 3"” ‘5 A15 lo» 7 ucc I03 W vs: “a m .n m 2 AM Im m m A7 Al) A5 M A5 n M A3 :22 mu {5mm vsumv M ms um
20 ETERNA INTEGRATION GUIDE
Figure 7 Eterna Extended Memory Example Schematic (page 2 of 2)
Eterna’s External memory function has been tested with the BOM options shown in
Table 5. The RAM components shown have been selected for low power operation
and their use will result in an increase of a few uA of current consumption. For
designs that are not energy constrained, substitution of general purpose RAMs with
equal or faster speed grades should be possible. Substitution of the multi-function
logic and octal latch components should be done carefully to maintain the timing
generated by the pulse generation circuits.
Table 5 External Memory Reference Bill of Materials
Reference
Value
Vendor
Vendor P/N
R6,R7,R9
0
Panasonic
ERJ-1GE0R00C
R5
100 kOhm
Panasonic
ERJ-1GEJ104C
R8,R10
499 Ohm
Vishay
CRCW0201499RFKED
C25,C27
30 pF
Murata
GRM0335C1E300JD01D
C21,C22,C23,
C24,C26
100 nF
Murata
GRM155R71C104KA88D
a Board S )eci ('12 Con i m non Guide dash option / me Eterna Board Specific Configuration Guide,
ETERNA INTEGRATION GUIDE 21
Reference
Value
Vendor
Vendor P/N
U3
128K x 8-bit RAM
Cypress
CY62128EV30LL-45ZAXI
U3 Alternate
128K x 8-bit RAM
Renasas
R1LV0108ESA-5SI#B0
U5, U6
Multifunction
Logic
NXP
74AUP1G58GM, 132
U2, U4
Octal Latch
NXP
74AHC573BQ,115
logic and octal latch components should be done carefully to maintain the timing
generated by the pulse generation circuits.
logic and octal latch components should be done carefully to maintain the timing
generated by the pulse generation circuits.
Device Configuration
Per the Eterna Board Specific Configuration Guide, the LTC5800-IPRA or
LTC5800-IPRB must have both the IO configured and the board support parameters
set to function correctly. The IO is configured by enabling the “External Bus” check
box on the IO Configuration page. On the “Board Support Parameters” page the
“CLI Port Selection (0x03)” check box must be checked and the “UARTC1” option
must be set in the selection box. In addition, the “IP Manager Ext. Memory Size
(0x17)” check box must be checked and the appropriate LTC dash option / memory
foot print option must be set in the selection box. Please see the Eterna Board
Specific Configuration Guide, for complete details on all of the IO Configuration
settings and Board Support Parameters.
22 ETERNA INTEGRATION GUIDE
Trademarks
SmartMesh Industrial and Eterna are trademarks of Dust Networks, Inc. The Dust Networks logo, Dust, Dust Networks, and
SmartMesh are registered trademarks of Dust Networks, Inc. The Linear logo is a registered trademark of Linear Technology
Corporation. All third-party brand and product names are the trademarks of their respective owners and are used solely for
informational purposes.
ARM and Cortex are trademarks or registered trademarks of ARM Limited in the EU and other countries.
Copyright
This documentation is protected by United States and international copyright and other intellectual and industrial property laws.
It is solely owned by Dust Networks, Inc. and its licensors and is distributed under a restrictive license. This product, or any
portion thereof, may not be used, copied, modified, reverse assembled, reverse compiled, reverse engineered, distributed, or
redistributed in any form by any means without the prior written authorization of Dust Networks, Inc.
RESTRICTED RIGHTS: Use, duplication, or disclosure by the U.S. Government is subject to restrictions of FAR 52.227-14(g)
(2)(6/87) and FAR 52.227-19(6/87), or DFAR 252.227-7015 (b)(6/95) and DFAR 227.7202-3(a), and any and all similar and
successor legislation and regulation.
Disclaimer
This documentation is provided “as is” without warranty of any kind, either expressed or implied, including but not limited to,
the implied warranties of merchantability or fitness for a particular purpose.
This documentation might include technical inaccuracies or other errors. Corrections and improvements might be incorporated
in new versions of the documentation.
Dust Networks does not assume any liability arising out of the application or use of any products or services and specifically
disclaims any and all liability, including without limitation consequential or incidental damages.
Dust Networks products are not designed for use in life support appliances, devices, or other systems where malfunction can
reasonably be expected to result in significant personal injury to the user, or as a critical component in any life support d evice or
system whose failure to perform can be reasonably expected to cause the failure of the life support device or system, or to affect
its safety or effectiveness. Dust Networks customers using or selling these products for use in such applications do so at their
own risk and agree to fully indemnify and hold Dust Networks and its officers, employees, subsidiaries, affiliates, and
distributors harmless against all claims, costs, damages, and expenses, and reasonable attorney fees arising out of, directly or
indirectly, any claim of personal injury or death associated with such unintended or unauthorized use, even if such claim alleges
that Dust Networks was negligent regarding the design or manufacture of its products.
Dust Networks reserves the right to make corrections, modifications, enhancements, improvements, and other changes to its
products or services at any time and to discontinue any product or service without notice. Customers should obtain the latest
relevant information before placing orders and should verify that such information is current and complete. All products are sold
subject to Dust Network's terms and conditions of sale supplied at the time of order acknowledgment or sale.
Dust Networks does not warrant or represent that any license, either express or implied, is granted under any Dust Networks
patent right, copyright, mask work right, or other Dust Networks intellectual property right relating to any combination,
machine, or process in which Dust Networks products or services are used. Information published by Dust Networks regarding
third-party products or services does not constitute a license from Dust Networks to use such products or services or a warranty
or endorsement thereof. Use of such information may require a license from a third party under the patents or other intellectual
property of the third party, or a license from Dust Networks under the patents or other intellectual property of Dust Network s.
Dust Networks, Inc is a wholly owned subsidiary of Linear Technology Corporation.
© Dust Networks, Inc. 2012 through 2015. All Rights Reserved.
Document Number:
040-0102 Eterna Integration Guide
Last Revised:
June 11, 2015
Document Status
Product Status
Definition
Advanced Information
Planned or under
development
This document contains the design specifications for product development. Dust
Networks reserves the right to change specifications in any manner without notice.
Preliminary
Engineering samples
and pre-production
prototypes
This document contains preliminary data; supplementary data will be published at a
later date. Dust Networks reserves the right to make changes at any time without
notice in order to improve design and supply the best possible product. The
product is not fully qualified at this point.
No identification noted
Full Production
This document contains the final specifications. Dust Networks reserves the right to
make changes at any time without notice in order to improve design and supply the
best possible product.
Obsolete
Not in production
This document contains specifications for a product that has been discontinued by
Dust Networks. The document is printed for reference information only.
ETERNA INTEGRATION GUIDE 23

Products related to this Datasheet

SERIAL PROGRAMMER ETERNA
Available Quantity: 22
Unit Price: 716.22
IC RF TXRX+MCU 802.15.4 72VFQFN
Available Quantity: 0
Unit Price: 43.97
IC RF TXRX+MCU 802.15.4 72VFQFN
Available Quantity: 0
Unit Price: 125.2