USD

DM-25 Manual Datasheet by Greenlee Communications

View All Related Products | Download PDF Datasheet
INSTRUCTION MANUAL
MANUAL DE INSTRUCCIONES
MANUEL D’INSTRUCTIONS
BEDIENUNGSANLEITUNG
52059485 REV 1 © 2012 Greenlee Textron Inc. 1/12
Read and understand all of the instructions and safety information in
this manual before operating or servicing this tool.
Lea y entienda todas las instrucciones y la información sobre
seguridad que aparecen en este manual, antes de manejar estas
herramientas o darles mantenimiento.
Lire attentivement et bien comprendre toutes les instructions et
les informations sur la sécurité de ce manuel avant d’utiliser ou de
procéder à l’entretien de cet outil.
Vor Bedienung oder Wartung dieses Messgerätes bitte alle
Anweisungen und Sicherheitsinformationen in diesem Handbuch genau
durchlesen und beachten.
Register this product at www.greenlee.com / Registre este producto en
www.greenlee.com / Enregistrez votre produit en ligne, www.greenlee.com /
Dieses Produkt kann unter www.greenlee.com registriert werden
DM-25
Digital Multimeter
Multímetro digital
Multimètre numérique
Digital-Multimeter
Español.............17
Français ...........31
Deutsch ............ 45
D4
2
Description
The Greenlee DM-25 Digital Multimeter is a hand-held testing device with the
following measurement capabilities: AC and DC voltage, and resistance. This
meter also checks diodes, verifies continuity, and tests 1.5 V and 9 V batteries.
Safety
Safety is essential in the use and maintenance of Greenlee tools and equip-
ment. This instruction manual and any markings on the tool provide informa-
tion for avoiding hazards and unsafe practices related to the use of this tool.
Observe all of the safety information provided.
Purpose of This Manual
This instruction manual is intended to familiarize all personnel with the
safe operation and maintenance procedures for the Greenlee DM-25 Digital
Multimeter.
Keep this manual available to all personnel. Replacement manuals are avail-
able upon request at no charge at www.greenlee.com.
Do not discard this product or throw away!
For recycling information, go to www.greenlee.com.
All specifications are nominal and may change as design improvements occur.
Greenlee Textron Inc. shall not be liable for damages resulting from misapplication or
misuse of its products.
® Registered: The color green for electrical test instruments is a registered trademark of
Greenlee Textron Inc.
KEEP THIS MANUAL
A ADANGER AWARNING ACAUTION gig“ ‘ g“ §I AWARNING
DM-25
3
SAFETY ALERT SYMBOL
This symbol is used to call your attention to hazards or unsafe practices
which could result in an injury or property damage. The signal word,
defined below, indicates the severity of the hazard. The message after the
signal word provides information for preventing or avoiding the hazard.
Immediate hazards which, if not avoided, WILL result in severe injury or
death.
Hazards which, if not avoided, COULD result in severe injury or death.
Hazards or unsafe practices which, if not avoided, MAY result in injury or
property damage.
Read and understand this material before operating
or servicing this equipment. Failure to understand how
to safely operate this tool could result in an accident
causing serious injury or death.
Important Safety Information
© GREENLEE. AWARNING 2% AWARNING
4
Electric shock hazard:
Contact with live circuits could result in severe injury
or death.
Electric shock hazard:
•The test leads supplied with this product comply with IEC 61010-
031:2008, UL 61010-031:2010 and CAN/CSA-C22.2 NO. 61010-031A-
07–Amendment 1:2010. These safety standards limit the exposed length
of the probe tip to 4 mm for measurement category III. These test leads
include a cap that must be in place when used in measurement category
III applications.
•Do not apply more than the rated voltage between any two input termi-
nals, or between any input terminal and earth ground.
•Do not contact the test lead tips or any uninsulated portion of the
accessory.
Failure to observe these warnings could result in severe injury or death.
Important Safety Information
AWARNING AWARNING AWARNING
DM-25
5
Electric shock and fire hazard:
•Do not expose this unit to rain or moisture.
•Do not use the unit if it is wet or damaged.
•Inspect the test leads before use. They must be clean and dry, and the
insulation must be in good condition. Do not use the unit if the contrasting
inner layer of insulation is visible.
•Use this unit for the manufacturer’s intended purpose only, as described in
this manual. Any other use can impair the protection provided by the unit.
Failure to observe these warnings could result in severe injury or death.
Electric shock hazard:
•Do not operate with the case open.
•Before opening the case, remove the test leads from the circuit and shut
off the unit.
Failure to observe these warnings could result in severe injury or death.
Electric shock hazard:
•Unless measuring voltage, shut off and lock out power. Make sure that all
capacitors are discharged. Voltage must not be present.
•Set the selector and connect the test leads so that they correspond to the
intended measurement.
•Using this unit near equipment that generates electromagnetic interfer-
ence can result in unstable or inaccurate readings.
Failure to observe these warnings could result in severe injury or death.
Important Safety Information
© GREENLEE. ACAUTION ACAUTION
6
Important Safety Information
Electric shock hazard:
Do not change the measurement function while the test leads are connected
to a component or circuit.
Failure to observe this precaution may result in injury and can damage the
unit.
Electric shock hazard:
•Do not attempt to repair this unit. It contains no user-serviceable parts.
•Do not expose the unit to extremes in temperature or high humidity. Refer
to “Specifications.”
Failure to observe these precautions may result in injury and can damage
the unit.
Note: The test leads of this unit are not removable. Do not attempt to remove
them.
EB?
DM-25
7
Identification
Display Icons
4. HV 600 V AC or DC range selected
5. Polarity indicator
6. Low battery indicator
7. 1 Overload indicator
Symbols on the Unit
Warning—Read the instruction manual
Battery
Double insulation
1
2
3
4
5
6
7
1. LCD display
2. Selector to select a function or
turn power off
3. Permanently attached test
leads and probes
© GREENLEE. AWARNING chf:j Cg; @313 : J
8
Using the Test Leads
Electric shock hazard:
The test leads supplied with this product comply with IEC 61010-031:2008,
UL 61010-031:2010 and CAN/CSA-C22.2 NO. 61010-031A-07–Amendment
1:2010. These safety standards limit the exposed length of the probe tip to 4
mm for measurement category III. These test leads include a cap that must
be in place when used in measurement category III applications.
Failure to observe this warning could result in severe injury or death.
CAT II 600VCAT III 600V
CAT III 600V
Cap can be removed for measurement category I or II applications.
Cap must be in place for
measurement category III
applications.
AWARNING
DM-25
9
Operation
Electric shock hazard:
Contact with live circuits could result in severe injury
or death.
1. Refer to the Settings Table. Set the selector to the proper setting. Start with
the highest measurement range.
2. Refer to “Typical Measurements” for specific measurement instructions.
3. Test the unit on a known functioning circuit or component.
•If the unit does not function as expected on a known functioning circuit,
replace the battery.
•If the unit still does not function as expected, call Greenlee for technical
assistance at 800-435-0786.
4. Take the reading from the circuit or component to be tested. If the resolu-
tion is not satisfactory, remove the meter from the circuit and change to
the next lower range.
Settings Table
To measure this value: Set the selector to this symbol:
Continuity*
Diode
Resistance Ω
Battery Batt.
Voltage (DC)
Voltage (AC)
* Tone indicates continuity. The threshold is between 30 Ω and 100 Ω.
10
Typical Measurements
AC Voltage
Measurement
Resistance
Measurement
600
2000k
DM-25
11
Typical Measurements
Continuity Check
Diode
Measurement
200
2000
Reverse Bias
Forward Bias
Red Probe
12
Accuracy
Refer to the “Specifications” section for operating conditions and temperature
coefficient.
Accuracy is specified as follows: ± (a percentage of the reading + a fixed
amount) at 23 °C ± 5 °C (73.4 °F ± 9 °F), 0% to 75% relative humidity.
Accuracy is specified from 5% to 100% of the range unless noted otherwise.
AC Voltage
Range
(40 Hz to 400 Hz) Accuracy Input Impedance
200.0 V ± (1.2% + 1.0 V) 450 kΩ
600 V* ± (1.2% + 10 V)
* 600 V range is specified from 20% to 100% ofrange.
DC Voltage
Range Accuracy Input Impedance
20.00 V ± (0.8% + 0.05 V)
1 MΩ200.0 V ± (0.8% + 0.5 V)
600 V* ± (1.0% + 5 V)
* 600 V range is specified from 20% to 100% ofrange.
Resistance
Range Accuracy Open Circuit Voltage
200.0 Ω ± (1.2% + 0.5 Ω)
< 3 VDC
2000 Ω ± (1.0% + 5 Ω)
20.00 kΩ ± (1.0% + 0.05 kΩ)
200.0 kΩ ± (1.0% + 0.5 kΩ)
2000 kΩ ± (1.2% + 5 kΩ)
DM-25
13
Accuracy (con’t)
Battery Test
Test Current: Approximately 30 mA for 1.5 V, 8 mA for 9 V
Accuracy: ± (5% + 0.1 V)
Diode Test
Measuring Range: 2000 mV (on 2000 Ω setting)
Test Current (typical): 1.0 mA
Open Circuit Voltage (typical): < 3 V
Continuity
Tone Threshold: Between 30 Ω and 100 Ω
Specifications
Display: 3-1/2–digit LCD (1999 maximum count)
Polarity: Automatic
Sampling Rate: Approximately 2.5 per second
Temperature Coefficient: 0.2 x (accuracy) per °C below 18 °C or above 28 °C
Operating Conditions:
Temperature: 0 °C to 40 °C (32 °F to 104 °F)
Relative Humidity: 0% to 75%
Altitude: 2000 m (6500') maximum
Indoor use only
Pollution Degree: 2
Storage Conditions:
Temperature: –10 °C to 50 °C (14 °F to 122 °F)
Relative Humidity: 0% to 85%
Remove battery.
Battery: One 9 V battery (NEDA 1604, JIS 006P, or IEC 6F22)
Overload Protections: 600 VAC RMS and 600 VDC
Overvoltage Category: Category III 600 V
14
Measurement Categories
These definitions were derived from the international safety standard for
insulation coordination as it applies to measurement, control, and labora-
tory equipment. These measurement categories are explained in more detail
by the International Electrotechnical Commission; refer to either of their
publications: IEC 61010-1 or IEC 60664.
Measurement Category I
Signal level. Electronic and telecommunication equipment, or parts thereof.
Some examples include transient-protected electronic circuits inside photo-
copiers and modems.
Measurement Category II
Local level. Appliances, portable equipment, and the circuits they are plugged
into. Some examples include light fixtures, televisions, and long branch circuits.
Measurement Category III
Distribution level. Permanently installed machines and the circuits they are
hard-wired to. Some examples include conveyor systems and the main circuit
breaker panels of a building’s electrical system.
Measurement Category IV
Primary supply level. Overhead lines and other cable systems. Some examples
include cables, meters, transformers, and other exterior equipment owned by
the power utility.
Statement of Conformity
Greenlee Textron Inc. is certified in accordance with ISO 9001 (2000) for our
Quality Management Systems.
The instrument enclosed has been checked and/or calibrated using equipment
that is traceable to the National Institute for Standards and Technology (NIST).
AWARNING
DM-25
15
Maintenance
Electric shock hazard:
Before opening the case, remove the test leads from the circuit and shut off
the unit.
Failure to observe this warning could result in severe injury or death.
Battery
Cover
Battery
Replacing the Battery
1. Disconnect the unit
from the circuit. Turn
the unit OFF.
2. Remove the rubber
boot.
3. Remove the screw
from the battery cover.
4. Remove the battery
cover.
5. Replace the battery
(observe polarity).
6. Replace the battery
cover, screw, and
rubber boot.
Cleaning
Periodically wipe the case with a damp cloth and mild detergent; do not use
abrasives or solvents.
16
D4
DM-25
17
Descripción
El multímetro modelo DM-25 de Greenlee es una unidad de bolsillo que cabe
perfectamente en la palma de la mano y permite realizar los siguientes tipos
de mediciones: Tensión de CA y CC, y resistencia. Además, este multímetro
verifica diodos, continuidad y prueba baterías de 1,5 V y 9 V.
Acerca de la seguridad
Es fundamental observar métodos seguros al utilizar y dar mantenimiento a
las herramientas y equipo Greenlee. Este manual de instrucciones y todas las
marcas que ostenta la herramienta le ofrecen la información necesaria para
evitar riesgos y hábitos poco seguros relacionados con su uso. Siga toda la
información sobre seguridad que se proporciona.
Propósito de este manual
Este manual de instrucciones tiene como propósito familiarizar a todo el
personal con los procedimientos de operación y mantenimiento seguros para
el Multímetro digital modelo DM-25 de Greenlee.
Manténgalo siempre al alcance de todo el personal. Puede obtener copias
adicionales de manera gratuita, previa solicitud en www.greenlee.com.
¡No deseche ni descarte este producto!
Para información sobre reciclaje, visite www.greenlee.com.
Todas las especificaciones son nominales y pueden cambiar conforme tengan lugar
mejoras de diseño. Greenlee Textron Inc. no se hace responsable de los daños que puedan
surgir de la mala aplicación o mal uso de sus productos.
® Registrado: El color verde para instrumentos de verificación eléctricos es una marca
registrada de Greenlee Textron Inc.
CONSERVE ESTE MANUAL
APELIGRO AADVERTENCIA AATENCION HM“ AADVERTENCIA
18
SÍMBOLO DE ALERTA
SOBRE SEGURIDAD
Este símbolo se utiliza para indicar un riesgo o práctica poco segura que
podría ocasionar lesiones o daños materiales. Cada uno de los siguientes
términos denota la gravedad del riesgo. El mensaje que sigue a dichos
términos le indica cómo puede evitar o prevenir ese riesgo.
Peligros inmediatos que, de no evitarse, OCASIONARÁN graves lesiones o
incluso la muerte.
Peligros que, de no evitarse, PODRÍAN OCASIONAR graves lesiones o
incluso la muerte.
Peligro o prácticas peligrosas que, de no evitarse, PUEDEN OCASIONAR
lesiones o daños materiales.
Lea y entienda este documento antes de manejar
esta herramienta o darle mantenimiento. Utilizarla sin
comprender cómo manejarla de manera segura podría
ocasionar un accidente, y como resultado de éste,
graves lesiones o incluso la muerte.
Importante Información sobre Seguridad
AADVERTENCIA AADVERTENCIA
DM-25
19
Peligro de electrocución:
El contacto con circuitos activados podría ocasionar
graves lesiones o incluso la muerte.
Peligro de electrocución:
•Los cables de prueba suministrados con este producto cumplen con las
normativas IEC 61010-031:2008, UL 61010-031:2010 y CAN/CSA-C22.2
NO. 61010-031A-07–Enmienda 1:2010. Estas normativas de seguridad
limitan la longitud expuesta de la punta de la sonda a 4 mm para la
categoría de medición III. Estos cables de prueba incluyen una tapadera
que debe estar colocada en posición cuando se los utiliza en aplicaciones
con categoría de medición III.
•No aplique más de la tensión nominal entre dos terminales de entrada
cualesquiera, o entre un terminal de entrada cualquiera y una conexión a
tierra.
•No toque las puntas de los cables de prueba ni ninguna parte del
accesorio que carezca de forro aislante.
De no observarse estas advertencias podrían sufrirse lesiones graves o
incluso la muerte.
Importante Información sobre Seguridad
© GREENLEE. AADVERTENCIA AADVERTENCIA
20
Peligro de electrocución e incendio:
•No exponga esta unidad a la lluvia ni a la humedad.
•No utilice esta unidad si se encuentra mojada o dañada.
•Revise minuciosamente los cables de prueba, antes de utilizarlos.
Deberán estar limpios y secos, y su forro aislante deberá estar en buenas
condiciones. No use la unidad si es visible la capa de aislamiento interior
de contraste.
•Utilice la unidad únicamente para los fines que ha sido diseñada por el
fabricante, tal como se describe en este manual. Cualquier otro uso puede
menoscabar la protección proporcionada por la unidad.
De no observarse estas advertencias podrían sufrirse lesiones graves o
incluso la muerte.
Peligro de electrocución:
•A menos que vaya a medir tensión, apague y bloquee la energía.
Asegúrese que todos los condensadores estén totalmente sin carga. No
debe haber tensión alguna.
•Coloque el interruptor de selección y conecte los cables de prueba de
modo que correspondan al tipo de medición que se desea efectuar.
•Al utilizar esta unidad cerca de equipo que genere interferencia
electromagnética quizá se obtenga una lectura inexacta e inestable.
De no observarse estas advertencias podrían sufrirse lesiones graves o
incluso la muerte.
Importante Información sobre Seguridad
AADVERTENCIA AATENCION AATENCION
DM-25
21
Importante Información sobre Seguridad
Peligro de electrocución:
•No haga funcionar esta unidad con la caja abierta.
•Antes de abrir la caja, retire del circuito los cables de prueba y apague la
unidad.
De no observarse estas advertencias podrían sufrirse lesiones graves o
incluso la muerte.
Peligro de electrocución:
No cambie la función de medición mientras los cables de prueba estén
conectados a un componente o circuito.
De no observarse esta advertencia podrían sufrirse lesiones o daños a la
unidad.
Peligro de electrocución:
•No intente reparar esta unidad, ya que contiene partes que deben recibir
mantenimiento por parte de un profesional.
•No exponga la unidad a ambientes de temperatura extrema o altos niveles
de humedad. Consulte la sección “Especificaciones”.
De no observarse estas precauciones podrían sufrirse lesiones y daños a la
unidad.
Nota: Los cables de prueba de esta unidad no son removibles. No intente
retirarlos.
EB?
22
Identificación
Iconos de la pantalla
4. HV Escala de 600V CA o CC seleccionada
5. Indicador de polaridad
6. Indicador de batería baja
7. 1 Indicador de sobrecarga
Símbolos en la unidad
Advertencia — Lea el manual de instrucciones
Batería
Doble forro aislante
1
2
3
4
5
6
7
1. Pantalla de cristal líquido
2. Interruptor de selección para
seleccionar una función o
apagar (OFF) la unidad
3. Sondas y cables de prueba
permanentemente conectados
AADVERTENCIA cc] GETS
DM-25
23
Cómo utilizar los cables de prueba
Peligro de electrocución:
Los cables de prueba suministrados con este producto cumplen con las
normativas IEC 61010-031:2008, UL 61010-031:2010 y CAN/CSA-C22.2
NO. 61010-031A-07–Enmienda 1:2010. Estas normativas de seguridad
limitan la longitud expuesta de la punta de la sonda a 4 mm para la
categoría de medición III. Estos cables de prueba incluyen una tapadera que
debe estar colocada en posición cuando se los utiliza en aplicaciones con
categoría de medición III.
De no observarse esta advertencia podrían sufrirse lesiones graves o incluso
la muerte.
CAT II 600VCAT III 600V
CAT III 600V
Se puede retirar la tapadera para aplicaciones
con categoría de medición I o II.
La tapadera debe estar en
posición para aplicaciones
con categoría de medición III.
© GREENLEE. AADVERTENCIA 2%
24
Operación
Peligro de electrocución:
El contacto con circuitos activados podría ocasionar
graves lesiones o incluso la muerte.
1. Consulte la Tabla de ajustes. Coloque el interruptor de selección en el valor
adecuado. Empiece por la escala de medición más alta.
2. Consulte la sección “Mediciones más comunes” en relación con las
instrucciones específicas para cada tipo de medición.
3. Pruebe la unidad en un circuito o componente que se sabe está
funcionando perfectamente.
•Si la unidad no funciona como debería en un circuito que se sabe está
funcionando perfectamente, reemplace la batería.
•Si la unidad aún sigue sin funcionar como debería, llame a Greenlee al
800-435-0786 para obtener asistencia técnica.
4. Anote la lectura del circuito o componente que se está verificando. Si la
resolución de la lectura no es satisfactoria, desconecte el medidor del
circuito y cambie a la siguiente escala inferior.
Tabla de ajustes
Para medir este valor: Coloque el interruptor de selección
en este símbolo:
Continuidad*
Diodo
Resistencia Ω
Batería Batt.
Tensión (CC)
Tensión (CA)
* El tono es señal de continuidad. El umbral está entre 30 Ω y 100 Ω.
DM-25
25
Mediciones más comunes
Medición de
tensión de CA
Medición de
resistencia
600
2000k
26
Mediciones
más comunes
Verificación
de continuidad
Verificación
de diodo
200
2000
Sonda
roja
Polarización
inversa
Polarización
directa
DM-25
27
Precisión
Consulte la sección “Especificaciones” en relación con las condiciones de
operación y el coeficiente detemperatura.
La precisión se especifica de la siguiente manera: ± (un porcentaje de la
lectura + una cantidad fija) a23 °C ± 5 °C (73,4 °F ± 9 °F), 0% a 75% de
humedad relativa.
La precisión se especifica a partir de 5% hasta el 100% de la escala, a menos
que se indique algodiferente.
Tensión de CA
Escala
(40 Hz a 400 Hz) Precisión Impedancia de entrada
200,0 V ± (1,2% + 1,0 V) 450 kΩ
600 V* ± (1,2% + 10 V)
* La escala de 600 V se especifica del 20% al 100% de la escala.
Tensión de CC
Escala Precisión Impedancia de entrada
20,00 V ± (0,8% + 0,05 V)
1 MΩ200,0 V ± (0,8% + 0,5 V)
600 V* ± (1,0% + 5 V)
* La escala de 600 V se especifica del 20% al 100% de la escala.
Resistencia
Escala Precisión Tensión de circuito abierto
200,0 Ω ± (1,2% + 0,5 Ω)
< 3 VDC
2000 Ω ± (1,0% + 5 Ω)
20,00 kΩ ± (1,0% + 0,05 kΩ)
200,0 kΩ ± (1,0% + 0,5 kΩ)
2000 kΩ ± (1,2% + 5 kΩ)
28
Precisión (continuación)
Prueba de batería
Corriente de prueba: Aproximadamente 30 mA para 1,5 V; 8 mA para 9 V
Precisión: ± (5% + 0,1 V)
Verificación de diodos
Escala de medición: 2000 mV (en el ajuste de 2000 Ω)
Corriente de prueba (típica): 1,0 mA
Tensión de circuito abierto (típica): < 3 V
Continuidad
Umbral de tono: Entre 30 Ω y 100 Ω
Especificaciones
Pantalla: Pantalla de cristal líquido (LCD) de 3-1/2–dígitos
(resolución máxima de 1999 puntos)
Polaridad: Automática
Frecuencia de muestreo: Aproximadamente 2,5 por segundo
Coeficiente de temperatura: 0,2 x (precisión) por °C menor que 18 °C
o mayor que 28 °C
Condiciones de funcionamiento:
Temperatura: 0 °C a 40 °C (32 °F a 104 °F)
Humedad relativa: 0% a 75%
Altitud: 2000 m (6500 pies) máxima
Uso en interiores únicamente
Grado de contaminación: 2
Condiciones de almacenamiento:
Temperatura: –10 °C a 50 °C (14 °F a 122 °F)
Humedad relativa: 0% a 85%
Retire la batería.
Batería: Una batería de 9 voltios (NEDA 1604, JIS 006P o IEC 6F22)
Protecciones contra sobrecarga: 600 V CA RMS y 600 V CC
Categoría de sobretensión: Categoría III, 600 V
DM-25
29
Categorías de medición
Las siguientes definiciones proceden de la norma de seguridad internacional
sobre la coordinación de aislamientos tal y como se aplica a equipos de
medición, control y laboratorio. En las publicaciones IEC 61010-1 y IEC 60664
de la International Electrotechnical Commission (Comisión Electrotécnica
Internacional) se detallan más a fondo estas categorías de medición.
Categoría de medición I
Nivel de señal. Equipo electrónico y de telecomunicaciones, o partes del
mismo. Como ejemplo pueden citarse los circuitos electrónicos protegidos
contra tensiones momentáneas dentro de fotocopiadores y modems.
Categoría de medición II
Nivel local. Aparatos eléctricos, equipo portátil, y los circuitos a los que
están conectados. Como ejemplo pueden citarse dispositivos de iluminación,
televisores y circuitos de rama larga.
Categoría de medición III
Nivel de distribución. Máquinas instaladas permanentemente y los circuitos a
los que están cableados. Como ejemplo pueden citarse sistemas conductores
y los paneles del interruptor automático principal del sistema eléctrico de un
edificio.
Categoría de medición IV
Nivel de abastecimiento primario. Líneas aéreas y otros sistemas de cable.
Como ejemplo pueden citarse cables, medidores, transformadores y cualquier
otro equipo exterior perteneciente a la empresa de servicio eléctrico.
Certificado de Conformidad
Greenlee Textron Inc. cuenta con certificación conforme a ISO 9001 (2000)
para nuestros Sistemas de Gerencia de Calidad.
El instrumento provisto ha sido inspeccionado y/o calibrado mediante el uso de
equipo reconocido por el Instituto Nacional de Normas y Tecnologías (National
Institute for Standards and Technology [NIST]).
© GREENLEE. AADVERTENCIA
30
Mantenimiento
Peligro de electrocución:
Antes de abrir la caja, retire del circuito los cables de prueba y apague la
unidad.
De no observarse esta advertencia podrían sufrirse lesiones graves o incluso
la muerte.
Cómo reemplazar la batería
1. Desconecte la unidad
del circuito. Apague (OFF)
la unidad.
2. Retire la cubierta
de goma.
3. Retire el tornillo de la
tapa del compartimiento
de las baterías.
4. Retire la cubierta del
compartimiento de la batería.
5. Reemplace la batería
(observela polaridad).
6. Vuelva a colocar la cubierta
de la batería, el tornillo y la
cubierta de goma.
Limpieza
Limpie periódicamente la caja utilizando un paño húmedo y detergente suave;
no utilice abrasivos ni solventes.
Cubierta del
compartimiento
de la batería
Batería
D4
DM-25
31
Description
Le multimètre numérique DM-25 de Greenlee est un appareil de contrôle
portable offrant les capacités de mesure suivantes: tension alternative et
continue et résistance. Cet appareil permet également la vérification de diodes,
le contrôle de continuité et le contrôle de piles de 1,5 V et de 9 V.
Sécurité
Lors de l’utilisation et de l’entretien des outils et des équipements de Greenlee,
votre sécurité est une priorité. Ce manuel d’instructions et toute étiquette
sur l’outil fournit des informations permettant d’éviter des dangers ou des
manipulations dangereuses liées à l’utilisation de cet outil. Suivre toutes les
consignes de sécurité indiquées.
Objet de ce manuel
Ce manuel d’instructions a pour objet de familiariser tout le personnel avec
les procédures préconisées pour une utilisation et un entretien sans danger du
multimètre numérique DM-25 de Greenlee.
Mettre ce manuel à la disposition de tous les employés. On peut obtenir des
exemplaires gratuits sur simple demande sur le site Web www.greenlee.com.
Ne pas se débarrasser de ce produit ou le jeter !
Pour des informations sur le recyclage, visiter www.greenlee.com.
Toutes les spécifications sont nominales et peuvent changer avec l’amélioration de la
conception. Greenlee Textron Inc. ne peut être tenue responsable des dommages résultant
d’une application inappropriée ou d’un mauvais usage de ses produits.
® Déposé : La couleur verte des instruments de vérification électrique est une marque
déposée de Greenlee Textron Inc.
CONSERVER CE MANUEL
ADANGER AAVERTISSEMENT AATI'ENTION
32
SYMBOLE D’AVERTISSEMENT
Ce symbole met en garde contre les risques et les manipulations
dangereuses pouvant entraîner des blessures ou l’endommagement
du matériel. Le mot indicateur, défini ci-dessous, indique la gravité
du danger. Le message qui suit le mot indicateur indique comment
empêcher le danger.
Danger immédiat qui, s’il n’est pas pris en considération ENTRAINERA
des blessures graves, voire mortelles.
Danger qui, s’il n’est pas pris en considération, POURRAIT entraîner des
blessures graves, voire mortelles.
Dangers ou manipulations dangereuses qui, s’ils ne sont pas pris en
considération, POURRAIENT EVENTUELLEMENT entraîner des dommages
à la propriété ou causer des blessures.
Consignes de sécurité importantes
AAVERTISSEMENT AAVERTISSEMENT AAVERTISSEMENT
DM-25
33
Lire attentivement et bien comprendre cette
documentation avant d’utiliser ou de procéder à
l’entretien de cet équipement. Négliger de comprendre
comment utiliser cet outil en toute sécurité pourrait
provoquer un accident et entraîner des blessures
graves, voire mortelles.
Risque de décharge électrique :
Un contact avec des circuits sous tension pourrait
entraîner des blessures graves, voire mortelles.
Danger de choc électrique :
•Les fils de mesure fournis avec ce produit sont conformes à IEC 61010-
031:2008, UL 61010-031:2010 et CAN/CSA-C22.2 NO. 61010-031A-
07–Amendement 1:2010. Ces normes de sécurité limitent à 4 mm la
longueur d’embout de sonde exposée pour les mesures de catégorie III.
Ces fils de mesure comportent un capuchon qui doit être en place pour
effectuer des mesures de catégorie III.
•Ne pas appliquer plus que la tension nominale entre deux bornes d’entrée
ou entre une borne d’entrée et une prise de terre.
•Ne pas toucher les extrémités des fils d’essai ni aucune autre partie non
isolée de l’accessoire.
Le non-respect de ces mises en garde peut entraîner des blessures graves
ou la mort.
Consignes de sécurité importantes
© GREENLEE. AAVERTISSEMENT AAVERTISSEMENT
34
Danger de choc électrique et d’incendie :
•Ne pas exposer l’appareil à la pluie ou à l’humidité.
•Ne pas utiliser l’appareil s’il est mouillé ou endommagé.
•Vérifier les fils de mesure avant de les utiliser. Ils doivent être propres et
secs et l’isolation doit être en bon état. Ne pas utiliser l’appareil si la gaine
isolante intérieure de couleur contrastée est visible.
•Utiliser cet appareil exclusivement pour l’emploi prévu par le fabricant, tel
que décrit dans ce manuel. Toute autre utilisation peut compromettre la
protection offerte par l’appareil.
Le non-respect de ces mises en garde peut entraîner des blessures graves
ou la mort.
Danger de choc électrique :
•Couper et condamner l’alimentation du circuit contrôlé, sauf pour les
mesures de tension. Vérifier que tous les condensateurs sont déchargés. Il
ne doit y avoir aucune tension.
•Régler le sélecteur et raccorder les fils de mesure comme il se doit pour la
mesure à effectuer.
•L’utilisation de cet appareil à proximité de matériel émettant un brouillage
électromagnétique peut produire des mesures instables ou erronées.
Le non-respect de ces mises en garde peut entraîner des blessures graves
ou la mort.
Consignes de sécurité importantes
AAVERTISSEMENT AATTENTION AATTENTION
DM-25
35
Consignes de sécurité importantes
Danger de choc électrique :
•Ne pas utiliser avec le boîtier ouvert.
•Avant d’ouvrir le boîtier, retirer les fils d’essai du circuit et mettre l’appareil
hors tension.
Le non-respect de ces mises en garde peut entraîner des blessures graves
ou la mort.
Danger de choc électrique :
Ne pas changer de fonction de mesure alors que les fils de mesure sont
raccordés à un circuit ou composant.
Le non-respect de cette mise en garde peut entraîner des blessures et des
dommages de l’appareil.
Danger de choc électrique :
•Ne pas tenter de réparer cet appareil. Il ne contient aucune pièce
réparable par l’utilisateur.
•Ne pas exposer l’appareil à des températures extrêmes ou à une forte
humidité. Voir «Caractéristiques techniques».
Le non-respect de ces précautions peut entraîner des blessures et des
dommages de l’appareil.
Remarque: Les fils de mesure de cet appareil ne sont pas détachables. Ne
pas tenter de les débrancher.
EB?
36
Identification
Icônes de l’afficheur
4. HV Calibre 600 V alternatif ou continu sélectionné
5. Indicateur de polarité
6. Indicateur pile faible
7. 1 Indicateur de surcharge
Symboles apparaissant sur l’appareil
Avertissement — Lire le manuel d’instructions
Pile
Double isolation
1
2
3
4
5
6
7
1. Afficheur à cristaux liquides
(LCD)
2. Sélecteur de fonction et de
mise hors tension
3. Fils et sondes de mesure
non détachables
AAVERTISSEMENT
DM-25
37
Utilisation des fils de mesure
Danger de choc électrique :
Les fils de mesure fournis avec ce produit sont conformes à IEC 61010-
031:2008, UL 61010-031:2010 et CAN/CSA-C22.2 NO. 61010-031A-07–
Amendement 1:2010. Ces normes de sécurité limitent à 4 mm la longueur
d’embout de sonde exposée pour les mesures de catégorie III. Ces fils de
mesure comportent un capuchon qui doit être en place pour effectuer des
mesures de catégorie III.
Le non-respect de cette mise en garde peut entraîner des blessures graves
ou la mort.
CAT II 600VCAT III 600V
CAT III 600V
Le capuchon peut être retiré pour les mesures de catégorie I ou II.
Le capuchon doit être en
place pour effectuer des
mesures de catégorie III.
© GREENLEE. 2% AAVERTISSEMENT
38
Utilisation
Risque de décharge électrique :
Un contact avec des circuits sous tension pourrait
entraîner des blessures graves, voire mortelles.
1. Se reporter au Tableau des réglages. Placer le sélecteur sur le réglage qui
convient. Commencer par le calibre de mesure le plus élevé.
2. Voir les instructions de mesure particulières sous «Mesures types».
3. Tester l’appareil sur un circuit ou un composant connu.
•Si l’appareil ne fonctionne pas comme prévu sur un circuit opérationnel
connu, changer la pile.
•Si l’appareil ne fonctionne toujours pas comme prévu, appeler le service
d’assistance technique de Greenlee au 800-435-0786.
4. Effectuer la mesure sur le circuit ou le composant à contrôler. Si la
résolution n’est pas satisfaisante, débrancher l’appareil du circuit et le
régler sur le calibre inférieur suivant.
Tableau des réglages
Pour mesurer cette valeur: Régler le sélecteur sur ce symbole:
Continuité*
Diode
Résistance Ω
Pile Batt.
Tension (continue)
Tension (alternative)
* La tonalité indique la continuité. Le seuil se situe entre 30 Ω et 100 Ω.
DM-25
39
Mesures types
Mesure
de tension
alternative
Mesure de
résistance
600
2000k
40
Mesures types
Contrôle de
continuité
Mesure de diode
200
2000
Sonde
rouge
Polarisation
inverse
Polarisation
directe
DM-25
41
Précision
Voir les conditions d’utilisation et le coefficient de température dans la section
« Caractéristiques techniques».
La précision est spécifiée comme suit: ± (un pourcentage de la mesure + une
quantité fixe) à 23 °C ± 5 °C (73,4 °F ± 9 ºF), 0% à 75% d’humidité relative.
La précision concerne une plage de 5% à 100% du calibre, sauf indication
contraire.
Tension alternative
Calibre
(40 Hz à 400 Hz) Précision Impédance d’entrée
200,0 V ± (1,2 % + 1,0 V) 450 kΩ
600 V* ± (1,2 % + 10 V)
* La précision du calibre 600 V est valable sur 20% à 100% du calibre.
Tension continue
Calibre Précision Impédance d’entrée
20,00 V ± (0,8 % + 0,05 V)
1 MΩ200,0 V ± (0,8 % + 0,5 V)
600 V* ± (1,0 % + 5 V)
* La précision du calibre 600 V est valable sur 20% à 100% du calibre.
Résistance
Calibre Précision Tension en circuit ouvert
200,0 Ω ± (1,2 % + 0,5 Ω)
< 3 VDC
2000 Ω ± (1,0 % + 5 Ω)
20,00 kΩ ± (1,0 % + 0,05 kΩ)
200,0 kΩ ± (1,0 % + 0,5 kΩ)
2000 kΩ ± (1,2 % + 5 kΩ)
42
Précision (suite)
Contrôle des piles
Intensité de contrôle: environ 30 mA pour 1,5 V, 8 mA pour 9 V
Précision: ± (5% + 0,1 V)
Contrôle de diode
Calibre de mesure: 2000 mV (sur réglage de 2000 Ω)
Intensité de contrôle (type): 1,0 mA
Tension en circuit ouvert (type): < 3 V
Continuité
Seuil de tonalité: Entre 30 Ω et 100 Ω
Caractéristiques techniques
Afficheur: Cristaux liquides (LCD) de 3 chiffres et 1/2 (valeur maximale 1999)
Polarité: Automatique
Fréquence d’échantillonnage: 2,5 fois par seconde environ
Coefficient de température: 0,2 x (précision) par °C en dessous
de 18 °C ou au-dessus de 28 °C
Conditions d’utilisation:
Température: 0 °C à 40 °C (32 °F à 104 °F)
Humidité relative: 0% à 75%
Altitude: 2000 m au maximum
Utilisation à l’intérieur uniquement
Degré de pollution: 2
Conditions d’entreposage:
Température: –10 °C à 50 °C (–14 °F à 122 °F)
Humidité relative: 0% à 85%
Enlever la pile.
Pile: Une pile de 9 V (NEDA 1604, JIS 006P ou IEC 6F22)
Protections antisurcharge: 600 VAC eff. et 600 VDC
Catégorie de surtension: Catégorie III 600 V
DM-25
43
Catégories de mesure
Ces définitions sont dérivées des normes internationales sur la sécurité pour la
coordination de l’isolation telle qu’elle s’applique à la mesure, au contrôle et à
l’équipement de laboratoire. Ces catégories de mesure sont expliquées plus en
détail par la Commission électrotechnique internationale ; se reporter à l’une
de ces deux publications : IEC 61010-1 ou IEC 60664.
Catégorie de mesure I
Niveau de signal. Pièces ou équipement électronique et de télécommunication.
Par exemple, les circuits électroniques protégés contre les courants
transitoires, dans les photocopieurs et les modems.
Catégorie de mesure II
Niveau local. Appareils, équipement portatif et les circuits dans lesquels ils
sont branchés. Par exemple, les appareils d’éclairage, les téléviseurs et les
dérivations.
Catégorie de mesure III
Niveau de distribution. Les machines installées en permanence et les circuits
auxquels elles sont câblées. Par exemple, les systèmes de convoyeurs et les
panneaux de disjoncteurs principaux du système électrique d’un édifice.
Catégorie de mesure IV
Niveau d’alimentation principal. Lignes surélevées et autres systèmes de
câbles. Par exemple, les câbles, les compteurs, les transformateurs et autres
équipements extérieurs appartenant aux fournisseurs en électricité.
Déclaration de conformité
Greenlee Textron Inc. est certifiée selon ISO 9001 (2000) pour nos Systèmes de
gestion de la qualité.
L’instrument ci-inclus a été vérifié et/ou étalonné avec des moyens de mesure
raccordés aux étalons du National Institute of Standards and Technology (NIST).
© GREENLEE. AAVERTISSEMENT
44
Entretien
Danger de choc électrique :
Avant d’ouvrir le boîtier, retirer les fils d’essai du circuit et mettre l’appareil
hors tension.
Le non-respect de cette mise en garde peut entraîner des blessures graves
ou la mort.
Changer la pile
1. Débrancher l’appareil du
circuit. Mettre l’appareil
hors tension (OFF).
2. Ôter la gaine en
caoutchouc.
3. Enlever la vis
du couvercle du
compartiment de pile.
4. Retirer le couvercle du
compartiment de pile.
5. Changer la pile
(respecter la polarité).
6. Remettre le couvercle,
la vis et la gaine en
caoutchouc en place.
Nettoyage
Nettoyer régulièrement le boîtier avec un chiffon humide et un détergent doux.
Ne pas utiliser de produits abrasifs ou de solvants.
Couvercle du
compartiment
de pile
Pile
D4
DM-25
45
Beschreibung
Das Digital-Multimeter DM-25 von Greenlee ist ein tragbares Testgerät
mit folgenden Messmöglichkeiten: Wechsel- und Gleichspannung sowie
Widerstand. Darüber hinaus kann dieses Messgerät auch zum Testen von
Dioden, zur Durchgangsprüfung und zum Testen von Batterien mit einer
Spannung von 1,5V und 9 V eingesetzt werden.
Sicherheitsvorkehrungen
Sicherheitsvorkehrungen sind bei der Verwendung und der Wartung der
Geräte und Ausrüstung von Greenlee entscheidend. Die vorliegende Anleitung
und etwaige am Gerät angebrachte Beschriftungen geben Hinweise zur
Vermeidung von Gefahren und gefährlichen Praktiken in Bezug auf die
Handhabung dieses Geräts. Bitte alle hier angegebenen Sicherheitshinweise
beachten.
Zweck dieses Handbuchs
Dieses Handbuch dient dazu, das Personal mit den sicheren Betriebs- und
Wartungsverfahren für das Digital-Multimeter DM-25 von Greenlee vertraut zu
machen.
Bitte dieses Handbuch allen Mitarbeitern zugänglich machen. Ersatz-
Handbücher sind auf Anfrage kostenlos erhältlich unter www.greenlee.com.
Dieses Produkt nicht wegwerfen.
Recycling-Informationen sind unter www.greenlee.com nachzulesen.
Alle technischen Daten sind Nennwerte. Bei Designverbesserungen sind Änderungen der
Nennwerte vorbehalten. Greenlee Textron Inc. haftet nicht für Schäden, die sich aus der
falschen Anwendung oder dem Missbrauch seiner Produkte ergeben.
® eingetragen: Die Farbe Grün für elektrische Testgeräte ist eine eingetragene Marke von
Greenlee Textron Inc.
DIESES HANDBUCH UNBEDINGT AUFBEWAHREN
AGEFAHR AWARNUNG AVORSICHT AWARNUNG gig“
46
SICHERHEITS-WARNSYMBOL
Dieses Symbol macht auf gefährliche oder riskante Praktiken
aufmerksam, die zu Schäden oder Verletzungen führen können.
DasSignalwort, wie nachfolgend definiert, gibt den Schweregrad der
Gefahr an. Der dem Signalwort folgende Hinweis informiert darüber, wie
die Gefahr verhindert oder vermieden wird.
Akute Gefahr, die bei Nichtvermeiden zu schweren Verletzungen oder
zum Tod FÜHRT.
Gefahr, die bei Nichtvermeiden zu schweren Verletzungen oder zum Tod
führen KANN.
Gefahr oder unsichere Praktiken, die bei Nichtvermeiden zu Verletzungen
oder Sachschäden führen KÖNNEN.
Vor Betrieb oder Wartung dieses Geräts die
Bedienungsanleitung sorgfältig durchlesen und
beachten. Mangelndes Verständnis der sicheren
Betriebsweise dieses Geräts kann zu Unfällen mit
schweren oder tödlichen Verletzungen führen.
Wichtige Sicherheitshinweise
AWARNUNG AWARNUNG
DM-25
47
Stromschlaggefahr:
Das Berühren von Stromkreisen kann zu schweren
Verletzungen oder zum Tod führen.
Stromschlaggefahr:
•Die im Lieferumfang dieses Produkts enthaltenen Messleitungen
entsprechen IEC 61010-031:2008, UL 61010-031:2010 und
CAN/CSA-C22.2 NO. 61010-031A-07–Ergänzung 1:2010. Diese
Sicherheitsstandards beschränken die freiliegende Länge der
Sondenspitze für die Messkategorie III auf 4 mm. Zu diesen Messleitungen
gehört eine Kappe, die für Anwendungen der Messkategorie III aufgesetzt
sein muss.
•Zwischen zwei Eingangsanschlüssen bzw. einem Eingangsanschluss und
der Erdung nicht mehr als die Nennspannung anlegen.
•Die Enden der Messleitungen oder die nicht isolierten Teile des
Zubehörteils dürfen nicht berührt werden.
Das Nichtbeachten dieser Warnungen könnte zu schweren oder tödlichen
Verletzungen führen.
Wichtige Sicherheitshinweise
Hinweis: Die Messleitungen dieses Geräts können nicht abgenommen
werden. Es darf kein Versuch unternommen werden, sie abzunehmen.
© GREENLEE. AWARNUNG AWARNUNG
48
Stromschlag- und Brandgefahr:
•Dieses Gerät darf weder Regen noch Feuchtigkeit ausgesetzt werden.
•Das Gerät nicht benutzen, wenn es nass oder beschädigt ist.
•Vor dem Einsatz die Messleitungen oder Zubehörteile überprüfen. Sie
müssen sauber und trocken und die Isolation muss in einem guten
Zustand sein. Das Gerät nicht verwenden, wenn die kontrastierende innere
Isolierung sichtbar ist.
•Dieses Gerät darf nur zu seinem vom Hersteller bestimmten Zweck, wie
in dieser Anleitung beschrieben, verwendet werden. Davon abweichende
Verwendungszwecke beeinträchtigen u. U. den vom Gerät gebotenen
Schutz.
Das Nichtbeachten dieser Warnungen könnte zu schweren oder tödlichen
Verletzungen führen.
Stromschlaggefahr:
•Das Gerät nicht mit offenem Gehäuse betreiben.
•Vor dem Öffnen des Gehäuses die Messleitungen vom Stromkreis
entfernen und das Gerät ausschalten.
Das Nichtbeachten dieser Warnungen könnte zu schweren oder tödlichen
Verletzungen führen.
Wichtige Sicherheitshinweise
AWARNUNG AVORSICHT AVORSICHT
DM-25
49
Wichtige Sicherheitshinweise
Stromschlaggefahr:
•Das Gerät ausschalten und die Stromzufuhr blockieren, wenn es nicht
zur Messung der Spannung eingesetzt wird. Darauf achten, dass alle
Kondensatoren entladen sind. Es darf keine elektrische Spannung
vorhanden sein.
•Den Wahlschalter gemäß der vorzunehmenden Messung einstellen und die
Messleitungen entsprechend anschließen.
•Die Verwendung dieses Geräts in der Nähe von Anlagen, die
elektromagnetische Störungen hervorrufen, kann zu instabilen bzw.
ungenauen Messwerten führen.
Das Nichtbeachten dieser Warnungen könnte zu schweren oder tödlichen
Verletzungen führen.
Stromschlaggefahr:
Bei an einer Komponente oder einem Stromkreis angeschlossenen
Messleitungen darf die Messfunktion nicht geändert werden.
Nichtbeachten dieser Sicherheitsvorkehrungen kann zu Verletzungen oder
Schäden am Gerät führen.
Stromschlaggefahr:
•An diesem Gerät keine Reparaturen vornehmen. Es enthält keine Teile, die
vom Benutzer gewartet werden können.
•Das Gerät keinen extremen Temperaturen oder hoher Luftfeuchtigkeit
aussetzen. Weitere Hinweise sind unter „Technische Daten“ zu finden.
Nichtbeachten dieser Sicherheitsvorkehrungen kann zu Verletzungen oder
Schäden am Gerät führen.
EB?
50
Bezeichnungen
Anzeigesymbole
4. HV Gewählter 600 V AC oder DC Bereich
5. Polaritätsanzeige
6. Anzeige „Niedriger Batteriestand“
7. 1 Überlastanzeige
Symbole am Gerät
Warnhinweis – Bedienungsanleitung lesen
Batterie
Doppelisolierung
1
2
3
4
5
6
7
1. LCD-Anzeige
2. Wahlschalter zur Auswahl
einer Funktion oder zum
Ausschalten des Geräts
3. Fest angeschlossene
Messleitungen und Messfühler
AWARNUNG Eij:j :(Cj azL:11iT:J
DM-25
51
Verwendung der Messleitungen
Stromschlaggefahr:
Die im Lieferumfang dieses Produkts enthaltenen Messleitungen
entsprechen IEC 61010-031:2008, UL 61010-031:2010 und CAN/CSA-
C22.2 NO. 61010-031A-07–Ergänzung 1:2010. Diese Sicherheitsstandards
beschränken die freiliegende Länge der Sondenspitze für die Messkategorie
III auf 4 mm. Zu diesen Messleitungen gehört eine Kappe, die für
Anwendungen der Messkategorie III aufgesetzt sein muss.
Das Nichtbeachten dieser Warnung kann zu schweren oder tödlichen
Verletzungen führen.
CAT II 600VCAT III 600V
CAT III 600V
Für Anwendungen der Messkategorie I oder II
kann sie jedoch abgenommen werden.
Für Anwendungen der
Messkategorie III muss
die Kappe aufgesetzt sein.
© GREENLEE. AWARNUNG 2%
52
Bedienung
Stromschlaggefahr:
Das Berühren von Stromkreisen kann zu schweren
Verletzungen oder zum Tod führen.
1. Siehe „Tabelle der Einstellungen“ Den Wahlschalter auf die korrekte
Einstellung einstellen. Zuerst den höchsten Messbereich messen.
2. Siehe „Typische Messungen“ für spezifische Messanleitungen.
3. Das Gerät an einem funktionierenden Stromkreis oder einer
funktionsfähigen Komponente testen.
•Wenn das Messgerät an einem funktionierenden Stromkreis nicht wie
erwartet funktioniert, die Batterie austauschen.
•Wenn das Messgerät anschließend immer noch nicht wie erwartet
funktioniert, unter der Rufnummer 800-435-0786 Kontakt mit dem
technischen Kundendienst von Greenlee aufnehmen.
4. Den Messwert von dem zu testenden Stromkreis oder der zu testenden
Komponente ablesen. Wenn die Auflösung nicht zufrieden stellend ist, das
Messgerät vom Stromkreis trennen und zum nächstniedrigeren Bereich
wechseln.
Tabelle der Einstellungen
Zur Messung von: Den Wahlschalter auf dieses Symbol stellen:
Durchgang*
Diode
Widerstand Ω
Batterie Batt.
Spannung (Gleichspannung)
Spannung (Wechselspannung)
* Das akustische Signal weist darauf hin, dass Stromdurchgang vorhanden
ist. Der Schwellenwert liegt zwischen 30 Ω und 100 Ω.
DM-25
53
Typische Messungen
Wechselspannungsmessung
Widerstandsmessung
600
2000k
54
Typische Messungen
Durchgangsprüfung
Diodenmessung
200
2000
Roter
Messfühler
Sperrvorspannung
Durchlassspannung
DM-25
55
Messgenauigkeit
Informationen zu den Betriebsbedingungen und zum Temperaturkoeffizienten
sind im Abschnitt „Technische Daten“ zu finden.
Die Messgenauigkeit ist wie folgt angegeben: ± (Prozentanteil des Messwerts
+ ein fester Wert) bei 23 °C ± 5 °C (73,4 °F ± 9 °F), 0 % bis 75 % relative
Luftfeuchtigkeit.
Die Messgenauigkeit ist zuverlässig im Bereich zwischen 5 % und 100 %, falls
nicht anderweitig ausgewiesen.
Wechselspannung
Bereich
(40 Hz bis 400 Hz) Messgenauigkeit Eingangsimpedanz
200,0 V ± (1,2 % + 1,0 V) 450 kΩ
600 V* ± (1,2 % + 10 V)
* Die Messgenauigkeit im 600 V Bereich ist zuverlässig zwischen 20 % und
100 % des Bereichs.
Gleichspannung
Bereich Messgenauigkeit Eingangsimpedanz
20,00 V ± (0,8 % + 0,05 V)
1 MΩ200,0 V ± (0,8 % + 0,5 V)
600 V* ± (1,0 % + 5 V)
* Die Messgenauigkeit im 600 V Bereich ist zuverlässig zwischen 20 % und
100 % des Bereichs.
Widerstand
Bereich Messgenauigkeit Leerlaufspannung
200,0 Ω ± (1,2 % + 0,5 Ω)
< 3 VDC
2000 Ω ± (1,0 % + 5 Ω)
20,00 kΩ ± (1,0 % + 0,05 kΩ)
200,0 kΩ ± (1,0 % + 0,5 kΩ)
2000 kΩ ± (1,2 % + 5 kΩ)
56
Messgenauigkeit (Fortsetzung)
Prüfen der Batterie
Prüfstrom: Ca. 30 mA für 1,5 V, 8 mA für 9 V
Messgenauigkeit: ± (5 % + 0,1 V)
Diodentest
Messbereich: 2000 mV (bei einer Einstellung von 2000 Ω)
Prüfstrom (typisch): 1,0 mA
Leerlaufspannung (typisch): < 3 V
Durchgang
Signal-Schwellenwert: Zwischen 30 Ω und 100 Ω
Technische Daten
Anzeige: 3-1/2 Ziffer-LCD (mit maximal 1999 Punkten)
Polarität: Automatisch
Abfragefrequenz: Ca. 2,5 pro Sekunde
Temperaturkoeffizient: 0,2 x (Messgenauigkeit) pro Grad °C unter 18 °C
oder über 28 °C
Betriebsbedingungen:
Temperatur: 0 °C bis 40 °C
Relative Luftfeuchtigkeit: 0 % bis 75 %
Höhe über NN: max. 2000 m
Nur in Innenräumen verwenden
Verschmutzungsgrad: 2
Lagerbedingungen:
Temperatur: -10 °C bis 50 °C
Relative Luftfeuchtigkeit: 0 % bis 85 %
Batterie herausnehmen
Batterie: Eine 9 V-Batterie (NEDA 1604, JIS 006P oder IEC 6F22)
Überlastschutz: 600 V AC Effektivwert und 600 V DC
Überspannungskategorie: Kategorie III, 600 V
DM-25
57
Messkategorien
Diese Definitionen stammen aus den internationalen Sicherheitsnormen für
Isolierungen – abgestimmt auf die Anwendbarkeit bei Mess-, Steuer- und
Laborgeräten. Genauere Beschreibungen dieser Messkategorien sind in
den beiden folgenden Veröffentlichungen der International Electrotechnical
Commission zu finden: IEC 61010-1 oder IEC 60664.
Messkategorie I
Signalebene. Elektronische und Telekommunikationsgeräte oder deren
Teile. Dazu gehören beispielsweise elektronische Schaltkreise mit
Überspannungsschutz in Fotokopiergeräten oder Modems.
Messkategorie II
Lokalebene. Haushaltgeräte, tragbare Geräte und die Stromnetze, an denen sie
angeschlossen sind. Dazu gehören beispielsweise Lampen, Fernsehgeräte und
lange Abzweigkreise.
Messkategorie III
Verteilungsebene. Fest installierte Maschinen und die Netze, an denen sie
fest angeschlossen sind. Dazu gehören beispielsweise Förderanlagen und
die Hauptstromunterbrechungs-Schalttafeln der elektrischen Anlage eines
Gebäudes.
Messkategorie IV
Primärversorgungsebene. Freileitungen und andere Kabelsysteme. Dazu
gehören beispielsweise Kabel, Elektrizitätszähler, Transformatoren und
sonstige Anlagen im Freien, die der Stromversorgungsgesellschaft gehören.
Konformitätserklärung
Greenlee Textron Inc. ist für seine Qualitätsverwaltungssysteme gemäß
ISO9001 (2000) zertifiziert.
Das gelieferte Gerät wurde mit Betriebsmitteln überprüft bzw. kalibriert, die auf
das National Institute for Standards and Technology (NIST) rückführbar sind.
EEEEEEEEE
58
Wartung
Stromschlaggefahr:
Vor dem Öffnen des Gehäuses die Messleitungen vom Stromkreis entfernen
und das Gerät ausschalten.
Das Nichtbeachten dieser Warnung kann zu schweren oder tödlichen
Verletzungen führen.
Batteriefachdeckel
Batterie
Auswechseln der Batterie
1. Das Gerät vom Netz
trennen. Das Gerät
AUSSCHALTEN.
2. Die Gummikappe
abnehmen.
3. Die Schraube aus dem
Batteriefachdeckel
herausschrauben.
4. Den Deckel des
Batteriefachs abnehmen.
5. Die Batterie austauschen
(dabei die Polarität
beachten).
6. Den Batteriefachdeckel wieder aufsetzen, die
Schraube eindrehen und die Gummikappe erneut anbringen.
Reinigung
Das Gehäuse regelmäßig mit einem feuchten Tuch und einem milden
Reinigungsmittel abwischen. Keine Scheuer- oder Lösungsmittel verwenden.
DM-25
59
Lifetime Limited Warranty
Greenlee Textron Inc. warrants to the original purchaser of these goods for use that
these products will be free from defects in workmanship and material for their useful
life, excepting normal wear and abuse. This warranty is subject to the same terms and
conditions contained in Greenlee Textron Inc.’s standard one-year limited warranty.
For all Test Instrument repairs, contact Customer Service at 800-435-0786 and request a
Return Authorization.
For items not covered under warranty (such as items dropped, abused, etc.), a repair cost
quote is available uponrequest.
Note: Prior to returning any test instrument, please check replaceable batteries or make
sure the battery is at fullcharge.
Garantía limitada válida durante la vida útil del producto
Greenlee Textron Inc. le garantiza al comprador original de estos bienes de uso, que
los mismos estarán libres de defectos de materiales y fabricación durante su vida útil,
excepto en el caso de que sean maltratados o hayan sufrido el deterioro normal. Esta
garantía está sujeta a los mismos términos y condiciones de la garantía estándar limitada
válida por un año, otorgada por Greenlee Textron Inc.
Para reparaciones de todo instrumento de verificación, comuníquese con el Departamento
de Servicio al Cliente al 800-435-0786 y solicite una autorización de devolución.
Puede obtener, previa solicitud, una cotización de precios de reparación para aquellos
artículos que no están cubiertos bajo esta garantía (los que se han dejado caer o han sido
maltratados).
Aviso: Antes de devolver un instrumento de verificación, revise si las baterías están bajas
y es necesario reemplazarlas.
EEEEEEEE
4455 Boeing Drive • Rockford, IL 61109-2988 • USA • 815-397-7070
An ISO 9001 Company • Greenlee Textron Inc. is a subsidiary of Textron Inc.
USA
Tel: 800-435-0786
Fax: 800-451-2632
Canada
Tel: 800-435-0786
Fax: 800-524-2853
International
Tel: +1-815-397-7070
Fax: +1-815-397-9247
www.greenlee.com
Made in China
Garantie à vie limitée
La société Greenlee Textron Inc. garantit à l’acheteur d’origine de ces produits que ces
derniers ne comportent aucun défaut d’exécution ou de matériau pour la durée de leur vie
utile, sauf l’usure normale. Cette garantie est assujettie aux mêmes conditions que celles
contenues dans les modalités et conditions de la garantie limitée standard d’un an de
Greenlee Textron Inc.
Pour toutes les réparations d’instruments de mesure, appeler le service après vente au
800 435-0786 et demander une autorisation de retour.
Lorsque les articles ne sont pas protégés par une garantie (comme si l’appareil tombe,
s’il est soumis à un usage abusif, etc.), une soumission pour le prix de réparation sera
présentée sur demande.
Remarque : Avant de renvoyer un appareil de mesure, veuillez vérifier les piles
remplaçables ou vous assurer que la batterie est complètement chargée.
Lebenslange beschränkte Garantie
Greenlee Textron Inc. garantiert dem Erstkäufer dieser Produkte, dass sie unter Ausschluss
von normalem Verschleiß oder Missbrauch für den Zeitraum ihrer Nutzungsdauer frei von
Bearbeitungs- und Materialfehlern sind. Diese Garantie unterliegt denselben Bedingungen,
die auch für die standardmäßige beschränkte Einjahresgarantie von Greenlee Textron Inc.
gelten.
Bei allen Reparaturen von Messgeräten muss eine Rücksendegenehmigung bei der
Kundendienstabteilung unter +1-800-435-0786 angefordert werden.
Bei Geräten ohne Garantieschutz (z.B. heruntergefallene oder missbrauchte Produkte)
kann auf Anfrage ein Kostenvoranschlag für die Reparatur erstellt werden.
Hinweis: Bitte prüfen Sie vor dem Einsenden des Geräts die austauschbaren Batterien
bzw. stellen Sie sicher, dass die Batterie vollständig geladen ist.

Products related to this Datasheet

DMM 600V AC/DC
Available Quantity: 0
Unit Price: 33.32