SPX-3 Ref Manual Datasheet by VersaLogic Corporation

SPX—3 5% % VERSAIDGIC CORPORATION
Reference
Manual
DOC. REV. 4/9/2013
SPX-3
CANbus Controller
Serial Peripheral Expansion
(SPX) Board
a"? Wmmqq WWW.VERSALOGIC.COM
SPX-3 Reference Manual ii
WWW.VERSALOGIC.COM
12100 SW Tualatin Road
Tualatin, OR 97062-7341
(503) 747-2261
Fax (971) 224-4708
Contents Copyright © 2013
All Rights Reserved
Notice:
Although every effort has been made to ensure this document is error-free, VersaLogic makes no
representations or warranties with respect to this product and specifically disclaims any implied warranties
of merchantability or fitness for any particular purpose.
VersaLogic reserves the right to revise this product and associated documentation at any time without
obligation to notify anyone of such changes.
PC/104 and the PC/104 logo are trademarks of the PC/104 Consortium.
MSPX3
SPX-3 Reference Manual iii
Product Release Notes
Rev. 1
Production release.
Support Page
The SPX support page, at http://www.versalogic.com/private/SPX3support.asp, contains additional
information and resources for this product including:
Reference Manual (PDF format)
Data sheets and manufacturers’ links for chips used in this product
Utility routines and benchmark software
This is a private page for SPX users that can be accessed only be entering this address directly. It cannot
be reached from the VersaLogic homepage.
SPX-3 Reference Manual iv
Table of Contents
Introduction ................................................................................................................... 1
Description .......................................................................................................................... 1
About SPI ............................................................................................................... 1
Technical Specifications ..................................................................................................... 2
RoHS-Compliance .............................................................................................................. 3
About RoHS ........................................................................................................... 3
Warnings ............................................................................................................................. 3
Electrostatic Discharge .......................................................................................... 3
Technical Support ............................................................................................................... 4
Repair Service ........................................................................................................ 4
Physical Details ............................................................................................................. 5
SPX-3 Board Layout ........................................................................................................... 5
Hardware Assembly ............................................................................................... 6
Connector Functions and Interface Cables ......................................................................... 7
Jumper Summary ................................................................................................................ 7
J1 Connector Pinout ............................................................................................................ 7
CANbus .......................................................................................................................... 8
Description .......................................................................................................................... 8
CAN network configuration .................................................................................. 9
External Connections ........................................................................................... 10
Using CANbus ..................................................................................................... 10
Interrupt Selection ............................................................................................... 11
Programming Notes ............................................................................................. 11
SPI Interface ........................................................................................................ 11
Base Board SPI Registers .......................................................................................... 13
SPX-3 Reference Manual 1
Introduction
Description
The VersaLogic SPX-3 is a CANbus expansion module designed to be used with any SPX
enabled base board. Its features include:
Microchip MCP2515 CAN
controller, 2.0B (PeliCAN
compatible) at 1 Mbit/s
Microchip MCP2551 CAN
transceiver, meets or exceeds all
ISO11898-2 standards
0-8 byte length in the data field
Standard 11-bit ID and 29-bit ID
extended data frames
VersaLogic SPX boards are a line of I/O expansion boards using the industry standard Serial
Peripheral Interface (SPI) bus. These are small 1.2” x 3.775” boards that can be mounted on the
PC/104 and PC/104-Plus stack using normal standoffs. They can also mount up to two feet away
from the base board using custom cabling.
SPX boards are electrically connected to a base board via a 14-pin 2 mm cable. Up to four boards
can be daisy-chained together. The SPI bus requires each chip to have a discrete chip-select
signal, and the 14-pin interface supplies four chip-select signals. The maximum clock rate is 8
MHz.
Power for SPX boards is supplied through the interface cable. I/O connections on SPX boards
are provided through screw terminal/wire connections.
All SPX boards are RoHS compliant and industrial temperature rated.
ABOUT SPI
The SPI bus specifies four logic signals: SCLK Serial clock (output from master); MOSI
Master output, slave input (output from master); MISO Master input, slave output (output from
slave); and SS Slave select (output from master).
The SPI implementation on VersaLogic CPU boards adds additional features, such as hardware
interrupt input to the master. The master initiates all SPI transactions. A slave device responds
when its slave select is asserted and it receives clock pulses from the master.
Slave selects are controlled in one of two modes: manual or automatic. In automatic mode, the
slave select is asserted by the SPI controller when the most significant data byte is written. This
initiates a transaction to the specified slave device. In manual mode, the slave select is controlled
by the user and any number of data frames can be sent. The user must command the slave select
high to complete the transaction.
The SPI clock rate can be software configured to operate at speeds between 1 MHz and 8 MHz.
All four common SPI modes are supported through the use of clock polarity and phase controls.
1
Introduction
SPX-3 Reference Manual 2
Technical Specifications
Specifications are typical at 25°C with 5.0V supply unless otherwise noted.
Board Size: 1.2" x 3.775"; SPX compliant
Storage Temperature: -40° C to 85° C
Free Air Operating Temperature:
-40° C to +85° C
Power Requirements:
+5.0V ± 5% @ 25.04 mA (125.2 mW),
(CANbus idle) typ., 100.04 mA (500.2
mW) max.
(Interface cable provides 500 mA total, to be
shared by all SPX modules)
CANbus:
CAN V2.0B at 1 Mbit/s
Standard 11-bit ID and 29-bit ID extended
data frames
Two receive buffers with prioritized message
storage
Six 29-bit filters
Two 29-bit masks
Three prioritized transmit buffers
112 max number of nodes
Minimum bit rate: 15 kbps
Maximum bit rate: 1.0 Mbps*
CANH, CANL Vmax: +40V, -40V
Fundamental Oscillator: 24 MHz
Compatibility:
SPX Full compliance
(Any 3.3V signaling SPI interface, 8 MHz
maximum clock)
Weight: 0.0xx lbs (0.0xx kg)
Compliance:
RoHS Full compliance
CANopen minimum bit rate: 15 kbps
SAE J1939
Specifications are subject to change without notice.
Introduction
SPX-3 Reference Manual 3
RoHS-Compliance
The SPX-3 is RoHS-compliant.
ABOUT ROHS
In 2003, the European Union issued Directive 2002/95/EC regarding the Restriction of the use of
certain Hazardous Substances (RoHS) in electrical and electronic equipment.
The RoHS directive requires producers of electrical and electronic equipment to reduce to
acceptable levels the presence of six environmentally sensitive substances: lead, mercury,
cadmium, hexavalent chromium, and the presence of polybrominated biphenyls (PBB) and
polybrominated diphenyl ethers (PBDE) flame retardants, in certain electrical and electronic
products sold in the European Union (EU) beginning July 1, 2006.
VersaLogic Corporation is committed to supporting customers with high-quality products and
services meeting the European Union’s RoHS directive.
Warnings
ELECTROSTATIC DISCHARGE
Electrostatic discharge (ESD) can damage boards, disk drives, and other components. The circuit
board must only be handled at an ESD workstation. If an approved station is not available, some
measure of protection can be provided by wearing a grounded antistatic wrist strap. Keep all
plastic away from the board, and do not slide the board over any surface.
After removing the board from its protective wrapper, place the board on a grounded, static-free
surface, component side up. Use an antistatic foam pad if available.
The board should also be protected inside a closed metallic anti-static envelope during shipment
or storage.
Sugyon @Ver ng' om
Introduction
SPX-3 Reference Manual 4
Technical Support
If you are unable to solve a problem with this manual please visit the SPX Product Support web
page listed below. If you have further questions, contact VersaLogic technical support at (503)
747-2261. VersaLogic technical support engineers are also available via e-mail at
Support@VersaLogic.com.
REPAIR SERVICE
If your product requires service, you must obtain a Returned Material Authorization (RMA)
number by calling (503) 747-2261. VersaLogic’s standard turn-around time for repairs is five
working days after the product is received.
Please provide the following information:
Your name, the name of your company and your phone number
The name of a technician or engineer that can be contact if any questions arise.
Quantity of items being returned
The model and serial number (barcode) of each item
A detailed description of the problem
Steps you have taken to resolve or recreate the problem
The return shipping address
Warranty Repair All parts and labor charges are covered, including return shipping
charges for UPS Ground delivery to United States addresses.
Non-warranty Repair All non-warranty repairs are subject to diagnosis and labor charges,
parts charges and return shipping fees. Please specify the shipping
method you prefer and provide a purchase order number for invoicing
the repair.
Note Please mark the RMA number clearly on the outside of the box before
returning. Failure to do so can delay the processing of your return.
SPX Support Website
http://www.versalogic.com/private/SPX3support.asp
Inca
SPX-3 Reference Manual 5
Physical Details
SPX-3 Board Layout
The figure below shows the dimensions of the SPX-3 board, as well as the location of
connectors, jumpers, and mounting holes.
Figure 1. SPX-3 Board Layout
(Not to scale. All dimensions in inches.)
2
1
5
1
1.2”
3.775
+
+
+
+
3.375
J1
SPX to Base
Board
J2
CAN
V1
Slave Select
1
0.39
0.55”
0.8”
0.125” DIA x4
Use 3mm or #4
standoffs
V2
Terminating
Resistor
Physical Details
SPX-3 Reference Manual 6
HARDWARE ASSEMBLY
The SPX-3 mounts on two hardware standoffs using the corner mounting holes. These standoffs
are secured to the board, typically across the PC/104 and PC/104-Plus stack locations, using pan
head screws, shown in Figure 2.
Standoffs and screws are available as part number VL-HDW-101.
Figure 2. SPX Board Mounting
Two SPX boards mounted
across the PC/104 and
PC/104-Plus stack locations
Physical Details
SPX-3 Reference Manual 7
Connector Functions and Interface Cables
The following table shows the function of each connector, as well as mating connectors and
cables.
Table 1: Connector Functions and Interface Cables
Connector
Function
Mating
Connector
Transition
Cable
Cable
Description
J1
SPX to Base
Board
FCI 89361-714LF or
equivalent
CBR-1401
CBR-1402
2 SPX Module Cable
4 SPX Module Cable
J2
CANbus
Bare wires to 5-pin
screw terminal
16-28 AWG wire
Jumper Summary
Table 2: Jumper Summary
Jumper
Block
Description
As
Shipped
V1[1-2]
Slave Select 0
In
V1[3-4]
Slave Select 1
Out
V1[5-6]
Slave Select 2
Out
V1[7-8]
Slave Select 3
Out
V2
Termination
In
J1 Connector Pinout
Table 3: J1 Connector Pinout
Pin
Signal Name
Description
1
V5_0
+5.0V
2
SCLK
Serial Clock
3
GND
Ground
4
MISO
Master In Slave Out
5
GND
Ground
6
MOSI
Master Out Slave In
7
GND
Ground
8
SS0#
Slave Select 0
9
SS1#
Slave Select 1
10
SS2#
Slave Select 2
11
SS3#
Slave Select 3
12
GND
Ground
13
SINT#
SPI Interrupt
14
V5_0
+5.0V
Microchiy MCPZSIS CAN comroller MCPZSS] high-speed CAN transceiver MCU CAN Controller Transceiver Nude Node fl 1200 120!) U l l l
SPX-3 Reference Manual 8
CANbus
Description
The CAN system is constructed according to the OSI layered communications model. The SPX-3
provides the data-link and physical layers for a CAN V2.0B interface that operates at speeds of
up to 1 Mbit/s. In this manual, usage of the SPX-3 will be described in consolidation of these two
layers.
The SPX-3 CANbus interface is implemented using the Microchip MCP2515 CAN controller
and MCP2551 high-speed CAN transceiver. For detailed information on these chips, refer to
their respective data sheets.
CAN is a multi-node half-duplex bus system that utilizes Station ID numbers to represent each
node. To transmit data, the transmitting node assembles a data frame, which begins with the
recipient’s Station ID and is followed by up to eight bytes of data payload, and then an
acknowledge period during which the receiving node transmits an acknowledge bit when the
frame is transmitted onto the bus. There are also utility bits within the frame, not mentioned here,
that are used by the nodes to process the frame. See the MCP2515 datasheet for more detailed
information about CAN frames. When a frame is received, the node compares the Station ID to
sets of masks and filters to determine if it should accept the frame payload, or discard it. Filters
and masks can be set up to accept ID-specific frames, all frames (broadcast), or subnet (similar to
Ethernet). The figure below shows a typical CAN network.
Figure 3. Typical CAN Network
3
AN754, Sync Propseg PS1 P32 '3 r (fixed) (Programmableb (Programmable) (Programmable) | | \ \ | I TO I | Um) I 4 CAN BN Tlme Fl
CANbus
SPX-3 Reference Manual 9
CAN NETWORK CONFIGURATION
When setting up a CAN network, the bit timing is critical. Each node may operate with its own
oscillator base frequency that can differ in value from other nodes on the bus. The CAN
controller has configuration settings to “normalize” the oscillator frequency to produce a
Nominal Bit Time that must be common to all nodes on the bus. Microchip’s application note,
AN754, describes in detail the aspects of CAN bit timing as does the MCP2515 datasheet. The
normalized oscillator period is abstracted to discrete Time Quanta (TQ). TQs are then used as the
base time unit for constructing the Nominal Bit Time in several distinct segments. These
segments are used for bus synchronization and cover for the differences in node oscillator base
frequencies and bus length. The figure below shows a CANbus bit as constructed from its base
oscillator.
Figure 4. CANbus Bit
The next aspects to consider for setting up the CAN network are Station IDs, masks and filters.
The MCP2515 allows the use of Extended IDs, increasing the ID size to 29 bits. This gives the
network designer greater flexibility for setting up subnets and organizing data flow. The masks
and filters are set up similarly to the receive buffer register layout and work on either an 11-bit
ID or the 29-bit ID regardless of the type of data frame received. Systems can use any
combination of Standard IDs and Extended IDs for nodes in the same network. The masks and
filters work as shown in Table 4.
CANbus
SPX-3 Reference Manual 10
Table 4: CAN Masks and Filters
ID Mask
Bit
ID Filter
Bit
Station
ID Bit
Accept/Reject
0
X*
X
Accept
1
0
0
Accept
1
0
1
Reject
1
1
0
Reject
1
1
1
Accept
* X = Don’t care.
EXTERNAL CONNECTIONS
CANbus is transmitted through connector J2 of the SPX-3 as shown in the following table.
Table 5: CAN Connectors
J2
Pin
Signal
Name
Description
1
NC
No connection
2
CANH
CAN high-level bus signal
3
CANL
CAN low-level bus signal
4
NC
No connection
5
Ground
Ground
USING CANBUS
Communicating on the CAN bus with the SPX-3 is handled through sets of transmit and receive
buffers within the MCP2515 CAN controller. To transmit a message, one of the three transmit
buffers is selected (the lowest numerical buffer, TXB0, has the highest priority) and the recipient
Station ID is loaded first, followed by up to eight bytes of data. To initiate a transfer, a Request-
To-Send command is sent to the SPX-3, and if the bus is idle, an appropriate CAN data frame
will be transmitted on the bus. If an error is encountered, an error frame may be transmitted by
the remote node indicating so. Reads to the MCP2515 Status and Error Flag Registers can help
pinpoint the problem. Note: If not operating in One-Shot Mode, a frame will be retransmitted
continuously until a valid acknowledge is received by any node on the bus. A good indication of
a mismatch in Bit Time between nodes is the presence of acknowledge errors.
Message reception is done by reading the appropriate receive buffer when it contains a valid
message. The receive buffer, RXB0, has the higher priority. A valid message is one that has
successfully passed through the bit masks and filters of the receiver. Any other CAN frames are
discarded. Notice of a valid message in a receive buffer can be found by polling the Main or
Receive Status Registers or configuring the MCP2515 to generate an interrupt according to
desired conditions.
CANbus
SPX-3 Reference Manual 11
The MCP2551 CAN transceiver has a “slope control” capability to adjust the slew rate of the
CANbus signaling for operation in extremely noisy environments. This setting is controlled by
the use of a resistor, R1, on the SPX-3 (Rs in the MCP2551 datasheet). The default setting is
“High-Speed”: R1 is a 0805 zero-ohm resistor connected to ground. R1 can be replaced with
another 0805 resistor of a desired value to utilize the Slope Control feature. See the MCP2551
datasheet for more information.
INTERRUPT SELECTION
The SPX-3 has a hardware interrupt capability that involves configuring the MCP2515 to choose
among eight sources from which to generate an interrupt. More than one interrupt source is
possible. After this is set, an IRQ can be assigned and enabled in the SPISTATUS register (I/O
address 0x1D9 of EBX-11 Rev. 6.xx or later). Note that all SPI device hardware interrupt signals
are wire-OR’d on the base board, including on-board devices and SPX expansion modules. The
selected IRQ is shared with PC/104 ISA bus devices. CMOS settings must be configured for the
desired ISA IRQ. Care must be given to ensure the interrupt is handled as intended.
PROGRAMMING NOTES
The Microchip MCP2515 CAN controller SPI interface has a range of different commands
designed to take full advantage of its abilities. The VersaLogic SPX controller in its current
revision (EBX-11 Rev 6.xx) fully supports all of these commands. In EBX-11 Rev 5.xx and
below the Bit Modify command, the Load TX Buffer instruction, and Read RX Buffer
instructions were not supported, but all other commands were. These operations can be
performed using normal register read and write instructions. The effects of missing these
commands are primarily an inconvenience to the programmer, but may affect throughput of very
large data payloads due to the extra overhead required for single register SPI read/writes. The
EBX-11 Rev. 6.xx compatible SPX interface incorporates features that allow the use of the full
command set of the MCP2515, and is recommended. Driver support is also planned for future
release.
The SPX-3 incorporates the MCP2515 using an SPI-only configuration. The MCP2515 pins
CLKOUT, TX0RTS, TX1RTS, TX2RTS, RX0BF, and RX1BF pins are not connected.
SPI INTERFACE
All CANbus instructions are sent and received by the base board using the base board’s SPX
interface. The VersaLogic SPI implementation (SPX interface), employs four 8-bit data registers,
SPIDATA3-0. Writing the MSB to the SPIDATA3 register triggers the SPI transaction. See
Appendix A for more information about base board registers.
The MCP2515 operates in SPI Mode 0,0 (SCLK idle low, valid data on rising edge) or mode 1,1
(EBX-11 Rev. 6.xx SPX mode 1,0). Frame lengths vary from 8 bits to 32 bits according to the
instruction. MCP2515 instructions are shown in Table 6 along with their respective frame
lengths.
MCP2515 eel
CANbus
SPX-3 Reference Manual 12
Table 6: CAN Controller Instructions
MCP2515 SPI
Instruction
SPI Frame
Length
MSB Format
Middle Byte
Middle Byte
LSB
Reset
8-bit
0xC0
N/A
N/A
N/A
Read
24-bit
0x03
Register Address
Data Out
N/A
Read Rx Buffer
8-bit manual
1001 0nm0**
N/A
N/A
N/A
Write
24-bit
0x02
Register Address
Data to Write
N/A
Load Tx Buffer
8-bit manual
1001 0abc**
N/A
N/A
N/A
RTS
8-bit
1000 0nnn*
N/A
N/A
N/A
Read Status
16-bit
0xA0
Data Out
Repeat Data
Out
N/A
RX Status
16-bit
0xB0
Data Out
Repeat Data
Out
N/A
Bit Modify
32-bit
0x05
Register Address
Mask Value
Data Value
* The digit selected determines which transmit buffer to send. 0, 2, or 4 send TXB0, TXB1, or
TXB2 respectively. Only one digit may be used.
** Buffer address is selected according to bits n, and m in the case of Rx buffers and a,b, and c in the
case of Tx buffers. Only one buffer is used at a time.
For detailed information regarding the MCP2515 setup and usage, refer to the MCP2515
datasheet and higher OSI layer CAN protocol specification (if used).
SPX-3 Reference Manual 13
Base Board SPI Registers
The following tables describe the SPI control and data registers of the EBX-11 Rev. 6.00
and later. This is the standard set of SPI registers for VersaLogic CPU boards with an
SPX interface. See the reference manual for details and updates.
SPICONTROL (READ/WRITE) 1D8h
D7
D6
D5
D4
D3
D2
D1
D0
CPOL
CPHA
SPILEN1
SPILEN0
MAN_SS
SS2
SS1
SS0
Table 7: SPI Control Register 1 Bit Assignments
Bit
Mnemonic
Description
D7
CPOL
SPI Clock Polarity Sets the SCLK idle state.
0 = SCLK idles low
1 = SCLK idles high
D6
CPHA
SPI Clock Phase Sets the SCLK edge on which valid data will be read.
0 = Data read on rising edge
1 = Data read on falling edge
D5-D4
SPILEN
SPI Frame Length Sets the SPI frame length. This selection works in
manual and auto slave select modes.
SPILEN1 SPILEN0 Frame Length
0 0 8-bit
0 1 16-bit
1 0 24-bit
1 1 32-bit
D3
MAN_SS
SPI Manual Slave Select Mode This bit determines whether the slave
select lines are controlled through the user software or are automatically
controlled by a write operation to SPIDATA3 (1DDh). If MAN_SS = 0, then the
slave select operates automatically; if MAN_SS = 1, then the slave select line
is controlled manually through SPICONTROL bits SS2, SS1, and SS0.
0 = Automatic, default
1 = Manual
D2-D0
SS
SPI Slave Select These bits select which slave select will be asserted. The
SSx# pin on the base board will be directly controlled by these bits when
MAN_SS = 1.
SS2 SS1 SS0 Slave Select
0 0 0 None, port disabled
0 0 1 SPX Slave Select 0, J17 pin-8
0 1 0 SPX Slave Select 1, J17 pin-9
0 1 1 SPX Slave Select 2, J17 pin-10
1 0 0 SPX Slave Select 3, J17 pin-11
1 0 1 On-Board A/D Converter Slave Select
1 1 0 On-Board Digital I/O Ch 0-Ch 15 Slave Select
1 1 1 On-Board Digital I/O Ch 16-Ch 31 Slave Select
A
Base Board SPI Registers
SPX-3 Reference Manual 14
SPISTATUS (READ/WRITE) 1D9h
D7
D6
D5
D4
D3
D2
D1
D0
IRQSEL1
IRQSEL0
SPICLK1
SPICLK0
HW_IRQ_EN
LSBIT_1ST
HW_INT
BUSY
Table 8: SPI Control Register 2 Bit assignments
Bit
Mnemonic
Description
D7-D6
IRQSEL
IRQ Select These bits select which IRQ will be asserted when a hardware
interrupt from a connected SPI device occurs. The HW_IRQ_EN bit must be
set to enable SPI IRQ functionality.
IRQSEL1 IRQSEL0 IRQ
0 0 IRQ3
0 1 IRQ4
1 0 IRQ5
1 1 IRQ10
Note: The on-board digital I/O chips must be configured for open-drain and
mirrored interrupts in order for any SPI device to use hardware interrupts (see
Error! Reference source not found.).
D5-D4
SPICLK
SPI SCLK Frequency These bits set the SPI clock frequency.
SPICLK1 SPICLK0 Frequency
0 0 1.042 MHz
0 1 2.083 MHz
1 0 4.167 MHz
1 1 8.333 MHz
D3
HW_IRQ_EN
Hardware IRQ Enable Enables or disables the use of the selected IRQ
(IRQSEL) by an SPI device.
0 = SPI IRQ disabled, default
1 = SPI IRQ enabled
Note: The selected IRQ is shared with PC/104 ISA bus devices. CMOS
settings must be configured for the desired ISA IRQ.
D2
LSBIT_1ST
SPI Shift Direction Controls the SPI shift direction of the SPIDATA
registers. The direction can be shifted toward the least significant bit or the
most significant bit.
0 = SPIDATA data is left-shifted (MSbit first), default
1 = SPIDATA data is right-shifted (LSbit first)
D1
HW_INT
SPI Device Interrupt State This bit is a status flag that indicates when the
hardware SPX signal SINT# is asserted.
0 = Hardware interrupt on SINT# is deasserted
1 = Interrupt is present on SINT#
This bit is read-only and is cleared when the SPI device’s interrupt is cleared.
D0
BUSY
SPI Busy Flag This bit is a status flag that indicates when an SPI
transaction is underway.
0 = SPI bus idle
1 = SCLK is clocking data in and out of the SPIDATA registers
This bit is read-only.
Base Board SPI Registers
SPX-3 Reference Manual 15
SPI DATA REGISTERS
SPIDATA0 (READ/WRITE) 1DAh
D7
D6
D5
D4
D3
D2
D1
D0
MSbit
LSbit
SPIDATA1 (READ/WRITE) 1DBh
D7
D6
D5
D4
D3
D2
D1
D0
MSbit
LSbit
SPIDATA2 (READ/WRITE) 1DCh
D7
D6
D5
D4
D3
D2
D1
D0
MSbit
LSbit
SPIDATA3 (READ/WRITE) 1DDh
D7
D6
D5
D4
D3
D2
D1
D0
MSbit
LSbit
SPIDATA3 contains the most significant byte (MSB) of the SPI data word. A write to this
register will initiate the SPI clock and, if the MAN_SS bit = 0, will also assert a slave select to
begin an SPI bus transaction. Increasing frame sizes from 8-bit use the lowest address for the
least significant byte of the SPI data word; for example, the LSB of a 24-bit frame would be
SPIDATA1. Data is sent according to the LSBIT_1ST setting. When LSBIT_1ST = 0, the MSbit
of SPIDATA3 is sent first, and received data will be shifted into the LSbit of the selected frame
size set in the SPILEN field. When LSBIT_1ST = 1, the LSbit of the selected frame size is sent
first, and the received data will be shifted into the MSbit of SPIDATA3.