o o 0000
DAQCplate Users Guide
Contents
1 Overview
2 Board Layout
3 Address Selection Header
4 Digital Outputs (DOUT)
o 4.1 Connector
o 4.2 Specifications
o 4.3 Functions
o 4.4 Examples
4.4.1 Simple External LED
4.4.2 Driving an Inductive Load
5 Analog Inputs (ADC)
o 5.1 Connector
o 5.2 Specifications
o 5.3 Functions
o 5.4 Examples
5.4.1 Using a Potentiometer to Generate a Variable Voltage
5.4.2 Measure Temperature Using an LM35 Sensor
6 Digital Inputs (DIN)
o 6.1 Connector
o 6.2 Specifications
o 6.3 Functions
o 6.4 Examples
6.4.1 Monitor an External Button
6.4.2 Measure Temperature with a DS18B20 Temperature Sensor
7 Analog (DAC) and Pulse Width Modulator (PWM) Outputs
o 7.1 Connector
o 7.2 Specifications
7.2.1 PWM
7.2.2 Analog Outputs
o 7.3 Functions
o 7.4 Example
7.4.1 Speed Control of a DC Motor
8 Switch and Bicolor LED
o 8.1 Functions
8.1.1 Bicolor LED
8.1.2 Switch
o 8.2 Using the Switch to Power Down Your Raspberry Pi
8.2.1 Setup
8.2.2 Operation
9 Interrupts
o 9.1 Functions
9.1.1 General
9.1.2 Digital Input
9.1.3 Switch
o 9.2 Example
10 Hybrid Functions
o 10.1 Distance Measurement with the HC-SR04
o 10.2 Connection
o 10.3 Functions
o 10.4 Example
11 Using an Auxiliary Power Supply
LED Array fi'Idraoech , I ,W Digiial Outputs Analog Inputs Digital Inputs
Overview
This page provides the major features of the Pi-Plates DAQCplate Data Acquisition and Control
board. This page can be considered to be a “living” document which means that it will
see continual updates and corrections. All of the code examples below are written for Python 2.7.
However, one of our customers, Jeremy Deters, has coded an experimental C# library along with
a simple dashboard app for Windows 10 IOT. The two archives are available here and here. In
addition, Nahuel Lofeudo has written a Java library for the DAQCplate and the RELAYplate.
These can be downloaded from GitHub here.
http://pi-plates.com/downloads/PiPlates%200.9.3.zip
http://pi-plates.com/downloads/DAQCdashboard.zip
https://github.com/nahuellofeudo/piplates
The following definitions apply in the Function descriptions below:
addr: the address of the DAQCplate board being addressed. Can be 0-7 and is set via the
address selection header described below.
bit: the channel or terminal being controlled by the command.
Board Layout
The terminal blocks and their functions are shown below. Note that you can also look on the
bottom of the board and see the function of each terminal.
2 4 6 Address 0 Addvess 1 Address 2 Address 3 Address 4 Address 5 Address 6 Address 7 r 3 5 open collector
Address Selection Header
Up to eight DAQCplates can be used in a single stack of Pi-Plates. To do this, each board has to
be set to a unique address. When shipped, the DAQCplate is set to address zero. The address is
set by positioning jumpers on the small, six pin header in the upper right corner of board as
shown in the image above. Use the diagram below to set the address:
Note that Pi-Plates only read their address when they are powered up. So you will have to cycle
power to your stack after you change the board address.
Digital Outputs (DOUT)
The digital output connector provides seven open collector outputs, a pair of 5VDC outputs for
driving loads, and a flyback protection terminal for inductive loads. Use these outputs to drive
LED strings, DC motors, relays, solenoids, buzzers, unipolar stepper motors, resistive heating
elements, ultrasonic rangefinders, and incandescent automotive light bulbs. Each digital output
also has a green LED connected to it. Whenever a digital output is turned on the corresponding
green LED will come on. You do not need to connect anything to the digital outputs to control
these LEDs. Conversely, these LEDs will not affect anything that you attach to the digital
outputs.
https://en.wikipedia.org/wiki/Open_collector
Do>m 0 55:0 m .5930 w 59:0 m 55.6 N 55:0 F 59:0 0 59:0 5329a ENS“. Digital Output Connector
Connector
Refer to the diagram at the top of this page as well as the one below to locate the Digital Output
terminals:
Specifications
Each of the 7 Digital Outputs is an open collector Darlington transistor
Maximum sink current is 350mA
Maximum load voltage is 12VDC
On voltage is typically 1.1V with a load current of 200mA
When using a relay or solenoid, the high side power supply should be connected to the
“Flyback Protection” terminal
If necessary, the on-board 5VDC is available on pins 9 and 10. If you choose to use it
then make sure your power supply can provide enough current for your Raspberry Pi
(~700mA), your Pi-Plates (~90mA for each DAQCplate with all LEDs on) and any
components you connect to a DOUT terminal.
Functions
addr must be in the range of 0 through 7
bit must be in the range of 0 through 6
setDOUTbit(addr, bit) – set single bit
clrDOUTbit(addr, bit) – clear single bit
toggleDOUTbit(addr, bit) – toggle a single bit
setDOUTall(addr,byte) – control all seven bits at once. The byte value must be in the
range of 0 through 127.
fritzfing fritzing
Examples
Simple External LED
Use a simple breadboard to build up this LED circuit. Connect the anode of the LED (the long
wire) to one end of a 220 ohm resistor. Route a red wire from the other side of the resistor to a
5VDC terminal on the DAQCplate digital output terminal block. Route a black wire from the
cathode of the LED to Output 0 of the terminal block. Assuming the DAQCplate board is at
address 0, type DAQC.setDOUTbit(0,0) to turn the LED on. Type DAQC.clrDOUTbit(0,0) to
turn off the LED.
Driving an Inductive Load
3:20 p 52. m 5:... m E... q 59: m .22. N :35 — 5::— a .35 :_ on>m 9520 2.23292 I fasuuié I 2.23ng I «52.352 I 2:33.52 I 22.35 I 222325; I 8323.9: l Digital Input Connector Analog Input Connector
1. Use a simple breadboard to build up this 5V solenoid circuit.
2. Connect the red wire from the solenoid to a pair of red wires that route from the
breadboard.
3. Attach one of these to a 5VDC terminal on the DAQCplate digital output terminal block.
4. Connect the other red wire to the Flyback Protection terminal. Route a black wire to
Output 0 of the terminal block.
5. Assuming the DAQCplate board is at address 0, type DAQC.setDOUTbit(0,0) to turn the
solenoid on.
6. Type DAQC.clrDOUTbit(0,0) to turn off the solenoid.
Analog Inputs (ADC)
Use the analog input to measure sensors that produce a variable output voltage. These eight
terminals can be used for measuring voltage, temperature, humidity, light brightness,
potentiometers, strain gauges, and much more.
Connector
Refer to the diagram at the top of this page as well as the one below to locate the Analog Input
terminals:
Specifications
10 bit resolution
4mV per bit
Maximum input voltage: 4.097 volts
Minimum measurable voltage: ~65mV
All inputs have ESD protection
All inputs have over and undervoltage protection
Bandwidth of each input is limited to 50Khz to minimize high frequency noise.
o o o o 000.00.00.33... ..o-...-.- icon-o...- . . . .u-u....-...-.-...-. tau-tooolootnnlvvouo Ito-nooo-oouno-vOI-o .clllo.o-...-.-|l|-n itzi’ng f:
Functions
addr must be in the range of 0 through 7
channel must be in the range of 0 through 8
getADC(addr, channel) – return voltage from single channel. Reading channel 8 will
return the 5VDC power supply voltage.
getADCall(addr) – return voltage from all channels
Examples
Using a Potentiometer to Generate a Variable Voltage
1. Attach a 10K potentiometer to a protoboard as shown on the left side of the diagram
below.
2. Route the red wire to one of the 5VDC terminals (terminal 9 or 10) on the Digital Output
Block
3. Route the black wire to the ground terminal on the Analog Input Block (terminal 9)
4. Route the yellow wire to Analog Input 0 on the Analog Input Block (terminal 1)
5. Go into the Python interactive environment and import the DAQCplate module by typing
import piplates.DAQCplate as DAQC
6. Assuming a DAQCplate board address of 0, type DAQC.getADC(0,0) from the command
prompt and look at the returned value
7. Rotate the “pot” and retype DAQC.getADC(0,0). Turning the “pot” completely clockwise
will return a value of around zero volts. Turning the “pot” almost completely counter
clockwise will return a value of 4.097 volts.
‘53 p .3... m .3... m .a... .. .3... m .3... N .3... . .3; ngital Input Connector a .3... t 55% E5 2.9.3.2.. I 2.2.9.... I 2.2.9.... I 3.2..ng I 9.2.5.3 I 2.2.9.2.. I :..._.._2( I 3.2.3.? I Analog Input Connector
Measure Temperature Using an LM35 Sensor
1. Attach an LM35 temperature sensor to a protoboard as shown on the right side of the
diagram above.
2. Route the red wire to one of the 5VDC terminals (terminal 9 or 10) on the Digital Output
Block
3. Route the black wire to the ground terminal on the Analog Input Block (terminal 9)
4. Route the yellow wire to Analog Input 0 on the Analog Input Block (terminal 1)
5. Go into the Python interactive environment and import the DAQCplate module by typing
import piplates.DAQCplate as DAQC
6. Assuming a DAQCplate board address of 0, type DAQC.getADC(0,0) from the command
prompt and look at the returned value. The LM35 will return a voltage that is
proportional to the temperature in degrees Celsius: 10mV = 1 degree C. If you are
performing this experiment inside then the DAQCplate measurement should return a
value of about 250mV for a temperature of 25C.
7. For more information about the LM35, go here.
http://www.ti.com/lit/ds/symlink/lm35.pdf
Digital Inputs (DIN)
Use the digital inputs to detect simple on-off devices such as buttons, rotary encoders, and the
output of another microcontroller such as an Arduino board. These inputs can also be used to
measure temperature when connected to a DS18B20 1-wire sensor.
Connector
Refer to the diagram at the top of this page as well as the one below to locate the Digital Input
terminals:
Specifications
All inputs have ESD protection
All inputs have over and undervoltage protection
Compatible with 3.3 and 5V logic
All inputs capable of triggering an interrupt to the Raspberry Pi
Special function to directly read DS18B20 1-wire temperature sensor
frvtzmq
Functions
addr must be in the range of 0 through 7
bit must be in the range of 0 through 7
getDINbit(addr,bit) – return single bit value
getDINall(addr) – return all eight bits
enableDINint(addr, bit, edge) – enable interrupts for an input change on the specified bit.
The “edge” value can be ‘r’ for rising, ‘f’ for falling, of ‘b’ for both.
disableDINint(addr,bit) – disable interrupts on the specified bit
getTEMP(addr,bit,scale) – a special function to read a DS18B20 temp sensor attached to
the specified bit input. Scale values can be ‘c’, ‘f’, or ‘k’ for Celsius, Fahrenheit, or
Kelvin. Note that this function takes about 1 second to complete
Examples
Monitor an External Button
1. Attach a normally open push button and a 10K ohm resistor to a protoboard as shown on
the left side of the diagram below
2. Route the red wire to one of the 5VDC terminals (terminal 9 or 10) on the Digital Output
Block
3. Route the black wire to the ground terminal on the Digital Input Block (terminal 9)
4. Route the yellow wire to Digital Input 0 on the Digital Input Block (terminal 1)
5. Go into the Python interactive environment and import the DAQCplate module by typing
import piplates.DAQCplate as DAQC
6. Assuming a DAQCplate board address of 0, type DAQC.getDINbit(0,0) from the
command prompt and look at the returned value. The DAQCplate should return a value
of 1 since the button is up and the input voltage is 5VDC.
7. While pushing the button, execute DAQC.getDINbit(0,0) from the command prompt
again. This time the DAQCplate should have returned a value of 0 since pressing the
button grounds the input.
vwm 7 Mm mm an snow m. mm mung Burma :1 mm om « Gmmd Pan Pwrm Analog and FWM Output Conneclor
Measure Temperature with a DS18B20 Temperature Sensor
1. Attach a DS18B20 temparature sensor and a 4.7K ohm resistor to a protoboard as shown
on the right side of the diagram above
2. Route the red wire to one of the 5VDC terminals (terminal 9 or 10) on the Digital Output
Block
3. Route the black wire to the ground terminal on the Digital Input Block (terminal 9)
4. Route the yellow wire to Digital Input 0 on the Digital Input Block (terminal 1)
5. Go into the Python interactive environment and import the DAQCplate module by typing
import piplates.DAQCplate as DAQC
6. Assuming a DAQCplate address of 0, type DAQC.getTEMP(0,0,’f’) from the command
prompt and look at the returned value. The DAQCplate should return the temperature in
degrees Fahrenheit.
7. Repeat the above but type DAQC.getTEMP(0,0,’k’) instead. The DAQCplate should
return the temperature in degrees Kelvin.
Analog (DAC) and Pulse Width Modulator
(PWM) Outputs
The DAQCplate board provides two linked Pulse Width Modulator (PWM) and Digital to
Analog Outputs. Each PWM can be independently set to any value between 0 and 100% The
analog outputs are simply the PWM signals that have passed through low pass filters. Therefore,
changing the value of PWM0 will alter the value of DAC0 and vice versa. The block diagram
below shows this relationship:
Connector
Refer to the diagram at the top of this page as well as the one below to locate the Analog Out and
and Pulse Width Modulator terminals:
Specifications
PWM
All outputs have ESD Protection
10 bit resolution
Oscillator frequency of 15.9Khz
Analog Outputs
All outputs have ESD protection
Voltage can be set from 0 to 4.097 volts
Derived from passing PWM signal through a 15.9Hz filter.
Functions
addr must be in the range of 0 through 7
channel must be a value of 0 or 1.
setPWM(addr,channel,value) – set PWM signal from 0 to 1023 (0 to 100%)
getPWM(addr,channel) – return current PWM setting. Returned value will be a number
between 0 and 1023.
setDAC(addr,channel,value) – set DAC output voltage from 0 to 4.097 volts.
getDAC(addr,channel) – return current DAC output voltage. Returned value will be
between 0 and 4.097 volts.
calDAC(addr) – calibrate the DAC outputs. Use this function before setting the DAC
value if you are unsure about the quality of your power supply.
Example
Speed Control of a DC Motor
This example assume that you have a small DC motor that operates at 5VDC max and pulls less
than 1 Amp:
Using: the Switch to Power Down Your Raspberry Pi below.
1. Attach the motor, a 1K resistor, a PN2222 NPN transistor, and the wiring to the
protoboard as shown in the diagram above.
https://www.fairchildsemi.com/datasheets/PN/PN2222A.pdf
2. Route the red wire to one of the 5VDC terminals (terminal 9 or 10) on the Digital Output
Block
3. Route the black wire to the ground terminal on the DAC/PWM terminal block (terminal
3)
4. Route the yellow wire to PWM Output 0 on the DAC/PWM terminal block (terminal 4)
5. Go into the Python interactive environment and import the DAQCplate module by typing
import piplates.DAQCplate as DAQC
6. Assuming a DAQCplate address of 0, type DAQC.setPWM(0,0,’512) to set the motor to
approximately half speed.
Switch and Bicolor LED
Each DAQCplate board has a small onboard switch and general purpose bicolor status LED. At
power up, the LED is set to green to indicate a successful hardware initialization. However, you
can use the LED functions below to change it as you see fit for your application.
When using the power control feature of the DAQCplate, pressing the switch will ground the
GPIO18 pin of the Raspberry Pi for approximately 5 seconds while turning on both the red and
green LEDs in the bicolor package. The DAQCplate will then wait for approximately 15 seconds
and then turn off the green LED leaving the red LED on. This indicates that the system is in the
off state and that it is safe to remove power. For more information on how to set up this feature,
jump to the section labeled Using the Switch to Power Down Your Raspberry Pi below.
Functions
Bicolor LED
addr must be in the range of 0 through 7
color values can be 0 for the red LED or 1 for the green.
setLED(addr,color) – turn on one of the LEDs in the bicolor LED package
clrLED(addr,color) – turn off one of the LEDs in the bicolor LED package
Switch
addr must be in the range of 0 through 7
getSWstate(addr) – returns current state of on board switch. A value of 1 is returned
when the switch is up and a value of 0 is returned when it’s down.
enableSWpower(addr) – pushing button on ppGPIO will short RPI GPIO23 to GND and
then remove 5VDC 45 seconds later. Note that this setting is saved in nonvolatile
memory and only has to be performed once. Be sure that you have downloaded and
installed the ppPOWER service described above to take full advantage of this feature.
disableSWpower(addr) – disables the above. Note that this setting is stored in nonvolatile
memory and only has to be performed once.
enableSWint(addr) – allows the switch to generate an interrupt when pressed. Global
interrupts must be enabled before using this function.
disableSWint(addr) – blocks switch on DAQCplate board from generating an interrupt.
Using the Switch to Power Down Your Raspberry Pi
Setup
Setting up your DAQCplate and Raspberry Pi for a graceful shutdown using the push button on
the DAQCplate requires the following steps:
Download, Install, and Run, the ppPower Service
Using the power down feature requires a program running in the background on your Raspberry
Pi that is monitoring GPIO18:
1. From the command line in your home directory execute: wget http://pi-
plates.com/downloads/ppPower-1.00.tar.gz
2. Unpack by executing: tar -xzf ppPower-1.00.tar.gz
3. Enter the ppPower directory: cd ppPower-1.00
4. From the command prompt execute sudo ./install-ppPower
5. The service is now installed and never has to be run again
6. Other functions in the ppPower-1.00 directory include:
1. sudo ./disable-ppPower leaves the software installed but disables auto start-up
feature
2. If auto startup is disabled you can manually start the service with sudo ./start-
ppPower
3. sudo ./stop-ppPower will stop the service at anytime. This feature is useful when
debugging your software
4. sudo .remove-ppPower completely removes the power control service from your
raspberry Pi
Reboot your Raspberry Pi
The ppPower service requires a reboot before installation is complete. To do that execute sudo
reboot from command line. After you’ve logged back into your Raspberry Pi proceed to the next
step.
Setup the Push Button on the DAQCplate to Act as a Power Switch
This is the easy part:
1. Enter the Python interpreter with the sudo python statement at the command prompt
2. Once in the interpreter, load the DAQCplate module with the statement import
piplates.DAQCplate as DAQC
3. Then, assuming an address of 0, tell the DAQCplate that you want to use the push button
as a power switch with the statement DAQC.enableSWpower(0)
4. That’s it. The DAQCplate will now tell the RPI to shut down whenever your press the
button. And, since this setting is saved in the flash memory of the DAQCplate, you never
have to run it again.
5. Exit the interpreter by pressing <CNTL>-D
Operation
When you’re ready to shut down your Raspberry Pi for the day simply push the button on the
DAQCplate. The bicolor LED on the programmed DAQCplate will turn orange for about 15
seconds to indicate that the Raspberry Pi is shutting down. Once it turns red, it is safe to remove
the power to your RPI.
A few notes:
1. If you have multiple DAQCplates in your stack, only one of them has to be programmed
to perform this function. The buttons on the other Pi-Plates are still available for your
applications
2. This service does require that you dedicate the GPIO18 pin on your Raspberry Pi for
monitoring the shutdown signal.
0 SW In7 ln6 lnS In4 In3 In2 In! InO lnlerrupl Flag Register
3. Pressing the button after the LED turns red will just turn the bicolor LED green again. It
will NOT turn your Raspberry Pi back on – that requires a power cycle
Interrupts
For detecting asynchronous events such as button presses and changes on the Digital Input
terminals, the DAQCplate supports the use of interrupts. An excellent tutorial on how to use
interrupts in Python can be found here. Note that Pi-Plates all use the GPIO22 pin on the
Raspberry Pi for generating an interrupt. If you don’t choose to use interrupts, GPIO22 is
available for your applications.
http://raspi.tv/2013/how-to-use-interrupts-with-python-on-the-raspberry-pi-and-rpi-gpio
Functions
General
addr must be in the range of 0 through 7
intEnable(addr) – enable interrupts from the DAQCplate. GPIO22 will be pulled low if
an enabled event occurs.
intDisable(addr) – disables and clears all interrupts on the DAQCplate
getINTflags(addr) – returns 16 bit flag value then clears all INT flags
The interrupt flag register mapping looks like:
Digital Input
addr must be in the range of 0 through 7
bit must be a value between 0 and 7
enableDINint(addr, bit, edge) – enable interrupts for an input change on the specified bit.
The “edge” value can be ‘r’ for rising, ‘f’ for falling, of ‘b’ for both.
disableDINint(addr,bit) – disable interrupts on the specified bit
Switch
addr must be in the range of 0 through 7
Python 2.7.3 (delaull, Mar 18 203 rediv _<|_| »="">
enableSWint(addr) – allows the switch to generate an interrupt when pressed. Global
interrupts must be enabled before using this function.
disableSWint(addr) – blocks switch on DAQCplate from generating an interrupt.
Example
Follow the steps below to get a basic idea of how to set up interrupts using a DAQCplate. To
really take advantage of them in Python, visit the tutorial mentioned above. Let’s start by setting
things up to generate an interrupt if the button is pushed:
pi@rpiBplus ~ $ sudo python
Python 2.7.3 (default, Mar 18 2
0
[GCC 4.6.3] on linux2
Type "help", "copyright", "credi
t
1
2
3
4
5
6
7
pi@rpiBplus ~ $ sudo python
Python 2.7.3 (default, Mar 18 2014, 05:13:23)
[GCC 4.6.3] on linux2
Type "help", "copyright", "credits" or "license" for more information.
>>> import piplates.DAQCplate as DAQC
>>> DAQC.enableSWint(0)
>>> DAQC.intEnable(0)
Verify that the INT line is high:
>>> DAQC.GPIO.input(22)
1
1
2 >>> DAQC.GPIO.input(22)
1
Now push the button and repeat the above:
>>> DAQC.GPIO.input(22)
0
1
2 >>> DAQC.GPIO.input(22)
0
The pushbutton has generated an interrupt! Lets confirm this and the clear the interrupt by
reading the Interrupt Flag Register:
>>> DAQC.getINTflags(0)
256
1
2 >>> DAQC.getINTflags(0)
256
Reading the Interrupt Flag Register indicates that bit 8 is high which maps to the push button.
Let’s confirm that we’ve cleared the interrupt and disable them now that we’re done:
>>> DAQC.GPIO.input(22)
1
>>> DAQC.getINTflags(0)
0
1
2
3
4
5
6
>>> DAQC.GPIO.input(22)
1
>>> DAQC.getINTflags(0)
0
>>> DAQC.intDisable(0)
>>>
And that’s it. Similar functionality is available for the Digital Inputs.
Here’s a second example. Open a new file called InterruptDemo.py with nano then copy and
paste the following code in:
import piplates.DAQCplate as D
A
import RPi.GPIO as GPIO
import time
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
import piplates.DAQCplate as DAQC
import RPi.GPIO as GPIO
import time
def buttonINT(channel):
time.sleep(.01) #debounce button before clearing interrupt
DAQC.getINTflags(0) #clear the interrupt
print " ____ _____ ___ "
print "| _ \ / _ \ \ / / |"
print "| |_) | | | \ \ /\ / /| |"
print "| __/| |_| |\ V V / |_|"
print "|_| \___/ \_/\_/ (_)"
GPIO.setup(22, GPIO.IN, pull_up_down=GPIO.PUD_UP)
GPIO.add_event_detect(22, GPIO.FALLING, callback=buttonINT)
DAQC.enableSWint(0) #enable the push button interrupt
DAQC.intEnable(0) #enable global interrupts
19
20
21
22
23
24
25
26
27
try:
while(1): #Cycle the LEDs on in the foreground
for i in range(0,7):
DAQC.setDOUTbit(0,i) #turn on a single LED
time.sleep(.1) #wait for 100msec
DAQC.clrDOUTbit(0,i) #turn off the LED and go to the next one
#wait for it...
except KeyboardInterrupt:
GPIO.cleanup() # clean up GPIO on CTRL+C exit
Once you’re done, save it and exit from nano. From the command prompt type sudo python
InterruptDemo.py
In the foreground, the above program is cycling the LEDs connected to the DOUT lines. But, if a
button press occurs, GPIO22 is pulled low by the DAQCplate. When the Raspberry Pi detects
this, it jumps to the buttonINT function. There it waits 10msec for a button debounce, clears the
interrupt by reading the Interrupt Flag Register, and then prints out a message. When the
function is complete, the RPI returns to cycling the LEDs.
Watch the lights. Push the button. POW!
Hybrid Functions
Hybrid functions use multiple signals and terminals to perform an operation.
Distance Measurement with the HC-SR04
The HC-SR04 is a low cost and ubiquitous ultrasonic rangefinder that, like a bat, uses reflected
sounds to measure distance. They can be used for robotics, measuring the amount of water in a
tank, or reporting the distance between your car and surrounding obstacles to name just a few
applications. They are also readily available and can be purchased from a number of vendors for
a very reasonable price. The interface requires a Digital Output from the DAQCplate to act as a
trigger and a Digital Input to measure the acoustical flight time. Since the device requires both an
output signal and an input, this is classified as a hybrid function.
Connection
Each HC-SR04 has four pins:
1. Vcc
2. Trigger
3. Echo
4. Ground
Connect Vcc to terminal 9 or 10 on the Digital Output block. Connect Ground to terminal 9 or 10
on the Digital Input . For Trigger and Echo, connection between an HC-SR04 and the
DAQCplate is done via Input/Output pairs. If you choose to measure distance on channel 0 then
you must connect the Trigger to DOUT0 and Echo to DIN0. If instead you want to used channel
6 then you must connect the Trigger to DOUT6 and Echo to DIN6. Up to seven HC-SR04s can
be connected to a single DAQCplate.
Functions
addr must be in the range of 0 to 7
channel must be in the range of 0 to 6
units controls what the units are of the returned value:
‘i’ returns distance in inches
‘c’ returns distance in centimeters
getRANGE(addr,channel,units) – returns distance from sensor in centimeters or inches
depending on the value of units
Example
1. Connect Ground to terminal 10 on the Digital Input block (it’s important to attach ground
first)
2. Connect Vcc (5VDC) to terminal 10 on the Digital Output block.
3. Connect Trig to terminal 2 on the Digital Output Block
4. Connect Echo to terminal 1 on the Digital Input Block
5. Position the sensor so that it is pointing at something nearby like your computer monitor
Follow the steps below and measure distance:
Python 2 (delauu, Mar we 20}
pi@dev-pi1 ~ $ sudo python
Python 2.7.3 (default, Mar 18 2
0
[GCC 4.6.3] on linux2
Type "help", "copyright", "credi
t
1
2
3
4
5
6
7
8
9
10
pi@dev-pi1 ~ $ sudo python
Python 2.7.3 (default, Mar 18 2014, 05:13:23)
[GCC 4.6.3] on linux2
Type "help", "copyright", "credits" or "license" for more information.
>>> import piplates.DAQCplate as DAQC
>>> DAQC.getRANGE(0,0,'i')
10.23
>>> DAQCp.getRANGE(0,0,'c')
25.61
>>>
The above example indicates that my HC-SR04 is just over ten inches or 25.6 centimeters from
my monitor. How cool is that?
Using an Auxiliary Power Supply
The DAQCplate has a pair of terminals on the Analog Input block that allow the use of a
high quality power supply. Reasons you may want to use this feature include:
You want better precision for your Digital to Analog converter output – cheap power
supplies tend to fluctuate with loads and therefore are poor candidates for precise outputs
You plan to stack a lot of Pi-Plates
You need more power for your digital output loads
There are a couple of rules when using this input:
1. It can’t be used with a power supply plugged into the RPI. Well, it -can- but it won’t buy
you anything and we can’t guarantee it will work with future versions of the raspberry Pi.
2. Do not exceed three amps of current – the reverse bias protection circuitry will not like it.
3. Be sure to use a high quality supply with internal fusing. A UL mark is a good indicator
of this.
4. If you use more than one DAQCplate board in your stack, only one can be used for
providing Auxiliary Power. By design, accidentally hooking up multiple supplies on
multiple DAQCplate boards should not cause any damage but, only one of the supplies
will be providing current.
Usage
1. Power down your stack and unplug the power supply currently attached to your
Raspberry Pi.
2. Referring to the image below, loosen the screws on terminals 9 and 10 of the Analog
Input Connector
c. on>m E520 h .3... 935 w .3... 3a.: m .3... 335 q :5... 3.52 m .35 use; a .3... 353 . .2... 32¢ a :35 anE Digital Input Connector Analog Input Connector
3. Noting the polarity, push the positive and negative wires of your power supply into the
5VDC In and Ground terminals and tighten the screws. Don’t worry if you accidentally
connect it backwards – the reverse bias protection circuit will prevent any damage.
4. Plug in your power supply and start coding!
http://pi-plates.com/daqc-users-guide/ 3/14/2017