Celsius to Fahrenheit Conversion Calculator

Celsius Temperature Scale

The Celsius scale is an interval system but not a ratio system, meaning it follows a relative scale but not an absolute scale. This can be seen because the temperature interval between 20°C and 30°C is the same as between 30°C and 40°C, but 40°C does not have twice the air heat energy of 20°C.

A temperature difference of 1 deg C is the equivalent of a temperature difference 1.8°F.

Fahrenheit Temperature Scale

Fahrenheit is a thermodynamic temperature scale, where the freezing point of water is 32 degrees Fahrenheit (°F) and the boiling point 212°F (at standard atmospheric pressure). This puts the boiling and freezing points of water exactly 180 degrees apart. Therefore, a degree on the Fahrenheit scale is 1/180 of the interval between the freezing point and the boiling point of water. Absolute zero is defined as -459.67°F.

A temperature difference of 1°F is the equivalent of a temperature difference 0.556°C.

 

Convert from:

Calculate Reset
Celsius Fahrenheit Kelvin Rankine Delisle Newton Réaumur Rømer

Related Products:

Temperature Sensors, Transducers RTD (Resistance Temperature Detector) Thermocouple, Temperature Probe Thermistors - PTC Thermistors - NTC Test Leads - Thermocouples, Temperature Probes Thermometers
Temperature Sensors, Transducers RTD (Resistance Temperature Detector) Thermocouple, Temperature Probe PTC Thermistors NTC Thermistors Test Leads - Thermocouples, Temperature Probes Thermometers
English  |  Français